Internet of Things
  • Technologies
  • More
Internet of Things
Forum Reinventing the Internet of Things: A Thought Experiment
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 13 answers
  • Subscribers 520 subscribers
  • Views 3047 views
  • Users 0 members are here
  • security
  • internet of things
  • protocols
  • iot
Related

Reinventing the Internet of Things: A Thought Experiment

spannerspencer
spannerspencer over 10 years ago

As discussed in no small part here on element14, and across the big fat Internets, the IoT is simultaneously fantastic, the "next big thing", and also fraught with problems.

 

These include things like security and standardised protocols. Gaps in the IoT concept that are the result of slow, organic evolution rather than systemic design flaws. But flaws they are, nonetheless.

 

And that got me thinking. If we were to invent the Internet of Things today -- deliberately and with forethought -- how would it differ from the ad-hoc network that gradually formed into the IoT we now know?

 

So as something of a thought experiment, I'd be fascinated to hear how you guys would approach it. If you could start afresh with the entire sector and concept of IoT, how would you do it, and what would be yours proceed for putting it all in place?

  • Sign in to reply
  • Cancel

Top Replies

  • spannerspencer
    spannerspencer over 10 years ago in reply to mcb1 +3 suggested
    Certainly I don't mean to suggest it's as essential as water and power, no -- and you're right that it's something we should try not to let ourselves become too reliant on. But right or wrong, I think…
  • crjeder
    crjeder over 10 years ago +3
    Since security is important I'd start reinventing there. But first let us analyse where existing solutions failed. AES is secure and solutions in hard- and software exist. BLE for instance encrypts communication…
  • rsc
    rsc over 10 years ago +2 suggested
    Personally, I have no interest in having my coffee pot, fridge, or microwave connected to the internet. I do have security cameras and such. It'd be nice to know where things went if stolen, so tracking…
Parents
  • mlease
    0 mlease over 10 years ago

    If we had the opportunity to start over again with the Internet of Things, the first thing I would do is not call it the Internet of Things. The "Internet of Things" is less meaningful than VERY broad terms like "transportation" (a Prius to jumbo jets to oil tankers) or "consumer products" (60" plasma TVs to bike computers to iPods) or "networking" (gigabit Ethernet to 4G LTE to Bluetooth).

     

    Unfortunately, when you look at everything that falls under the IoT it does look like a big incoherent mess because there are so many things that are lumped under IoT (mainly by the manufacturers to jump on the IoT bandwagon). The reality is everything in the IoT doesn't need to talk with everything else in the IoT. Within the many segments of the IoT, real standards and de facto standards have been and will continue to emerge. The cost, performance, security and other needs of the applications and devices in each segment will drive those standards.

     

    From a practical perspective, security is obviously a big issue and to a large extent we're still suffering from the lack of security that was originally designed into the Internet. The sheer amount of data that millions of IoT devices can generate will become a bigger issue for Internet congestion, storing all that data and making sense of all that data. Devices that stream massive amounts of data over the Internet should be the exception and smart devices that can interpret and report on the data they capture will hopefully become the norm. Hopefully the market forces will cause that to happen because it isn't the type of thing that can be mandated through standards.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mlease
    0 mlease over 10 years ago

    If we had the opportunity to start over again with the Internet of Things, the first thing I would do is not call it the Internet of Things. The "Internet of Things" is less meaningful than VERY broad terms like "transportation" (a Prius to jumbo jets to oil tankers) or "consumer products" (60" plasma TVs to bike computers to iPods) or "networking" (gigabit Ethernet to 4G LTE to Bluetooth).

     

    Unfortunately, when you look at everything that falls under the IoT it does look like a big incoherent mess because there are so many things that are lumped under IoT (mainly by the manufacturers to jump on the IoT bandwagon). The reality is everything in the IoT doesn't need to talk with everything else in the IoT. Within the many segments of the IoT, real standards and de facto standards have been and will continue to emerge. The cost, performance, security and other needs of the applications and devices in each segment will drive those standards.

     

    From a practical perspective, security is obviously a big issue and to a large extent we're still suffering from the lack of security that was originally designed into the Internet. The sheer amount of data that millions of IoT devices can generate will become a bigger issue for Internet congestion, storing all that data and making sense of all that data. Devices that stream massive amounts of data over the Internet should be the exception and smart devices that can interpret and report on the data they capture will hopefully become the norm. Hopefully the market forces will cause that to happen because it isn't the type of thing that can be mandated through standards.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • crjeder
    0 crjeder over 10 years ago in reply to mlease

    Wasn't the idea of IoT about different things talking to each other? E.g. your car telling your microwave to warm up the food 'cause you 'll arive shortly? Or your dryer talking to the power company to find out which time electricity is cheap enough for the budget you set?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to crjeder

    Hi! Yes, there is a requirement for M2M, P2M and P2P communications supported using IoT (machine-to-machine, people-to-machine, people-to-people).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mlease
    0 mlease over 10 years ago in reply to crjeder

    Yes, the idea of the IoT is things talking to other things (or computers or people and so on). Without going off on a tangent about the silliness and impracticality of many of the examples people spew out about the IoT, in general the things that need to talk to each other fit within application groups. Your home automation system wouldn't talk to the traffic signal on the corner which wouldn't talk with the ATM at the convenience store, each of those would be an application group that would talk with other things within its group.

     

    Even within application groups not everything needs to talk to everything, Your dryer doesn't need to talk with your home theater system which doesn't need to talk to your microwave oven which doesn't need to talk to your security cameras. It wouldn't even make sense for all of them to be on the same network. A security camera would need a high-bandwidth, low-latency network connection 24x7 to provide useful imagery while a window sensor or microwave oven would only very occasionally have short messages to exchange with something else and the network latency would be almost irrelevant. For performance and cost reasons, a window sensor would want some type of low-power mesh network, the microwave could use power-line networking and the security camera would want WiFi or even a wired Ethernet. This also touches on data generation and storage. To really be useful the security camera data would need to be stored for days, easily chewing up gigabytes of disk space (hopefully locally and not in the "cloud"). Most other things in a home network would generate very little data and most of it would be acted upon immediately so there would be little reason to store any of it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer