Internet of Things
  • Technologies
  • More
Internet of Things
Forum Has anyone built a truly low-power camera IoT device on an off-the-shelf SoM?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 518 subscribers
  • Views 811 views
  • Users 0 members are here
  • camera
  • iot
Related

Has anyone built a truly low-power camera IoT device on an off-the-shelf SoM?

inxnik
inxnik 10 months ago

I’m trying to achieve Amazon Ring–level battery life — several months on a 5000 mAh battery — using non-custom SoMs. The device should stay almost at zero power between photo sessions.

So far, all tested platforms (ESP32-S3, ESP32-P4, AmebaPro2 RTL8735BDM, Luckfox RV1103) show deep-sleep consumption ≥ 70 mA, far above the advertised values, making them unsuitable.

We also tested a two-chip architecture (small MCU like ATtiny85 waking the main SoM), but the main issue is boot-to-first-photo time. It must be <1 second, which is hard with Linux-based SoMs — yet only Linux SoMs support proper MIPI sensors like IMX219/IMX708.

Questions:

– Has anyone achieved a low-power camera system (photo only) on an existing SoM, with real deep sleep or fast wake-up?

– Is designing a custom board around a SoC the only realistic solution?

– Or can something like Radxa CM3 + a highly optimized Linux stack (Buildroot, custom suspend modes) reach <1 s wake and low idle power?

– Has anyone successfully built a battery-powered MIPI-camera device with either deep sleep or a two-chip wake architecture?

  • Sign in to reply
  • Cancel

Top Replies

  • obones
    obones 10 months ago +1
    I'm surprised at the levels you see for ESP32. Are you sure you disabled all peripherals and used deep sleep? Here is what I do: esp_sleep_enable_ext0_wakeup( GPIO_NUM_9 , 0 ); epd_poweroff_all…
Parents
  • BigG
    0 BigG 10 months ago

    Why are you focusing just on the SoM? There are range of image sensors with MIPI interface out there, and I'm sure some are more power hungry than others when powering on/off and capturing a frame in different lighting conditions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • BigG
    0 BigG 10 months ago

    Why are you focusing just on the SoM? There are range of image sensors with MIPI interface out there, and I'm sure some are more power hungry than others when powering on/off and capturing a frame in different lighting conditions.