Internet of Things
  • Technologies
  • More
Internet of Things
Forum Has anyone built a truly low-power camera IoT device on an off-the-shelf SoM?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 517 subscribers
  • Views 927 views
  • Users 0 members are here
  • camera
  • iot
Related

Has anyone built a truly low-power camera IoT device on an off-the-shelf SoM?

inxnik
inxnik 11 months ago

I’m trying to achieve Amazon Ring–level battery life — several months on a 5000 mAh battery — using non-custom SoMs. The device should stay almost at zero power between photo sessions.

So far, all tested platforms (ESP32-S3, ESP32-P4, AmebaPro2 RTL8735BDM, Luckfox RV1103) show deep-sleep consumption ≥ 70 mA, far above the advertised values, making them unsuitable.

We also tested a two-chip architecture (small MCU like ATtiny85 waking the main SoM), but the main issue is boot-to-first-photo time. It must be <1 second, which is hard with Linux-based SoMs — yet only Linux SoMs support proper MIPI sensors like IMX219/IMX708.

Questions:

– Has anyone achieved a low-power camera system (photo only) on an existing SoM, with real deep sleep or fast wake-up?

– Is designing a custom board around a SoC the only realistic solution?

– Or can something like Radxa CM3 + a highly optimized Linux stack (Buildroot, custom suspend modes) reach <1 s wake and low idle power?

– Has anyone successfully built a battery-powered MIPI-camera device with either deep sleep or a two-chip wake architecture?

  • Sign in to reply
  • Cancel

Top Replies

  • obones
    obones 11 months ago +1
    I'm surprised at the levels you see for ESP32. Are you sure you disabled all peripherals and used deep sleep? Here is what I do: esp_sleep_enable_ext0_wakeup( GPIO_NUM_9 , 0 ); epd_poweroff_all…
  • obones
    0 obones 11 months ago

    I'm surprised at the levels you see for ESP32.
    Are you sure you disabled all peripherals and used deep sleep?

    Here is what I do:

        esp_sleep_enable_ext0_wakeup(GPIO_NUM_9, 0);
        epd_poweroff_all();

        esp_deep_sleep_start();  // Sleep until we have received a GPIO interrupt

    The epd_poweroff_all() call disables entirely the epaper display that I'm using. Without it, I don't reach the sub mA consumption. Are you sure you did not leave the camera powered on?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG 11 months ago

    Why are you focusing just on the SoM? There are range of image sensors with MIPI interface out there, and I'm sure some are more power hungry than others when powering on/off and capturing a frame in different lighting conditions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lichurbagan
    0 lichurbagan 10 months ago

    If you need months of battery life, MIPI camera and <1 s perceived response then custom hardware is unavoidable, even if you reuse an existing SoC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Workshopshed
    0 Workshopshed 10 months ago in reply to obones

    I've used a simple transistor switch to control the power to things like servos and sensors when trying get the best battery life from a project.

    Also used a lower power sensor to wake the board and camera before.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lichurbagan
    0 lichurbagan 10 months ago in reply to Workshopshed

    What camera did you use? Was it the ESP32-CAM or something else?