Internet of Things
  • Technologies
  • More
Internet of Things
Forum Has anyone built a truly low-power camera IoT device on an off-the-shelf SoM?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 517 subscribers
  • Views 925 views
  • Users 0 members are here
  • camera
  • iot
Related

Has anyone built a truly low-power camera IoT device on an off-the-shelf SoM?

inxnik
inxnik 11 months ago

I’m trying to achieve Amazon Ring–level battery life — several months on a 5000 mAh battery — using non-custom SoMs. The device should stay almost at zero power between photo sessions.

So far, all tested platforms (ESP32-S3, ESP32-P4, AmebaPro2 RTL8735BDM, Luckfox RV1103) show deep-sleep consumption ≥ 70 mA, far above the advertised values, making them unsuitable.

We also tested a two-chip architecture (small MCU like ATtiny85 waking the main SoM), but the main issue is boot-to-first-photo time. It must be <1 second, which is hard with Linux-based SoMs — yet only Linux SoMs support proper MIPI sensors like IMX219/IMX708.

Questions:

– Has anyone achieved a low-power camera system (photo only) on an existing SoM, with real deep sleep or fast wake-up?

– Is designing a custom board around a SoC the only realistic solution?

– Or can something like Radxa CM3 + a highly optimized Linux stack (Buildroot, custom suspend modes) reach <1 s wake and low idle power?

– Has anyone successfully built a battery-powered MIPI-camera device with either deep sleep or a two-chip wake architecture?

  • Sign in to reply
  • Cancel

Top Replies

  • obones
    obones 11 months ago +1
    I'm surprised at the levels you see for ESP32. Are you sure you disabled all peripherals and used deep sleep? Here is what I do: esp_sleep_enable_ext0_wakeup( GPIO_NUM_9 , 0 ); epd_poweroff_all…
Parents
  • obones
    0 obones 11 months ago

    I'm surprised at the levels you see for ESP32.
    Are you sure you disabled all peripherals and used deep sleep?

    Here is what I do:

        esp_sleep_enable_ext0_wakeup(GPIO_NUM_9, 0);
        epd_poweroff_all();

        esp_deep_sleep_start();  // Sleep until we have received a GPIO interrupt

    The epd_poweroff_all() call disables entirely the epaper display that I'm using. Without it, I don't reach the sub mA consumption. Are you sure you did not leave the camera powered on?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Workshopshed
    0 Workshopshed 10 months ago in reply to obones

    I've used a simple transistor switch to control the power to things like servos and sensors when trying get the best battery life from a project.

    Also used a lower power sensor to wake the board and camera before.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Workshopshed
    0 Workshopshed 10 months ago in reply to obones

    I've used a simple transistor switch to control the power to things like servos and sensors when trying get the best battery life from a project.

    Also used a lower power sensor to wake the board and camera before.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • lichurbagan
    0 lichurbagan 10 months ago in reply to Workshopshed

    What camera did you use? Was it the ESP32-CAM or something else?