Internet of Things
  • Technologies
  • More
Internet of Things
Forum RE: Power Connection problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 518 subscribers
  • Views 495 views
  • Users 0 members are here
  • pico
  • raspberry_pi_3
Related

RE: Power Connection problem

GeoForeman
GeoForeman 3 months ago

Hi Everyone, I have a project  that needs to connect rp2040, rapsberry pi pico 0 to modules : HW‑357, 3.7v 4000mA battery, usb for charging, now for other sensors

Ky-008 ,HC-SR501 , NEO-M8, 3V-5V DC vibration motors ,microSD card breakout board / microSD card Adapter, please include the breadboard..

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett 3 months ago in reply to dang74 +4
    If you must have 3.3V you will have a hard choice. To get the most out of a nominal 3.7V Lithium Ion battery you would like to run it down to 3V or even 2.7V. Fully charged it will deliver 4V. For…
  • dougw
    dougw 3 months ago +1
    The battery could have a max voltage higher than its nominal 3.7V , maybe as high as 4.2 V. Pico has a regulator that outputs 3.3V and expects interface signals to be 3.3V compatible. Do you have a specific…
  • dougw
    dougw 3 months ago in reply to dang74 +1
    Systems that require multiple supply voltages are very common and it is much simpler now to use efficient switching converters to meet these requirements than it used to be. It is very common to generate…
Parents
  • robogary
    robogary 3 months ago

    Recommend you first draw or sketch a schematic and check each component for 3.7v capability. You may need to include 5v circuits as well as 3v circuits. 

    I usually build my own breadboard using convenient connectors for power distribution , usually pcb to screw terminals. Ill include screw terminals for an external fuse and on/off switch. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GeoForeman
    GeoForeman 3 months ago in reply to robogary

    Thanks I will draw it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • GeoForeman
    GeoForeman 3 months ago in reply to robogary

    Thanks I will draw it.