Internet of Things
  • Technologies
  • More
Internet of Things
Forum RE: Power Connection problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 518 subscribers
  • Views 491 views
  • Users 0 members are here
  • pico
  • raspberry_pi_3
Related

RE: Power Connection problem

GeoForeman
GeoForeman 3 months ago

Hi Everyone, I have a project  that needs to connect rp2040, rapsberry pi pico 0 to modules : HW‑357, 3.7v 4000mA battery, usb for charging, now for other sensors

Ky-008 ,HC-SR501 , NEO-M8, 3V-5V DC vibration motors ,microSD card breakout board / microSD card Adapter, please include the breadboard..

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett 3 months ago in reply to dang74 +4
    If you must have 3.3V you will have a hard choice. To get the most out of a nominal 3.7V Lithium Ion battery you would like to run it down to 3V or even 2.7V. Fully charged it will deliver 4V. For…
  • dougw
    dougw 3 months ago +1
    The battery could have a max voltage higher than its nominal 3.7V , maybe as high as 4.2 V. Pico has a regulator that outputs 3.3V and expects interface signals to be 3.3V compatible. Do you have a specific…
  • dougw
    dougw 3 months ago in reply to dang74 +1
    Systems that require multiple supply voltages are very common and it is much simpler now to use efficient switching converters to meet these requirements than it used to be. It is very common to generate…
Parents
  • dougw
    dougw 3 months ago

    The battery could have a max voltage higher than its nominal 3.7V , maybe as high as 4.2 V. Pico has a regulator that outputs 3.3V and expects interface signals to be 3.3V compatible. Do you have a specific question about the peripherals you mentioned? Are you looking for a schematic?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • GeoForeman
    GeoForeman 3 months ago in reply to dougw

    Hi, Sorry for being a noob. I want to start with the charging unit, I am using FP6277 as charger / booster, I want to connect the 3.7v 4000mA battery to the FP6277 and raspberry pi pico 0 : RP2040, in such a way that it it can charge the battery while connected to usb port and run and boost the voltage as necessary even without connected to USB. It would be helpful if you can send me a schematics so that I would have an idea. I need to see the connection how it is connected also to pico ports. Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett 3 months ago in reply to GeoForeman

    The FP6277 is a boost converter - not a battery charger.

    You don't need a booster to charge a Lithium Ion battery from USB - just a charger control chip.

    https://www.adafruit.com/product/259

    https://www.amazon.co.uk/Lithium-Battery-Charging-Protection-Functions/dp/B08DQXPNR1/ref=asc_df_B08DQXPNR1

    You could then connect the Pico directly to the battery.

    https://randomnerdtutorials.com/power-raspberry-pi-pico-6-different-ways/#batteries

    I haven't tried or tested any of the above.

    I suggest that you do a good bit more web research before spending money.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett 3 months ago in reply to GeoForeman

    The FP6277 is a boost converter - not a battery charger.

    You don't need a booster to charge a Lithium Ion battery from USB - just a charger control chip.

    https://www.adafruit.com/product/259

    https://www.amazon.co.uk/Lithium-Battery-Charging-Protection-Functions/dp/B08DQXPNR1/ref=asc_df_B08DQXPNR1

    You could then connect the Pico directly to the battery.

    https://randomnerdtutorials.com/power-raspberry-pi-pico-6-different-ways/#batteries

    I haven't tried or tested any of the above.

    I suggest that you do a good bit more web research before spending money.

    MK