Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Building A Direct Digital Synthesis Dual-Channel Signal Generator
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 11 Aug 2018 6:37 AM Date Created
  • Views 28982 views
  • Likes 17 likes
  • Comments 148 comments
  • mbed enabled
  • ad9834
  • signal generator
  • direct digital synthesis (dds)
  • arm mbed
  • freescale
  • mbed os 5
  • dds
  • kinetis
  • direct digital synthesizer
  • ad9954
  • frdm
  • frdm-kl25z
  • radiofrequencych
  • mbed
  • frdm-family
  • frequency synthesizer
  • mbed-os
  • nxp
Related
Recommended

Building A Direct Digital Synthesis Dual-Channel Signal Generator

shabaz
shabaz
11 Aug 2018

Introduction

This blog post discusses some practical implementations of super-low-cost ($30 upward) direct digital synthesis (DDS) based signal generator for home use. To save effort and time, they can all be built around an off-the-shelf microcontroller board, and an off-the-shelf direct digital synthesis (DDS) board.

image

There are several different ideas discussed in this blog post, and all are similar – the principles are exactly the same, just that frequency range and desired control/monitoring capabilities can be chosen to suit needs. They are all be lumped together since they are all so similar.

 

There is a three-minute demo of the user interface here:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

What Does it Do?

This project allows for the creation of controlled sine waves, at a desired frequency. This has uses for testing radio receivers, measuring the frequency response of filters, creating a radio transmission, creating a stimulus for testing amplifiers, and so on.

 

Manipulations such as frequency sweeping, frequency modulation and frequency shift keying (FSK) is possible with this project.

 

This project relies on an external amplifier or attenuator to adjust the signal level, although some limited adjustment is possible without additional hardware.

 

How Does it Work?

For a more in-depth look at DDS, see the blog post here Building a Frequency Synthesiser but briefly, the DDS board constructs a sine wave digitally by sending a table of numbers to a digital to analog converter (DAC). DDS devices allow a desired frequency to be programmed using an internal register (e.g. programmed via an SPI or other I/O bus). The programmed value is fed into a summing device or counter, known as a phase accumulator. This is just responsible for repeatedly adding the programmed value to the existing sum, on each clock cycle. So, if the desired frequency is a low value then the phase accumulator will increment in low values too. If the desired frequency is higher, then the phase accumulator will increment in larger chunks The phase accumulator loops back to zero once it reaches its maximum. Each possible value that the output of the accumulator can take represents a different point on a sinewave. A look-up table is used to convert from the phase accumulator output to an amplitude on the curve of a sine wave. This then drives a DAC and and external filter.

 

Some of the benefits are:

  • Extremely low noise close to the oscillation frequency
  • High granularity (sub-Hz is possible)
  • On-board RAM and instruction set allow for very fast frequency hopping or ramping (it is possible to achieve FM and FSK modulation using this method)

 

A disadvantage of DDS is that there can be some spurious content (usually relatively far away from the selected output frequency) that may need filtering for very demanding applications. Since filters can be expensive, often just a fixed low-pass filter is used, as in the project described here.

 

DDS boards are available from ebay, with a digital input interface, and an RF connector ready for providing the signal output. All that is required is to configure the DDS board to output the desired frequency, using a microcontroller for example.

 

For the project described here, a FRDM-KL25Z microcontroller boardmicrocontroller board is used. It is very low cost (about $15) and easy to program using a USB cable. For more detail about the board and the programming process, see here: Working with FRDM Boards and ARM mbed 

 

The board has 128 kbyte Flash and 16 kbyte RAM, and lots of input/output pins, on a near-credit-card-sized board around 5mm thick - it's really great!

(image source: NXP website)image

 

 

The easiest implementation was to not have any buttons or display on the device, and just enable the USB connection on the FRDM board to become a USB Serial interface. Thus whenever the user wishes to modify the frequency output, all that needs to be done is to connect the board to a PC via USB, and run terminal software such as PuTTY on Windows or ‘screen’ on Mac or Linux. A text-based menu system becomes the user interface.

image

 

With this method, the project can be constructed for about $30 or a bit more, depending on which DDS board is used. I tried two boards; a 0-10 MHz one, and a 0.05-160 MHz board.

 

If a permanent display is desired, an LCD screen can be attached. It adds another $20 to the cost. If buttons are needed, they can be added too. A rotary encoder or even a keypad could also be attached. There are plenty of free pins available on the FRDM board. Although I didn’t do it for this project, for information on how to attach a keypad, see here: Building a USB Keypad: A Mini-Project

 

In summary there’s a lot of flexibility concerning implementation. The core functionality uses the USB Serial menu system however. Code can be added to make use of the display, and buttons/keypad/encoder. I'd also like to incorporate a USB based SCPI interface (based on Jan Cumps SCPI project on element14) at some stage. This blog post is just to give ideas, not all combinations are implemented today so if you modify the code to implement a new combination, please do share the code.

 

The current code implements the text menu system, and rotary encoder for frequency selection, and display update indication of the menu selections and frequency. The plan is to extend rotary encoder usage so that it works with the menu system. So, if the text menu has the options such as sine and ramp at a particular menu level for instance, then the rotary encoder should also allow for selection of these two options before going into the next menu level in the hierarchy.

 

For this project I decided to develop my own menu system called picocli (I originally planned to take a Linux shell’s source code and run it Linux-kernel-less since the FRDM board has just a microcontroller). I may still revert to that, but for now I’m using custom code). It is at proof-of-concept level but functions reliably enough for now to use in this project, and it implements things like help, tab completion and a last-command history. It will be explored more in Part 2.

 

I also had to write a custom rotary encoder library rather than use an existing one, because I wanted to integrate things like velocity based modification of behaviour. Anyway, this was a short exercise compared to writing the menu system.

 

Making the Basic Configuration

The basic implementation (using a DDS board and the FRDM-KL25Z board connected to the PC for control via a USB serial interfaced menu) takes about five minutes to assemble. One or two boards are purchased and wired together with jumper cables.

image

 

For the DC to 10 MHz range, AD9834 boards are purchased. I have only tested a single AD9834 board, but two could be connected in theory if desired, for dual output, but there is no way to synchronise the two board outputs with the AD9834 chip.

 

For approx. 50 kHz to 160 MHz, AD9954 boards are used.

 

Nearly all the wiring throughout the project relied on jumper wires. To make these to custom lengths, this crimp toolthis crimp tool is great. It works with the crimpscrimps and then the result is inserted into SIL and DIL header socket shells. Standard pre-assembled jumper wires could be used too.

image

 

Here is a table of the specific wiring shown in the diagram above:

 

AD9834 DDS board markingFRDM-KL25Z board marking (conn. J9)
FSY  (fsync)B11 (PTB11) J9 pin 7
PS (phase select)B9 (PTB9)   J9 pin 3
SCK (clk)E3 (PTE3)   J9 pin 11
FS (freq select)B10 (PTB10) J9 pin 5
SDA (data)E2 (PTE2)   J9 pin 9
RST (reset)B8 (PTB8)   J9 pin 1
GND (0V)GND           J9 pin 12
5V5V              J9 pin 10

 

 

For using the 160 MHz boards, the connection diagram is below. Please note that I believe this diagram is correct, but I don’t have these actual boards to verify. I used some custom boards (based on the same chip) that I created a while back. However I see no reason why the ebay boards wouldn’t work.

image

 

With a bit of effort, it will be possible to have phase locked and phase adjustable outputs with these 160 MHz boards, since the AD9954 chip supports this capability. I have not tried it yet, because I’m still considering the optimal way to do that (I didn’t originally design my custom boards with that capability in mind : (

 

Still, there is plenty of room in the enclosure to add this capability at a future date once I’ve figured it out.

image

 

Building the Software

Instructions on how to use the development environment and how to push the compiled code into the board are described at the location mentioned earlier: Working with FRDM Boards and ARM mbed 

 

The code can be compiled and then programmed into the board via the USB cable. The next blog post will cover the software, but if you wish to use it now (it won’t be pretty code, it still needs tidying) then please let me know.

 

Using It

Connect up the output of the DDS board to an oscilloscope or spectrum analyzer, plug in the USB connection into the PC and the project should power up! Open up a serial terminal and connect to the board. Hit the Enter key and a command prompt (‘$’) should appear. You can type help or ? for assistance. Generally the menu structure has been designed to accept a command, or a command followed by parameters. Some commands will drop you into a new level in the menu, and you can exit that level by typing exit.

 

So, to output a sinewave at 1.2 MHz, type the following to enter the sinewave mode and invoke the signal output at the desired frequency:

 

$ sine
sine$ frequency 1.2M 
sine$ on

 

Here is another example, to generate a frequency sweep from 2.1 MHz to 2.2 MHz. Here the sweep command will drop you into the sweep mode, so type exit afterwards if you want to go into a different mode. You can type help or ? at any time to get help for the mode that you’re in:

 

sweep
range 2.1M 2.3M
on

 

There are extra parameters that can be configured (press ‘?’ to see the commands to do so) for adjusting the sweep steps and so on. I'd like to add a trigger output on the rear panel, so that the project can be used for basic scalar analysis of things like filters.

image

 

Adding a Display and User Controls

I decided to use an enclosure and front panel similar to what I’ve used before for this project: Building a SMT Pick-and-Place Buddy and so both projects rely on a Hammond instrument case and LCD on the front, and FRDM board stuck at the back so that the USB connector is accessible. The two signal outputs will also be at the back (using SMA connectors) because the front panel ended up becoming too full. It's not very convenient, but I can live with it.

image

 

This time I used a parallel mode LCD which is more inconvenient to use than the I2C displays, but I wanted to use it for the high quality output. The display uses ‘VATN’ LCD technology, which looks very close to Organic LED (OLED) in terms of contrast, when viewed at the right angle. So, it has near-OLED looks, but with LCD display lifetime, which seemed ideal for a test instrument. For the user input, I used a rotary encoder. An optical encoder with no detents is quite good for setting frequency, because it can be rapidly spun for getting from one end of the spectrum to the other in a short time. I used a Marquardt switch too. These almost feel like a keyboard switch, so they are light to press.

 

The Hammond case comes with aluminium plates, but plastic is easier to machine so I replaced the front panel with a black ABS plastic sheet instead, and cut a few other bits of plastic to hold the switch and rotary encoder at a convenient depth. A 3D printer could be used to make these, although I did it manually with sheet plastic.

image

 

After lots of epoxying, the front panel was semi-complete.

image

 

Sanding parts makes them easier to epoxy together. Thread-lock glue was used to hold some of the screwed bits together.

image

 

The particular rotary encoder I had operated at 5V whereas the FRDM-KL25Z board has 3.3V logic inputs, so a couple of potential divider resistor pairs were used on the quadrature encoder output lines, to drop from 5V to 3.3V (I used 1.8k and 3.3k resistors); the resistors can be seen attached to the header socket that will be connected to the rotary encoder in the photo below.

image

 

The LCD screen was a couple of millimetres taller than the inside of the case! : ( so I had to cut a shallow groove in the top and bottom of the case, to accommodate it. A piece of wood was glued to hold the display in the correct position. Jumper cables were used everywhere in case things ever need disassembly.

image

 

Performance

The performance is quite good, but that’s to be expected from DDS technology.

 

Here is what it looks like on an oscilloscope, using the AD9834 board; the output extends down to DC incidentally, because there is no output capacitor on the board.

image

 

The AD9954 board provides for up to 160 MHz output although at the low end it is limited; much lower than 50 kHz results in reduced amplitude, because my board has a transformer on the output. The ebay versions do not have this according to the photos on ebay, so they should extend down to DC.

image

 

It is hard to tell how good or bad a signal is from the ‘scope trace, so the FPC1500 spectrum analyzer was used. A span of 2MHz was examined when the DDS was set to 9.55MHz, and also 134MHz in the case of the AD9954. The result was good. The close-in noise is almost entirely due to the crystal oscillator module. The module on the AD9954 board for example contains an internal phase locked loop (PLL) to generate a 100MHz clock. Another PLL inside the AD9954 multiplies this by 4 to generate a 400MHz internal clock. I have a 400MHz oscillator module (which still uses a PLL) that I may try at some point; it has worse jitter than the 100MHz module, but it means that I can then disable the PLL inside the AD9954. Or I could try to source a better module, but it could get expensive.

 

The AD9834 board uses a similar style of oscillator module, with a PLL inside it too I suspect.

image

 

To see how this compared with a commercial signal generator, I connected a Rigol DG1022Z to the FPC1500. The DG1022Z has a 14-bit DAC internally, as does the AD9954 DDS chip.

 

The result is fairly similar when set to approximately the same power level. At higher output level this situation can change! - see the second spectrum trace below.

image

 

The DG1022Z operates to 25MHz, and I only tested at 10MHz. The AD9954 can go to 160MHz. Of course the DG1022Z is more flexible since it has arbitrary waveform capability too, but if just a sine wave and a few frequency modulation based schemes are required, then the AD9834 or AD9954 are great options.

 

Summary

A simple design has been presented to create a fairly usable signal generator. It costs less than $30 and perhaps half an hour of time to build and program it all. The full enclosure version takes longer of course.

 

It could be extended with an amplifier circuit if desired. If you build this project as-is or extend or modify it, it would be great to hear about it to bounce off ideas.

 

image

  • Sign in to reply
  • shabaz
    shabaz over 6 years ago in reply to derick007

    Hi Derek,

     

    I think you're probably close now that you're making use of the CS and IO_UPD pins. It may be worth putting a 1 millisec delay in between your two update commands (I had a delay in my code).

     

    Anyway, if the code I provided is compared, you can still see some differences.

    For instance, your reset code is:

      //reset the AD9954

      digitalWrite(resetpin, LOW);

      delay(1);                       // delay 1 ms

      digitalWrite(resetpin,HIGH);

      delay(1);

      digitalWrite(resetpin, LOW);

     

     

    and my reset code is:

    // Reset the AD9954 and get the pins into a known state
      RESET_HIGH;
      CS_BAR_HIGH; // initialize *CS to be high
      IO_UPD_LOW; // initialise IO_UPD to be low
      SCLK_LOW; // initialise SCLK to be low (data is toggled in on the rising edge)
      RESET_LOW; // bring the DDS board out of reset

     

    Your reset code doesn't set the pins into a known state inside the reset cycle. I don't know if this will have an effect, but it is worth doing, because my code worked with the AD9954 (using a different processor, not Arduino).

     

    Also, when I look at the first thing you configure after reset, the 'FTW' registers (Frequency Tuning Word), your code is:

     

    byte FTW1 [] = {6, 26, 57, 224, 0};

    digitalWrite(chipselectpin, LOW);     // toggle CS

      for (int i=0; i<5; i=i+1) {

      shiftOut(datapin, clockpin, MSBFIRST, FTW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    Your code is sending one instruction byte (value 6 which represents the register FTW1) and four data bytes. However, my code does this:

    write_bytes(FTW0, data, 4);

     

    i.e. my code is sending the four data bytes to FTW0, not FTW1.

    Since my code works, I think it is worth swapping to FTW0. It is likely FTW1 is only used for ramping outputs, where both FTW0 and FTW1 would need to be set I think.

     

    You may need to set the CFR2 register too (see the code example I sent).

     

    Also, my code sets the ASF register, to set the amplitude. Your code doesn't do that, and the default is zero, which is the lowest amplitude, so you may see an extremely low output (it will definitely not be observable on an oscilloscope).

    With the ASF register setting at its highest 0x3fff value, you should see output if your 'scope is set to 50mV or 100mV per division.

     

    With the 'scope, you can check that each of your pins (A1 to A5) are toggling as expected too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 6 years ago in reply to michaelkellett

    Michael, did as you suggested and made a few other changes - still getting zeros returned on the Arduino serial monitor.

     

    Still convinced the issue is reading from the AD9954.

     

     

    //************************************************ 

    //* SCLK test code for MKRZERO 

    //* rev 0.1 December 2019 

    //************************************************

     

     

    // DECLARING / DEFINING VARIABLES & THEIR TYPES

     

    char clockpin = A1;       // declaring or defining the variable named clockpin as a character type which has a value A1

    char datapin = A2;        // declaring or defining the variable named datapin as a character type which has a value A2

    char resetpin = A3;       // declaring or defining the variable named resetpin as a character type which has a value A3

    char ioupdatepin = A4;    // declaring or defining the variable named ioupdatepin as a character type which has a value A4

    char chipselectpin = A5;     // declaring or defining the variable named chipselectpin as a character type which has a value A5    

     

    // DECLARING / DEFINING DDS REGISTERS

    // INTEGERS ARE THE PRIMARY DATA TYPE FOR NUMBER STORAGE

    // THE DDS HAS 11 REGISTERS WHICH NEED TO BE PROGRAMMED

    // IN THIS EXAMPLE I WILL PROGRAM ONLY 1 REGISTER, FTW1

    // REGISTERS HAVE VARIOUS LENGTHS FROM 2 BYTES TO 5 BYTES

    // I HAVE DECLARED FTW1 AS A 5 BYTE ARRAY

    // THE NUMBER IN FTW1 ARE DECIMAL NUMBERS

     

     

    byte FTW1 [] = {6, 26, 57, 224, 0};      // declaring or defining the variable named FTW0[] (frequency tuning word 1) as a 5 byte array and byte data type

    int readin = 134;

    byte FREQREG[4];                         // This is the array into which I will read the values from FTW1

     

     

    void setup() {

     

      Serial.begin(57600);

     

      pinMode(clockpin, OUTPUT);    // sets pin A1 as OUTPUT

      pinMode(datapin, OUTPUT);    // sets pin A2 as OUTPUT

      pinMode(resetpin, OUTPUT);    // sets pin A3 as OUTPUT

      pinMode(ioupdatepin, OUTPUT);    // sets pin A4 as OUTPUT

      pinMode(chipselectpin, OUTPUT);    // sets pin A5 as OUTPUT

     

      

      //reset the AD9954

     

      digitalWrite(resetpin, LOW);

      delay(1);                       // delay 1 ms

      digitalWrite(resetpin,HIGH);

      delay(1);

      digitalWrite(resetpin, LOW);

     

      // WRITE TO AD9954

     

     

      // FTW1

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, FTW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  FTW1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      digitalWrite(ioupdatepin,HIGH);

      digitalWrite(ioupdatepin, LOW);

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms

     

     

      // READ FROM AD9954

     

      digitalWrite(chipselectpin, LOW);     // toggle CS

     

      shiftOut(datapin, clockpin, MSBFIRST, readin);  // the instruction word to read register FTW1 from AD9954 is sent

     

      // the next few lines transfer data from FTW1 register memory to the i/o buffer latches 

     

      digitalWrite(ioupdatepin, LOW);

      digitalWrite(ioupdatepin,HIGH);

      digitalWrite(ioupdatepin, LOW);

     

      pinMode(datapin, INPUT);    // sets pin A2 as INPUT

     

      for (int i=0; i<4; i=i+1) {

     

      FREQREG[i] = shiftIn(datapin, clockpin, MSBFIRST);

      }

     

      digitalWrite(chipselectpin, HIGH);     // toggle CS

      delay(1);                              // delay 1 ms 

    }

     

     

      void loop() {

     

        digitalWrite(chipselectpin, LOW);     // toggle CS

        delay(1);                              // delay 1 ms

     

          // if (Serial.available() > 0) {

         // FREQREG[0] = Serial.read();

        

        Serial.print(FREQREG[0], DEC);

        delay(10000);

     

       

       

        // FREQREG[1] = Serial.read();

        Serial.print(FREQREG[1], DEC);

        delay(10000);

        Serial.print(FREQREG[2]);

        Serial.print(FREQREG[3]);

     

        digitalWrite(chipselectpin, HIGH);     // toggle CS

        delay(1);                              // delay 1 ms

    }

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to derick007

    This won't work  - you need to crank the /CS (the / means it's active low) for every command.

     

    digitalWrite(ncs_pin, LOW);

    for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW3[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

    digitalWrite(ncs_pin,HIGH);

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derick007
    derick007 over 6 years ago in reply to michaelkellett

    Thanks Michael and Shabaz.

     

    I remember reading somewhere that as the CS pin is active low, it was ok to ground it - thats what I did.

     

    I now toggle the i/o update pin after writing to each register.

     

    I am now trying to read back one of the registers and display in the serial monitor to prove the reading/writing to the AD9954 is correct. Unfortunately I havent had much success and without any proper diagnostic equipment I think I may have bitten off more than I should have.

     

    //************************************************ 

    //* SCLK test code for MKRZERO 

    //* rev 0.1 December 2019 

    //************************************************

     

     

    // DECLARING / DEFINING VARIABLES & THEIR TYPES

     

    char clockpin = A1;       // declaring or defining the variable named clockpin as a character type which has a value A1

    char datapin = A2;        // declaring or defining the variable named datapin as a character type which has a value A2

    char resetpin = A3;       // declaring or defining the variable named resetpin as a character type which has a value A3

    char ioupdatepin = A4;    // declaring or defining the variable named ioupdatepin as a character type which has a value A4

     

    // DECLARING / DEFINING DDS REGISTERS

    // INTEGERS ARE THE PRIMARY DATA TYPE FOR NUMBER STORAGE

    // THE DDS HAS 11 REGISTERS WHICH NEED TO BE PROGRAMMED

    // REGISTERS HAVE VARIOUS LENGTHS FROM 2 BYTES TO 5 BYTES

    // I HAVE DECLARED EACH REGISTER HAS AN ARRAY OF INTEGER TYPE

    // THE NUMBERS IN THE ARRAYS ARE DECIMAL NUMBERS

     

    int CFR1 [] = {0, 174, 0, 112, 8};      // declaring or defining the variable named CFR1[] (control function register 1) as a 5 byte array and integer data type

    int CFR2 [] = {1, 0, 0, 164};           // declaring or defining the variable named CFR2[] (control function register 2) as a 4 byte array and integer data type

    int ASF [] = {2, 0, 0};                 // declaring or defining the variable named ASF[] (amplitude scale factor) as a 3 byte array and integer data type

    int ARR [] = {3, 0};                    // declaring or defining the variable named ARR[] (amplitude ramp rate) as a 2 byte array and integer data type

    int FTW0 [] = {4, 26, 57, 224, 0};      // declaring or defining the variable named FTW0[] (frequency tuning word 0) as a 5 byte array and integer data type

    int POW0 [] = {5, 0, 0};                // declaring or defining the variable named POW0[] (phase offset word) as a 3 byte array and integer data type

    int FTW1 [] = {6, 26, 57, 224, 0};      // declaring or defining the variable named FTW0[] (frequency tuning word 1) as a 5 byte array and integer data type

    int RSCW0 [] = {7, 0, 0, 0, 0};         // declaring or defining the variable named RSCW0[] (ram segment control word 0) as a 5 byte array and integer data type

    int RSCW1 [] = {8, 0, 0, 0, 0};         // declaring or defining the variable named RSCW1[] (ram segment control word 1) as a 5 byte array and integer data type

    int RSCW2 [] = {9, 0, 0, 0, 0};         // declaring or defining the variable named RSCW2[] (ram segment control word 2) as a 5 byte array and integer data type

    int RSCW3 [] = {10, 0, 0, 0, 0};         // declaring or defining the variable named RSCW3[] (ram segment control word 3) as a 5 byte array and integer data type

    int readin = 134;

    int FREQREG[4];

     

     

    void setup() {

     

      Serial.begin(57600);

     

      pinMode(clockpin, OUTPUT);    // sets pin A1 as OUTPUT

      pinMode(datapin, OUTPUT);    // sets pin A2 as OUTPUT

      pinMode(resetpin, OUTPUT);    // sets pin A3 as OUTPUT

      pinMode(ioupdatepin, OUTPUT);    // sets pin A4 as OUTPUT

     

      //reset the AD9954

     

      digitalWrite(resetpin, LOW);

      delay(1);                       // delay 1 ms

      digitalWrite(resetpin,HIGH);

      delay(1);

      digitalWrite(resetpin, LOW);

     

      // WRITE TO AD9954

     

      // CFR1

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, CFR1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to CFR1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // CFR2

     

      for (int i=0; i<4; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, CFR2[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to CFR2 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // ASF

     

      for (int i=0; i<3; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, ASF[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  ASF register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // ARR

     

      for (int i=0; i<2; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, ARR[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  ARR register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // FTW0

     

    for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, FTW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

    }

     

     

    // the next few lines transfer data from the i/o buffer latches to  FTW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // POW0

     

      for (int i=0; i<4; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, POW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  FTW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // FTW1

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, FTW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  FTW1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // RSCW0

     

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW0[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

     

      // the next few lines transfer data from the i/o buffer latches to  RSCW0 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // RSCW1

     

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW1[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

    // the next few lines transfer data from the i/o buffer latches to  RSCW1 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // RSCW2

     

     

      for (int i=0; i<5; i=i+1) {

     

    shiftOut(datapin, clockpin, MSBFIRST, RSCW2[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

      // the next few lines transfer data from the i/o buffer latches to  RSCW2 register memory

     

      digitalWrite(ioupdatepin, LOW);

      delay(1);                         // delay 1 ms

      digitalWrite(ioupdatepin,HIGH);

      delay(1);

      digitalWrite(ioupdatepin, LOW);

     

     

      // RSCW3

     

      for (int i=0; i<5; i=i+1) {

     

      shiftOut(datapin, clockpin, MSBFIRST, RSCW3[i]);  // each bit is approximately 5us. The clock signal also has a period of 5us, 1.5 us ON and 3.5 us OFF.

      }

     

     

      // READ FROM AD9954

     

      shiftOut(datapin, clockpin, MSBFIRST, readin);  // the instruction word to read register FTW1 from AD9954 is sent

     

      pinMode(datapin, INPUT);    // sets pin A2 as INPUT

     

      for (int i=0; i<4; i=i+1) {

     

      FREQREG[i] = shiftIn(datapin, clockpin, MSBFIRST); 

      }

     

      

       

       

    }

     

      void loop() {

     

          if (Serial.available() > 0) {

         // FREQREG[0] = Serial.read();

        

        Serial.print(FREQREG[0], DEC);

        delay(10000);

     

       

       

        // FREQREG[1] = Serial.read();

        Serial.print(FREQREG[1], DEC);

        delay(10000);

        Serial.print(FREQREG[2]);

        Serial.print(FREQREG[3]);

     

          }

       

       

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to derick007

    Hello Derek,

    Shabaz is correct (almost) re the /CS pin, actually it is essential that you control it - see the diagram on page 24 of the AD9954 data sheet - CS is used to frame the serial control messages.

     

    From page 21 you can see that the IO Update pin must be toggled after a write to registers since the data is transferred from buffers to working registers in the AD9954 only on the rising edge

    of UPDATE, synched with the SYNC_CLK (which is an AD5594 output). There is (probably)  no way that the Arduino can sync correctly with the SYNC_CLK so just toggle UPDATE after setting the

    registers and hope for the best.

     

    Your scope only has two channels so you will need to be creative about checking the signals:

    Use ch1 on SCLK and ch2 on SDIO and trigger from the falling edge of /CS - you should see bursts of clock cycles on SCLK and data patterns on SDIO.

     

    I haven't checked the code in the loop{}, and I've no idea exactly what shiftOut() does - but with your scope you should be able to see if its doing what page 24 requires, if not then let us know !

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>