Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Building a Mini 5V Supply in a DB-25 Shell
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 27 Nov 2021 1:42 PM Date Created
  • Views 45580 views
  • Likes 11 likes
  • Comments 9 comments
  • data-logging
  • sensors
  • power supply
  • das240-bat
  • LT3089
  • data logging
  • data_logging
Related
Recommended

Building a Mini 5V Supply in a DB-25 Shell

shabaz
shabaz
27 Nov 2021
Building a Mini 5V Supply in a DB-25 Shell

Table of Contents

  • Introduction
  • Circuit
  • Construction
  • Output Noise
  • Summary

Introduction

This is quite a niche blog post, but may be relevant for anyone who needs a simple, quick, low-noise power supply! This project is PCB-less, it can be very quickly scratched out onto 'resin bonded paper' FR2 copper-clad board, and made to fit into a small enclosure.


My use-case was to connect the power supply to operate sensors, for monitoring with a useful product called DAS240-BAT (click here for a review of it). The DAS240-BAT is a great data recorder. It has lots of channels, electronic switching, and a large display for real-time charting of measurements. (There's also a more integrated DAS220-BAT which I think would suit more users and is lower-cost, and the information below is relevant to both models, although I'll just refer to the DAS240-BAT since that is what I used/tested).


All types of sensors with a voltage output can be directly attached to the DAS240-BAT. Some sensors may require an external power supply or amplifier to operate. There is an almost undocumented feature on the DAS240-BAT that simplifies this – there is a DC power supply output on pins on a 25-way D-Sub connector (DB-25) on the instrument. This project is really simple – it's a small voltage regulator that attaches to that DB-25 connection, to provide 5V for external sensors.

image

Circuit

The DAS240-BAT supplies approximately 12V at up to 200 mA, which is more than enough to power up a few sensors hopefully. One approach would be to just wire up a 7805 regulator and call it a day. I wanted to have a supply with lower noise, in case it affected attached sensors. Hunting through the semiconductor parts bin, I found an LT3089 which seemed perfect – it has low noise (27uV RMS), and can support output current to beyond what the DAS240-BAT can supply anyway, plus the package is really nice for prototyping (it's almost like a surface-mount alternative to TO-220, but with seven pins), and allows for simple heatsinking to a circuit board.

image

Construction

I used single-sided copper-clad FR2 board (it blunts tools less than FR4, and is quite cheap from Aliexpress) and first cut it to size, held the LT3089 chip to it and used a pencil to mark off the location of each of the pins, and then used a 'Scorper' tool to quickly score out the relevant pads for this project. See here for more information on the scorper tool.  A knife could be used too. It's very quick, there's not a lot to do for this project! The layout I used is shown below (click to enlarge):

image
Ten minutes later, the work was complete with the few components soldered. Although I didn't use it here, for a complete ground plane, it is possible to apply adhesive copper tape on the underside of the board (I have not found a source of double-sided copper-clad FR2 board).

image

Here is what it looks like sitting inside the DB25 plastic backshell:

image


After some basic testing, I superglued the wires in place and snapped the backshell shut. Project complete : )


Output Noise

I attached a 100 ohm resistor on the output, so that the load was 50mA (this seemed reasonable for a few sensors), and then tested the supply under three scenarios; (a) inside a biscuit tin powered from a 12V bench supply, (b) in free air powered from a 12V bench supply, and (c) in free air powered from the DAS240-BAT while it was running data acquisition on two channels. The output was connected to a measurement amplifier set to 10 kHz bandwidth, and gain of 100. For more information on the measurement amplifier, click here.

image

For all three scenarios, the result was almost identical; I could not notice a difference. The 'scope trace shows from the automated measurement at the bottom that RMS noise was 1.21mV divided by 100, i.e. 12uV RMS, which is not bad:

image


With just over 500 kHz bandwidth (all filters disabled on the measurement amplifier), the output noise is as shown below, about 25uV RMS.

image

Summary

This was a basic one-evening project, and it turns out that the LT3089 makes a great low-noise supply. I was happy that no circuit board needed to be designed and ordered for this project; it was quicker to just score out the pads on the FR2 board. 


Thanks for reading!

  • Sign in to reply
Parents
  • michaelkellett
    michaelkellett over 4 years ago

    Nice PSU Shabaz. I 've never been into scraping boards but this looks like a convincing argument for it !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 4 years ago

    Nice PSU Shabaz. I 've never been into scraping boards but this looks like a convincing argument for it !