Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Building Frank's Milliohm Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 2 Jan 2019 5:13 AM Date Created
  • Views 10900 views
  • Likes 12 likes
  • Comments 32 comments
  • milliohmmeter
  • 4 wire measurement
  • project14
  • milliohm_measurement
  • milliohm measurement
  • milliohm
  • milliohm meter
Related
Recommended

Building Frank's Milliohm Meter

shabaz
shabaz
2 Jan 2019

Introduction

This short blog post documents the specific component values and any mods done to the revision 1 PCB from  fmilburn  Working Prototype of a Kelvin (4-Wire) Milliohm Meter  Project14  Test Instrumentation entry!

It is a project intended to create a 4-wire measurement meter for 0-4 ohm and 0-40 ohm ranges, with sub-milliohm granularity.

 

It is a physically small test instrument, but works well! In very limited tests, the typical discrepancy between a calibrated commercial meter and this project was ballpark 0.1% although from that one can't promise that will definitely always be the case.

Lego blocks shown for size comparison:

image

 

I recorded a 10-min video with some basic test results:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Schematic

I followed the schematic (Rev 1.0) in Frank's blog post here:

Working Prototype of a Kelvin (4-Wire) Milliohm Meter

Frank kindly sent me a spare PCB to construct it on.

It is better to wait for a Rev 2 board, but here's the values/mods on my PCB currently, I used these values for the tests:

image

 

Enclosure and Assembly

The Bopla enclosureBopla enclosure has two end panels, these were cut/filed. The body of the case needed no modifications, except for trimming some tabs slightly, which support the end panels, but are unnecessary. They were trimmed by scoring and snapping off with pliers (it is soft ABS plastic), so that the panel meter and banana sockets could fit:

image

The 24A banana sockets24A banana sockets (just slight overkill) had to go on the rear panel, there's no space on the front panel : )

image

For the DPDT latching push switchDPDT latching push switch a couple of pieces of 22x10x3mm plastic were used, epoxied, to hold the switch in the correct position behind the front panel. The panel meter is from aliexpress.

I didn't screw or glue in the PCB for now:

image

View from the other end, you can see the switch attachment to the front panel more clearly:

image

 

 

Tests

I've not done much testing, but as can be seen in the video, I measured some resistances and compared with a Keithley DMM 6500. I used some resistance wire that I'd purchased for a different project, and crimped some ferrules on the ends (this is all experimental..):

image

 

Here are the results:

Test # Value according to DMM 6500 Value measured by Milliohm Meter project
1 8.6-8.7 milliohm 8.7 milliohm
2 15.5-15.6 milliohm 15.4 milliohm
3 125.5 milliohm 127.5 milliohm
4 319.9 milliohm 320.4 milliohm
5 3.319 ohm 3.323 ohm

 

The largest discrepancy between the two meters is a 1.6% in test #3, but the difference is around 0.1% ballpark in all other tests, so it could well be that I didn't clip the connectors on the same way for test#3. There is a small difference in location each time the clips are connected and disconnected - it won't be completely identical, although I could have reduced that by not moving the test clips, and swapping the banana plug end each time. Anyway, I only intended to do quick sanity tests, not anything more accurate for now.

 

Also, I've not tested at a value lower than 8.7 milliohm.. there may well be a lower limit of a few milliohms, probably not of practical importance once it is in the (say) 0-3 milliohm ballpark perhaps, but I will check with a lower resistance than 8.7 milliohm at some point.

There is some occasional instability that needs investigating (mentioned in a discussion comment here: https://www.element14.com/community/people/fmilburn/blog/2018/10/18/pcb-for-a-kelvin-4-wire-milliohm-meter#start=25

Note: there was some instability, but this is the solution; add two 10k resistors:

image

Meter Improvement (Conversion to Differential Input)

See the comments below  PCB for a Kelvin (4-Wire) Milliohm Meter for some information about how the meter can be improved, to squeeze a bit more accuracy out of it. The information is reproduced here to make it easier to follow: 

image

image

Bigger is Better?

After completing this build, I decided to start building another one, based on an interim board from Frank (it is not a version 2.0, more a version 1.5 of sorts).

This new one is broadly the same as the one described in this blog post, but with a slightly newer version of PCB. I put it in a bigger case, because I wish to eventually make this one battery powered. It is incomplete, I still need to add the battery power circuitry, and I need to drill the holes for the banana sockets.

image

A view inside the unit:

image

 

Summary

This is just a rev 1.0 project, but it is promising how accurate and stable it is, considering the low cost. It functions well.

It was a lot of fun to construct and try it out this Xmas! The design has a lot of flexibility, and is easy to solder and experiment with. I'm looking forward to seeing the design evolve - it will only improve I think!

I still can't get over how small it looks next to the other test instruments though : )

There is a rev 2 discussion here:  New Improved DIY Milliohm Meter V2.0 

image

  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 7 years ago +7
    That's very neat and compact. The picture of it next to the Keithley box is lovely - perhaps you should have entered it in the Question of Scale competition! How does it get on measuring the DCR of inductors…
  • fmilburn
    fmilburn over 7 years ago +5
    Hi Shabaz, That was a great review! Thanks so much. It was a lot of fun seeing it up next to the Keithley. Your build is fantastic. Most of the credit for the design reaching the current stage goes to…
  • genebren
    genebren over 7 years ago +5
    Hi Shabaz, This was a great write-up on your build and verification of Frank's work. In watching the video, I began to wonder if some of the variations in the readings between to the two instruments might…
  • johnbeetem
    johnbeetem over 7 years ago

    I once had access to a "Short Squeak", an uncalibrated milli-Ohmmeter in the form of a probe with a speaker.  The lower the resistance, the higher the pitch.  It was great for finding shorts, particularly in multi-layer PCBs and ground planes.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jc2048

    Hi Jon,

     

    That's a good idea : ) it does look very cool next to the Keithley meter.

    I have some inductors and transformers to try it on, it could help to count windings on toroids maybe : )

    Also, excellent idea with the MOSFET RDS, I'll try that today too and report back.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 7 years ago

    That's very neat and compact. The picture of it next to the Keithley box is lovely - perhaps you should have entered it in the Question of Scale competition!

     

    How does it get on measuring the DCR of inductors? Is it stable?

     

    I'm also wondering whether you'd get a sensible value for RDS(on) for a power MOSFET. Don't see why not, though the manufacturers do their tests at a much higher current (the MOSFET I've used in the load is tested at 27.5A!) and it does vary a bit with current. It would be a very easy experiment if you wanted to try it (perhaps bias the gate with a 9V battery so that there are no complications in that area).

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jw0752

    It's been awesome seeing the project come together, the brainstorming and the decent documentation and PCB design that worked first time. Looking forward to seeing what other cool things you guys want to work on : )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to jw0752

    Thanks John,

     

    Working collaboratively has made this a lot more fun as well as resulting in a better outcome.  I would welcome the opportunity to do more projects like this.

     

    Frank

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>