Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Energy Saving: Building a Microcontroller-based System Power Controller
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 28 Jun 2022 10:04 PM Date Created
  • Views 89039 views
  • Likes 15 likes
  • Comments 7 comments
  • msp430g
  • low power
  • msp430
Related
Recommended

Energy Saving: Building a Microcontroller-based System Power Controller

shabaz
shabaz
28 Jun 2022

Table of Contents

  • Introduction
  • Using It
  • I2C Instruction Set
    • (a) Wake every n seconds (n is between 5 and 255)
    • (b) Wake every n minutes (n is between 1 and 255)
    • (c) Read Inputs
    • (d) Write Outputs
    • (e) Write to RAM
    • (f) Read from RAM
    • (g) Set RTC Time
    • (h) Set RTC Date
    • (i) Read RTC Time
    • (j) Read RTC Date
  • Building It
  • Testing It
  • Summary


Introduction


For ages, I’ve wanted an easy-to-use flexible/configurable circuit that would send devices to sleep but wake them up when needed. Finally, I got around to it, and this project was the result.


This project can be used to automatically power up and shut down circuits, to conserve battery power.


By default, it will wake up every 30 seconds and then shut down again after 2 seconds. This might be useful for temperature logging for instance. The circuit will also automatically awake if a particular pin input is set high; it could be attached to a push-button for powering on the system for instance.


You can modify the behavior at any time, by using I2C. As an example, you can send an I2C command to change the wake-up rate to 5 minutes, or any other value.


There are also some extra features; I tried to squeeze in as many as practical, within the memory constraints of the microcontroller I’m using for this project.


The extra features are:

  • 64 bytes of I2C-accessible battery-backed RAM for storing useful stuff
  • General-purpose pins for input/output (GPIO), again I2C-accessible
  • I2C-accessible real-time clock (RTC)


The project runs from a coin cell (CR2032) and it should last for several years of operation (average current consumption is under 1 uA).

image


Using It


The circuit diagram below shows how the circuit is used. As mentioned, it operates from a coin cell, but you can also connect it to an external power rail too (for instance, if the main circuit has a 3.3V supply, that can be used). The core component is the MSP430 microcontroller.

image

The PWR_EN pin is an output that switches on the power to the rest of the system. MOSFETs could be used to switch the power, as shown in the example below. This is just one option, it will depend on what is being powered.

image


The KEEP_AWAKE pin is an input to the MSP430 that can be used to keep the system awake for as long as desired. The MSP430 will read the KEEP_AWAKE pin value when power is enabled, and if the pin is high, then the power will continue to be kept enabled until the pin is set low. After it goes low, the KEEP_AWAKE pin won’t be read again until power is next enabled.


The IN0, IN1, OUT0, and OUT1 pins are general-purpose inputs/outputs that can be controlled via I2C. The IN0 pin also serves as an interrupt to power up the system, so it could be attached to a push button for instance, or it could be attached to some sort of trigger or sensor circuit if desired.


I2C Instruction Set


The I2C interface is optional. it’s not necessary to use the I2C interface if the default settings are satisfactory.


It is possible to issue I2C read or write instructions to address 0x40, to configure and operate the device. The I2C address is currently hard-coded to 0x40, but the code could be re-compiled with any value.


The general I2C procedure to send information to the device is to perform an I2C write transaction:


<start><address><instruction><data_1><data_2><data_n><stop>


The general I2C procedure to retrieve information from the device is to use two I2C transactions (the first being an I2C write, and the second being an I2C read):


<start><address><instruction><stop>
<start><address><read_data_1><read_data_2><read_data_n><stop>


Ten different functions, (a) to (j), are currently supported, as listed below. As an example, if it was desired to use function (a) to set the MSP430 to wake up the system every 45 seconds, the following pseudocode could be used:


address=0x40;
buf[0]=0x66;
buf[1]=45;
i2c_write(address, buf, 2); // write 2 bytes to I2C address 0x40

If you wanted to use function (f) to read from RAM locations 10 to 15, the following pseudocode would be used:


address=0x40;
buf[0]=10;
i2c_write(address, buf, 1); // write 1 byte to select the RAM location
i2c_read(address, buf, 6); // read 6 bytes of RAM content
print “RAM was read into buf[0] to buf[5]”;

The following section (a) to (j) documents all the I2C accessible features.

(a) Wake every n seconds (n is between 5 and 255)


Write Instruction: 0x66, data_1: n


(b) Wake every n minutes (n is between 1 and 255)


Write Instruction: 0x67, data_1: n


(c) Read Inputs


Write Instruction: 0x69
Read: n = read_data_1


Bits 0 and 1 of the byte n represent the two inputs. All other bits are to be ignored.


(d) Write Outputs


Write Instruction 0x70, data_1: n


Bits 0 and 1 of the byte n represent the two outputs. All other bits are ignored.


(e) Write to RAM


`Write Instruction i, data_1=n1, data_2=n2, …

The value i is an index between 0-63, to represent the memory locations 0-63. The values n1, n2, etc are any number of bytes to be written from that index location onward


(f) Read from RAM


Write instruction i
Read: n1=read_data_1, n2=read_data_2, …


The value i is an index between 0-63 to represent memory locations 0-63. The values read are retrieved from the index location onward


(g) Set RTC Time


Write Instruction 0x64, data_1=BCD_hour, data_2=BCD_min, data_3=BCD_sec, data_4=am_pm_indication


The values are in BCD format, for instance the 12th hour is represented by 0x12 hexadecimal. The am_pm_indication is 0 for AM, and 1 for PM.


(h) Set RTC Date


Write Instruction 0x65, data_1=year, data_2=month, data_3=date


The year is a value between 0 and 99, representing years since 2000, i.e. 2000 to 2099. The month is a value in the range 1-12. The date is in the range 1-31.


(i) Read RTC Time


Write Instruction 0x64
Read: BCD_hour=read_data_1, BCD_min=read_data_2, BCD_sec=read_data_3, am_pm_indication=read_data_4


See (g) to interpret the read values


(j) Read RTC Date


Write Instruction 0x65
Read: year=read_data_1, month=read_data_2, date=read_data_3


The year value read will be BCD encoded for the two least significant digits. For example if the year is 2022 then the year read will be 0x22. The month is BCD encoded too, but starting at zero. So, November would be read as 0x10. The date (0-31) is BCD encoded, for instance the 27th of the month will be read as 0x27. 

Building It


This project really just consists of the microcontroller, and a few components, as shown in the earlier circuit diagram. To program the microcontroller, the simplest and most cost-effective way is to buy a MSP-EXP430G2ET Launchpad board. It contains a 20-pin DIP socket for programming. It is also possible to program the chip in-circuit. To do that, the following four connections are made:

MSP430 Pin # Programmer Pin Name Notes
1 (VCC) VTARGET Used by the programmer to detect target voltage
20 (VSS) GND
16 (RST/TDIO) TDIO
17 (TCK) TCK (via 330 ohm) Connect a 330 ohm resistor in series

I tested the circuit on a piece of perfboard for now:

image

The source code is on GitHub, and it can be compiled using Code Composer Studio.

The main logic is in a single file called maincode.c, it can be edited if different functionality or default configuration tweaks are desired.

Note that nearly the entire Flash memory on the MSP430G2212 microcontroller is in use, so it will be difficult to add more features without removing some features. If you plan to add more features, then the MSP430G2452 can be used as a drop-in replacement, with four times the Flash capacity. However, it costs more.

Testing It

I decided to test the I2C interface using a Raspberry Pi 4, running I2C test code.

The code is on GitHub, at the same link as before, but in a folder called controller_test. (Note: the code will only run on a Pi 4; to use on older Pi models, it will need a code change which I have not got around to implementing).

To build the code, type make and then run the test by typing ./i2ctest

If the project is working correctly, the test will exercise some of the functionality, and the following output should be displayed.

pi@raspberrypi:~/development/controller_test$ make
g++ -Wall -I/usr/local/include -g -c -o i2cfunc.o i2cfunc.c
g++ -o i2ctest i2cfunc.o i2ctest.cpp -Wall -I/usr/local/include -g -lwiringPi


pi@raspberrypi:~/development/controller_test$ ./i2ctest
writing output
Reading inputs
input is 0x00
selecting address 0x00 and writing 10 bytes to RAM..
clearing local buffer..
reading 10 bytes from address 0 onward:
read 10 bytes: 0x01, 02, 03, 04, 05, 06, 07, 08, 09, 0a,
setting date to 27th June 2022
setting time to 1:19:01 AM
delaying 4 sec..
time is 01:19:05 0
changing wake rate to 10 sec
pi@raspberrypi:~/development/controller_test$


Summary


A simple, but reasonably flexible system power controller was built using an MSP430 microcontroller. It may come in handy for projects that are intended to run from batteries for long periods of time.


Thanks for reading!

  • Sign in to reply
Parents
  • fmilburn
    fmilburn over 4 years ago

    Hi Shabaz,

    Nice project, and very useful.  I learned to program the MSP430G2xxx series microcontrollers when I first became interested in microcontrollers.  As I remember, they don't have an RTC.  I haven't delved into your code yet but am curious why in the I2C instruction set example RTC information is written to and read from the microcontroller.  You must have an interesting application in mind for what is called the "main system" in your block diagram.  Thanks for posting, I still have some MSP430G2xxx processors in my stash and could put this to use.  And as you said in your previous blog, they can be purchased very cheaply right now.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to fmilburn

    Hi Frank,

    Thanks! I'm hoping to use this project for a long-term temperature logger, where the main system is a Pi Pico (which doesn't have great low-power capability). It would be nice to try it with the Raspberry Pi sometime too, since the existing options for it are quite expensive, like this: https://uk.pi-supply.com/products/pijuice-standard

    The RTC is software-based, I found an old PDF TI RTC software app note . 

    It may be useful for timestamp logging etc, so I figured it could be handy to include it, I just added the I2C interface to expose it.

    For other MSP430G2xxx processors, the entire project code will run on them, except that the I2C interface has two implementations, one is called USI, and the other is USCI. I'm using USI, so if the processor only has the USCI integrated peripheral, then the code would need to be modified.

    The processors that have USI include the MSP430G2212 and MSP430G2452 for instance, but there are others too. The MSP430G2553 has USCI so the code would need changing for that. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 4 years ago in reply to fmilburn

    Hi Frank,

    Thanks! I'm hoping to use this project for a long-term temperature logger, where the main system is a Pi Pico (which doesn't have great low-power capability). It would be nice to try it with the Raspberry Pi sometime too, since the existing options for it are quite expensive, like this: https://uk.pi-supply.com/products/pijuice-standard

    The RTC is software-based, I found an old PDF TI RTC software app note . 

    It may be useful for timestamp logging etc, so I figured it could be handy to include it, I just added the I2C interface to expose it.

    For other MSP430G2xxx processors, the entire project code will run on them, except that the I2C interface has two implementations, one is called USI, and the other is USCI. I'm using USI, so if the processor only has the USCI integrated peripheral, then the code would need to be modified.

    The processors that have USI include the MSP430G2212 and MSP430G2452 for instance, but there are others too. The MSP430G2553 has USCI so the code would need changing for that. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fmilburn
    fmilburn over 4 years ago in reply to shabaz

    I mostly have G2553s and a few of the newer FRAM models, but also a lonely G2452.  The project that came to mind for me would use a Raspberry Pi.  Thanks for posting!