Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Kelvin (4-Wire) Milliohm Meter: Version 1.3 Enclosure
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 30 May 2019 5:35 AM Date Created
  • Views 3965 views
  • Likes 7 likes
  • Comments 11 comments
  • test instrum
  • op amp
  • 4-wire measurement
  • test instrumentation
  • milliohm measurement
  • milliohm
  • milliohm meter
  • diytestinstruch
  • instrument
Related
Recommended

Kelvin (4-Wire) Milliohm Meter: Version 1.3 Enclosure

fmilburn
fmilburn
30 May 2019

This post documents an enclosure for the milliohm meter described here and is a tale of how the mechanical bits are often as difficult to get right as the electronics.  The meter parts have been stored away, and thus it was not really available due to the lack of an enclosure.  Today I finally got around to putting it all together.

 

Here it is all wired up but outside of the enclosure:

image

I am not that pleased with the wiring - too easy to bump loose and not that tidy - but easy removal seemed desirable and it could be hot glued or otherwise made more robust.  I have a new crimp tool on order along with different types of connectors so I can make a better job of it next time.

 

Shabaz posted his build based on Version 1.0 and made a comparison to a Keithley DMM 6500 here.  My new build is in a larger enclosure with banana sockets on the front and also incorporates a power on LED and out of range LED.  The enclosure, rocker switches, and panel mounted LEDs  were all ordered at the same time.  Lots of room inside. Unfortunately the enclosure is not quite tall enough and there is not room for labels on the front.  Doh!  Smaller toggle switches and new panel LEDs to match are on order.

image

It is useable again though.  Above it is measuring a 1 ohm 0.5% resistor.  The enclosure came with aluminum end plates but I thought I would try PLA on the 3D printer and that came out quite well I thought.  It took 3 attempts...

 

  • First trial - All of the holes and penetrations were too small by about a millimeter or two.  I "fixed" that with a file so everything fit but my filing was not that even so I modified the model and printed it again.
  • Second trial - Things fit but I didn't like the way it looked :-) and tweaked it a bit.  The volt meter also was a bit wobbly because of the plate thickness so a thicker lip was added around it.
  • Third time a charm - That is what you see above.

 

One of these days would like to make it auto-ranging.  Until then, this will do fine....

 

As I reflect back on this it seems that a element14 user generated brochure with tips on creating robust wiring and enclosures or just good builds in general would be nice...

 

Past Posts on this Project

Milliohm Meter: Version 1.3 First Test

Milliohm Meter: Version 1.0 Shabaz Build

Milliohm Meter: Version 1.0

 

Lots of other posts behind these...

  • Sign in to reply
  • fmilburn
    fmilburn over 6 years ago in reply to spiralphenomena

    One of these days I would like to make another iteration on the design.  As described in the blogs there is an intermittent glitch at low resistances in the less than 20 milliohm range that hasn’t been resolved but which can be worked around.  I think I still have a PCB from the last version.  If you want one contact me by personal message and I will look for it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spiralphenomena
    spiralphenomena over 6 years ago in reply to fmilburn

    I’m going to have to build one of these image thank you for your post

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to spiralphenomena

    Hi Martin,

     

    Yes, one of the switches on the front panel changes the range to 0-4 or 0-400 ohms. The link to 1.3 first test at the bottom of the post has a schematic which shows how it works.

    Frank

     

    edit:  schematic is here. https://www.element14.com/community/groups/open-source-hardware/blog/2019/01/24/kelvin-4-wire-milliohm-meter-version-2

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spiralphenomena
    spiralphenomena over 6 years ago

    Is there a way of manually telling it what range to use?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to jc2048

    Credit to Michael Kellett way back in the first comment to my first blog on this subject for suggesting the MCP6N16 instrumentation amplifier. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>