Passive Components
  • Technologies
  • More
Passive Components
Forum I want to make a capacitor discharge tool
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 15 answers
  • Subscribers 113 subscribers
  • Views 12156 views
  • Users 0 members are here
  • passives_featured
  • capacitor_discharge_tool
Related

I want to make a capacitor discharge tool

jw0752
jw0752 over 8 years ago

I want to make a capacitor discharge tool for use in an industrial application where the voltage may be as high as 400 volts and I have no idea what the maximum capacitance may be. I have been weighing the pros and cons of different resistor values. Then I thought, Why not ask some of the best engineers on the planet? If you have some insights for me it would be appreciated.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +8 suggested
    Sounds like it's for a switch mode power supply. Most of them are 470-1000uF, and to prevent damage you'd want to restrict the current to 1A. R= E/I so 400/1 = 400 ohms. Discharge from here https://www…
  • jw0752
    jw0752 over 8 years ago in reply to jc2048 +7 suggested
    Hi Jon, As promised I have run some experiments after returning home. I have taken a 2000 uF 200 Volt capacitor and charged it up. The formula for energy in a capacitor is 1/2 CV^2 which works out to about…
  • jw0752
    jw0752 over 8 years ago +7 suggested
    Last Post: I put the unit together this afternoon using the advice and wisdom from my Forum friends. The series resistor was lowered to 330 ohms and wattage increased to 5 Watts. I discharged the 2000…
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi John,

     

    Maybe a voltage alert could also be added, although a voltmeter could be used too.

    I was thinking maybe some comparator circuit that would tell you if the voltage is above (say) a few volts. It would have to work both-ways, so something like this window comparator maybe:

    http://www.ti.com/lit/ug/tidub01/tidub01.pdf

     

    It could be run from a dual supply, so that the window straddles 0V. For a suitable comparator, maybe the one used in this circuit: The Engineer’s Multi-Tool - Project Hydra , TLV1701 could be handy, because it could be powered from two 1.5V cells.

     

    On the input there would be some potential divider to reduce the 400V (or higher) down to a far lower value (and some diodes to act as a limiter).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago

    Hi John,

     

    Maybe a voltage alert could also be added, although a voltmeter could be used too.

    I was thinking maybe some comparator circuit that would tell you if the voltage is above (say) a few volts. It would have to work both-ways, so something like this window comparator maybe:

    http://www.ti.com/lit/ug/tidub01/tidub01.pdf

     

    It could be run from a dual supply, so that the window straddles 0V. For a suitable comparator, maybe the one used in this circuit: The Engineer’s Multi-Tool - Project Hydra , TLV1701 could be handy, because it could be powered from two 1.5V cells.

     

    On the input there would be some potential divider to reduce the 400V (or higher) down to a far lower value (and some diodes to act as a limiter).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 8 years ago in reply to shabaz

    Hi Shabaz,

    I like your idea of a discharge level indicator. It could be as simple as once the capacitor is into a window of safe voltage level a light could come on. I have printed the TI paper on Window Comparator Design. Since I have the Multi tool you designed I have all the support documentation on this that I can use to help design it.

    Thanks for your input.

    John

    • Cancel
    • Vote Up +3 Vote Down