Power & Energy
  • Technologies
  • More
Power & Energy
Blog The GaN BoosterPack Series: LMG5200 Evaluation Pack and Smart Instrument
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
  • Author Author: Jan Cumps
  • Date Created: 13 Dec 2016 4:46 PM Date Created
  • Views 3174 views
  • Likes 6 likes
  • Comments 6 comments
  • boosterpack
  • texas_instruments
  • gan
  • scpi
  • hercules
Related
Recommended

The GaN BoosterPack Series: LMG5200 Evaluation Pack and Smart Instrument

Jan Cumps
Jan Cumps
13 Dec 2016

This series of blogs describes the design of a GaN BoosterPack and its LabVIEW integration.

image

The LMG5200 is a GaN Half Bridge that can manage 80V and 10A. This BoosterPack allows you to evaluate the performance of the device. You can change its operating parameters via software and via the on-board rotary encoder.

 

The GaN BoosterPack is designed to be used with a Hercules LaunchPad.

The LaunchPad delivers the complementary signals required to drive the LMG5200 GaN Half Bridge.

The project comes with firmware that allows you to change the driver signals to your needs.

You can change duty cycle, frequency, deadband from LabVIEW or other lab automation software that supports USB and SCPI.

There's stand-alone firmware that changes the duty cycle when you rotate the rotary encoder on the BoosterPack, if you prefer that.

 

All schematics, PCBs, BOM and source code is attached to the blog posts.

 

{gallery} GaN BoosterPack

image

Hercules LaunchPad: proto setup

image

LabVIEW: test SCPI firmware

image

LabVIEW: Control software design

image

Hercules LaunchPad: First tests with a modded LMG5200 evaluation module

image

GaN BoosterPack: first schematic

image

GaN BoosterPack: KiCad 3d viewer

image

LMG5200: Layout Guidelines

image

GaN BoosterPack: one of the evaluation kit (reference design) PCB layers

image

GaN BoosterPack: KiCAD view of an internal PCB layer

image

GaN BoosterPack: Custom KiCAD footprint for LMG5200

image

GaN BoosterPack: Seeed Studio PCBs

image

GaN BoosterPack: Device under test

 

Related Blogs

Hercules LaunchPad and GaN FETs - Part 1: Control Big Power with a Flimsy Mouse Scroll Wheel
Hercules LaunchPad and GaN FETs - Part 2: Make a BoosterPack
Hercules LaunchPad and GaN FETs - Part 3a: BoosterPack Layout - Reference Design
Hercules LaunchPad and GaN FETs - Part 3b: BoosterPack Layout - my version
Hercules LaunchPad and GaN FETs - Side Note A: BoosterPack Layout - Custom KiCad Parts
Hercules LaunchPad and GaN FETs - Side Note B: Look at the PCB
Rotary Encoders - Part 1: Electronics
Checking Out GaN Half-Bridge Power Stage: Texas Instruments LMG5200 - Part 1: Preview
Rotary Encoders - Part 4: Capturing Input on a Texas Instruments Hercules LaunchPad with eQEP
Vintage Turntable repair: Can I fix a Perpetuum Ebner from 1958 - part 4 - Hercules LaunchPad Enhanced PWM try-out

 

 

 

Related Blogs : Smart Instrument with SCPI

Create a Programmable Instrument with SCPI - Part 1: Parser Library
Create a Programmable Instrument with SCPI - Part 2: Serial over USB
Create a Programmable Instrument with SCPI - Part 3: First Conversation *IDN?
Create a Programmable Instrument with SCPI - Part 4: Error Handling by Default
Create a Programmable Instrument with SCPI - Part 5: First Hardware Commands
Create a Programmable Instrument with SCPI - Part 6: LabVIEW Integration
Create a Programmable Instrument with SCPI - Part 7: Talk to Hardware Registers
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps +2
    Oops, maybe a little too over-enthousiast: The right leg of my sophisticated electronic load melted. It was nice to see - happened in just a blink of the eye. The base of that right arm turned red, and…
  • DAB
    DAB over 9 years ago +1
    Nice board work. Looking forward to seeing the board in testing. DAB
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to DAB +1
    It's performing ok at the moment, DAB I'm slowly checking how it behaves under load. I haven't put the design under big pressure yet. Currently running a 10.3V 1.2A load with a 14V input. The GaN package…
Parents
  • DAB
    DAB over 9 years ago

    Nice board work.

     

    Looking forward to seeing the board in testing.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to DAB

    It's performing ok at the moment, DAB

     

    image

     

     

    I'm slowly checking how it behaves under load.

    I haven't put the design under big pressure yet.

    Currently running a 10.3V 1.2A load with a 14V input. The GaN package temperature stabilises at 8° above ambient temperature.

     

    I've done brief tests with 60V input. But I'm trying to avoid vaporising the chip before I had the chance to evaluate the design...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to DAB

    It's performing ok at the moment, DAB

     

    image

     

     

    I'm slowly checking how it behaves under load.

    I haven't put the design under big pressure yet.

    Currently running a 10.3V 1.2A load with a 14V input. The GaN package temperature stabilises at 8° above ambient temperature.

     

    I've done brief tests with 60V input. But I'm trying to avoid vaporising the chip before I had the chance to evaluate the design...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps

    After a few hours with 60V 25mA in, 7.7V (unknown current) out, the inductor and IC run at 60°. The PCB i 50°C.

    Room temperature 21°.

     

    There's no cooling involved. No air flow or heatsink...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps

    Oops, maybe a little too over-enthousiast:

     

    image

     

     

    The right leg of my sophisticated electronic load melted.

    It was nice to see - happened in just a blink of the eye.

    The base of that right arm turned red, and the whole thing melted down int a ball. Not in a flash, but in a fluent gracious flow.

     

    Anyway, I'll have to produce a new load - I may use a similar setup as jc2048 with his matrix of resistors...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago in reply to Jan Cumps

    At least you did not release the magic smoke.

     

    DAB