Power & Energy
  • Technologies
  • More
Power & Energy
Forum Power supply for a tethered drone
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 281 subscribers
  • Views 5039 views
  • Users 0 members are here
Related

Power supply for a tethered drone

roineust
roineust over 4 years ago

There is a drone which I'm experimenting with and want to move from batteries to a 2-15 meters 14AWG tethered cable.

The drone voltage is 15-21 Volts and consumes up to 200 Amps.

What would be the best method of searching for and the best brand, model and condition new or used, to find a good but not expensive power supply for the drone?

What are the chances that the following ebay unbranded power supply, would be a bad choice?

www.ebay.com/.../284832076705

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 4 years ago +4
    I think you would be risking your $1200 - I've had mixed results from very low cost power supplies, never tried one as big as this. That's a very low price for a 6kw power supply - the spec on Ebay isn…
  • Gough Lui
    Gough Lui over 4 years ago +4
    Aside from that very suspect power supply, the cable is not going to be cheap or light. Just look at the ampacity charts ( learnmetrics.com/.../) and it seems you need something about 85mm^2 cross-section…
  • dougw
    dougw over 4 years ago +4
    That sounds like a beast of a drone - over 5 horsepower. At 200 Amps you would be looking at welding cables. Even the mains supply will need to be pretty substantial. Are you planning to put the power…
Parents
  • strb
    strb over 4 years ago

    My two cents: if you want to use a power supply to power up any kind of motor instead of a "traditional" battery please keep one thing in mind: batteries are bi-directional (they can sink or source current) while most power supplies are uni directional (they can only source, not sink). Every time you slow down your motor will discharge stator inductance on whatever is connected to it. That could create a huge voltage spike and over time it will damage the power supply if it can't sink current.

    I don't know how drone motors behave but in RC cars that's something to keep in mind. Even with battery and additional filtering capacitors this effect is noticeable.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • roineust
    roineust over 4 years ago in reply to strb

    Can the following power supply sink current:

    www.jameco.com/.../SE-1500-15-MEAN-WELL-AC-to-DC-Power-Supply-Single-Output-15-Volt-100-Amp-1-5kw_2104073.html

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • roineust
    roineust over 4 years ago in reply to strb

    Can the following power supply sink current:

    www.jameco.com/.../SE-1500-15-MEAN-WELL-AC-to-DC-Power-Supply-Single-Output-15-Volt-100-Amp-1-5kw_2104073.html

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to roineust

    ALL PS can sink or source 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago in reply to roineust

    Only two-quadrant (or four-quadrant) supplies technically will sink as well as source.

    Regular power supplies are made to source only, with a very limited amount of sink (usually a resistor in lower-cost supplies) for transient down-regulation. You are likely to cause OVP trips on attempting to slow-down the motor due to back-EMF.

    I wouldn't choose a 15V supply to power something that can accept 15-21V. The cable losses will reduce the voltage available so you may not have enough at the load to even run.

    The advice from shabaz to start small is very good advice.

    - Gough

    • Cancel
    • Vote Up +3 Vote Down