Power & Energy
  • Technologies
  • More
Power & Energy
Forum You might not want to monitor your electricity, but I do! Help?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 283 subscribers
  • Views 1786 views
  • Users 0 members are here
  • internet of things
  • raspberry pi
  • iot
  • power usage
  • energy efficiency
  • electricity monitoring
  • arduino
Related

You might not want to monitor your electricity, but I do! Help?

cstanton
cstanton over 10 years ago

Last month I asked people over Twitter and on the element14 Community how you monitored your electrical usage. I was surprised to discover that a lot of people, don't. I'm not to be dissuaded when there's statistics to be had, especially when it's something close to home (oh dear, I'm resorting to puns).

 

So I have one of these electricity monitors:

 

image

 

That my electric provider gave me, turns out they're really common, except I'm having a hard time determining how to get data out of it. You see, there's an RJ45 socket on the underside of it, which it turns out, dumps serial, but I cannot discover an authoritative answer on its pinout, though it turns out there are cables you can buy that're 'pre-made' for this, apparently it's also 3v3 logic. I decided to make my own:

 

image

 

Part one of my troubles is, how do I work out the correct pinout? Admittedly I am a novice when it comes to using oscilloscopes (and they're too high priced for my tastes) so what's a safe hack-ey way I can go about this? (the USB device in the pic' happens to be a UART type device which usefully has pins on it).

 

Part two of my troubles, is how shall I handle the data it outputs? About every second, it apparently dumps out XML over serial. Something like this:

 

<msg>                            start of message

   <src>CC128-v0.11</src>        source and software version

   <dsb>00089</dsb>              days since birth, ie days run

   <time>13:02:39</time>         24 hour clock time as displayed

   <tmpr>18.7</tmpr>             temperature as displayed

   <sensor>1</sensor>            Appliance Number as displayed

   <id>01234</id>                radio ID received from the sensor

   <type>1</type>                sensor Type, "1" = electricity

   <ch1>                         sensor channel

      <watts>00345</watts>       data and units

   </ch1>

   <ch2>

      <watts>02151</watts>

   </ch2>

   <ch3>

      <watts>00000</watts>

   </ch3>

</msg>                           end of message

 

I thought that perhaps I should connect it to an ArduinoArduino, or perhaps a Raspberry PiRaspberry Pi? I will need a way to do the following:

 

  • Receive the data and ensure it is legible
  • Store the data so that we can use it
  • Ensure the data is stored at an accurate or relevant timestamp (apparently the device just counts from when it was turned on)
  • Convert the values it gives to something that makes sense
  • Present the values that its stored in ways that are useful and relevant to cost
    • Such as graphs over time

 

The way I see this being useful, is to correlate the electricity usage with house temperature, external house temperature, and maybe further down the line link in my central heating system, so I'm creating almost a house profile, or prevent something turning on when electricity usage is high (for example, electricity is of course used when the boiler kicks in for the water pump, but I'm getting ahead of myself).

 

With all this in mind, does this change anyone else's mind about monitoring their electrical usage? Or perhaps someone can give me advice on where to begin with either part of this project? Or should I construct an electricity monitor out of something else entirely?

 

Thanks for reading!

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 10 years ago in reply to shabaz +2
    9600 baud? No, that doesn't seem it.. 1200 baud? Hmm, not there yet! 2400 baud? Hello data! Looks like the pin-out is correct after all. <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>22</sec…
  • mcb1
    mcb1 over 10 years ago in reply to shabaz +1
    I looked at it a while back, and after multiple revisions it seemed an odd design choice to still use an ATmega and its single built-in 10-bit ADC I didn't look too hard into the actual hardware side,…
  • shabaz
    shabaz over 10 years ago in reply to mcb1 +1
    Agree, it is easy to become OCD and want super-high granularity when in reality you might actually only be interested at the power-hungry stuff.
Parents
  • shabaz
    shabaz over 10 years ago

    Hi Christopher,

     

    Interesting project. If the unit autonomously dumps data every second, then perhaps just the TX output from the unit is needed, and not the RX, so if you had a USB-UART adapter then you could probe with the USB-UART-RX input line only, until you saw data on the terminal window.

     

    According to that link however it sounds like pin 8 is the one that will be outputting from the unit.

    I think this arrangement might work, but I'm not sure since I'm just basing it on that thread : ( :

    image

    Not that I like recommending FTDI parts : ) but it might be quickest to use that one since it is designed for 3.3V logic levels.  I'm designing a USB UART mini project here 5V UARTs on SBCs?   , maybe you might want to swap some day : )

    [EDIT: oh, just noticed you already have a USB UART. That is fine since it is 3.3V too.].

     

    Regarding software, there are a few challenges, firstly (regardless of programming language) the input needs to be read, but to also know when the entire information has been captured. One method is to set a timeout so if you have no more bytes to read for a certain amount of time then the read function exits and you can start parsing the data. If you're using C then this should be straightforward, there is the 'termios' option value VTIME that can be set appropriately (e.g. to 5 tenths of a second), and probably other languages offer the same thing since their libraries use the same underlying capabilities.

    As an example, there is some code here https://github.com/shabaz123/u1282a_fastlog/blob/master/fastlog.c   , it basically reads from a USB UART too and line 321 of the code is setting to 5 tenths of a second.

    Python will have the same thing I'm sure. There is also the 'expect' library (i.e. libexpect) but that feels like overkill.

    The next challenge is to parse the content, which really depends on how regular the structure is. I quite like just using the standard C++ string library for that, although some would say that is like bringing a knife to a gunfight. But equally there are libraries specifically to parse XML but that might be overkill since there isn't much to be parsed by the looks of it. So perhaps usual string find functions are ok to use, and (say) sscanf for reading in the values into floating point variables.

    Regarding what to do with the data, you could push to a cloud (I don't have any recommendation however) say every 5 minutes or (or simultaneously) plot it in real-time to the display. There is an example here, which uses 'kst': Raspberry Pi 3 Dynamic Current Consumption, Power and Temperature Tests

    To do that, I just got the program to dump data regularly to a file, and then 'kst' would read it every second. Maybe there is no need to worry about file size for about a month, and then possibly save it off (e.g. give it a filename with a timestamp). Or put it into a database, but the basic CSV file method isn't bad, easier too. It would be nice to have some analysis as part of the app though, e.g. the stats for the month, and the same month the previous year, etc. However that is all accoutrements, i.e. phase 2 type stuff maybe.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 10 years ago in reply to shabaz

    9600 baud?

    image

     

    No, that doesn't seem it..

     

    1200 baud?

    image

     

    Hmm, not there yet!

     

    2400 baud?

    image

     

    Hello data! Looks like the pin-out is correct after all.

     

     

    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>22</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00651</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>28</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>34</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>41</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00646</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>47</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>53</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>59</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>05</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00590</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>17</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00592</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>23</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00597</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>29</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>35</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>41</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00622</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>47</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00581</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>53</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>59</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>05</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00601</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00642</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00630</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00590</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>48</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>54</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00625</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00604</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00646</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00578</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>47</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00584</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00592</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00587</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00578</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00583</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00596</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>48</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>54</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00610</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00600</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00614</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00648</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>48</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00583</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>54</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00636</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00602</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00648</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>43</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00651</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>49</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>55</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00605</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>01</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00596</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>07</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>19</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00584</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>31</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00584</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>37</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00583</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>43</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>49</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>55</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>01</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00602</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>07</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00622</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00615</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>19</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00635</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>31</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>44</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>02</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00599</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00667</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>32</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00650</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>37</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>44</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>56</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00640</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00634</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00710</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00619</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>31</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>37</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00592</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>43</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00604</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>49</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>55</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00624</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>07</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>14</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00598</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00609</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>26</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00620</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>32</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00625</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>44</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00590</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00604</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>56</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00609</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00608</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>14</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00595</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00607</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>27</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00613</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>33</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00616</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>45</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00630</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>51</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>57</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00606</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>02</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>14</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00595</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>26</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>32</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00579</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00581</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>45</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00579</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00606</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>57</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00605</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>

     

    It dumps data every 5 seconds by the look of it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to cstanton

    Oh Awesome!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 10 years ago in reply to cstanton

    Oh Awesome!!