• Tlaloque 1 bot explores ancient ruins

    Named after the Aztec rain god this robot isn’t really a robot per-se, but rather a one foot wide, 20 inches long and 8 inches high RC vehicle. Designed by engineer Hugo Armando Guerra Calva who graduated from the National Polytechnic Institute, the robot…
  • Wire & Cable Design

    With wire and cable changing in design almost daily. Do we still see copper as a mode of communication with as many companies trying to go wireless? Second part of the question is, if copper is still viable what style is being designed into the new applications…
  • BERNSTEIN - 637.0281.109 - SENSOR, ADJUSTABLE, C-SLOT - SMC, CABLE

    BERNSTEIN - 637.0281.109 - SENSOR, ADJUSTABLE, C-SLOT - SMC, CABLE The BERNSTEIN range of teachable electronic magnetic sensors combines two programmable switching points and fully integrated electronics in an enclosure that boasts the smallest dimensions…
  • LAPP KABEL - 0027547 - CABLE, HI FLEX, 4CORE, 0.75MM, PER M

    LAPP KABEL - 0027547 - CABLE, HI FLEX, 4CORE, 0.75MM, PER M Application OLFLEX-FD 855 P cables are especially high flexible oil resistant control- and supply cables special for use in power chains, automatic manipulators, in permanently moved machine…
  • World's first elastic electric and data cables

    Roboden and slacked electric cable comparison. (via Diginfo) From the Japanese company, Asahi Kasei Fibers , comes Roboden, the world's first elastic "electric/data/USB" cable. The company manufactures the famous Spandex material; it is only fitting that…
  • Wire and Cable Basics

    Basic installation of wire & cable can have a major impact on how long the cables will last. If you are installing cables on a welding robot, in a tray or cable reel, following some basic guidelines will always help. 1) Allow the cable to hang freely…
  • How to make a cable to connect to 0.1" dual-row pins?

    I need to make some 10-pin cables to connect my own sensors to a little circuit board called the U-HID, as seen here: The board has male dual-row headers, and are divided into 10-pin (2 rows of 5 pin) blocks, labeled J1, J2, etc. in the image. So, I want…