Sensors
  • Technologies
  • More
Sensors
Blog Audio-Technica U841A Microphone Teardown
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 23 Sep 2026 11:39 PM Date Created
  • Views 346 views
  • Likes 10 likes
  • Comments 17 comments
  • speech
  • reverse-engineering
  • microphone
  • audio
  • U841A
  • electret
  • condenser
  • conferencing
  • audio-technica
  • teardown
Related
Recommended

Audio-Technica U841A Microphone Teardown

shabaz
shabaz
23 Sep 2026


It’s not everyday I take apart a (reasonably pricey) microphone! But, I was curious, and taking things apart is sometimes how one learns.

A long time ago I took apart an Echo Dot, which contains very different microphone technology (MEMS devices, seven-fold), so check that out too if it's of interest.

Anyway, the U841A is an electret condenser mic, intended for (I believe) speech for audio/videoconferencing purposes. Hopefully any audio experts can provide more detail.


The microphone is very ruggedly built. The secret to opening it up, is to peel off that tiny circular logo on the top; it reveals a screw : ) Then the stamped metal grille lifts off.

image

There’s a lot to visually unpack just from the photo below. On the left, you’ll see three material layers; a thin (0.2 mm) stiff layer (kind of like collar lining! there must be a technical name for it..), followed by 2 mm thick soft acoustic foam, followed by (what feels like) nickel mesh 0.25 mm thick (very slightly magnetic), which is secured to the ground, and must be acting as electrical shielding.

The big green rectangle was originally a mystery, although I suspected it may be a transformer. Everything is superbly constructed.

image

Pulling it apart further (there’s a grub screw which holds the mini XLR connector in place, and it needs to be desoldered to remove the PCB. You can see the electret element has three wires, which suggests it contains an internal amplifier.

image

Here’s a closeup of the circuit board, with the green tape removed; now it’s clear that was hiding a transformer.

In the photo below, the board area can be split into three portions; the lower-left contains circuitry for filtering off RF interference arriving via the microphone cable, the center houses the transformer for constructing a balanced output, and the lower-right contains the audio amplifier. 

image

I tried reverse-engineering the circuit (without destroying it, hence I’m sure I have some of this wrong – and all of the non-polarized capacitor values are placeholder guesses).

image

I’m not sure what D1 is, it has a DA inscription. With some thought, the black component inscribed DA must be a capacitor. Edit: now measured out-of-circuit, it is a 100 nF capacitor.

D5/6/7 are guesses (they have a 561 inscription (Edit: see comments below, D6/7 are most likely 56V zener diodes), they may be 5.6V Zener diodes (although I was under the impression this mic supported a far higher phantom voltage input, so either I am mistaken about the part, or this mic may be a slightly different variant). Edit: D5 is possibly 5.6V zener. 

I can’t say I really understand what’s going on with the transformer input and please don’t assume I drew the circuit layout correctly. If you have suggestions/corrections, please let me know. I do intend to fire it up and feed in a signal in place of the mic element and take some measurements one day, but finding time is hard. Funnily enough, I've been thinking about constructing a microphone simulator (but for digital mics).

Any help would be appreciated. Thanks for reading!

  • Sign in to reply
Parents
  • jc2048
    jc2048 19 days ago

    Interesting tear-down. The transformer construction is fascinating. Would the core material just be steel, like a mains transformer, or something more exotic?

    I'd say D6 and D7 were 56V zeners. The marking is somewhat different to D5 (if they'd come from the same reel on the pick-and-place machine, you'd think they would be the same).

    It's very likely this microphone will run from a 48V phantom supply.

    Note that, if you try it on a mixer, you may not actually see the full 48V with the mic connected. Inside the mixer, pins 2 and 3 of the XLR are commonly fed via resistors from the 48V (if you have it enabled), so it will sit down from the 48 on load - probably somewhere around the 40V mark with it taking 2mA.

    The DA shape looks wrong for a cap and there's an NXP BSX384-C11 11V zener with DA marking in that style of package. But how that fits with the circuit you've drawn, I've got no idea.

    You've just reminded me that a while back I bought a couple of I2S MEMs microphones to experiment with. Must get and do that now the weather is more amenable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 18 days ago in reply to jc2048

    Hi Jon,

    Looking forward to hearing how it goes with the I2S mics!

    Despite the Pi Pico being able to handle PDM (filtering done in software), I'm slowly coming to the idea than maybe I ought to pick a different microcontroller if I want to experiment more with audio, even though I have managed to get the mics running with the Pico today, the audio sounds good (I am using IM72D128V01XTMA1‎ microphones).

    I had a look for different microcontrollers, and ordered some samples of MCXN236VKLT which is an NXP part, I've never used NXP microcontroller before.. it is more suitable than RP2040, but not as powerful as RP2350, but on the other hand is easier to hand-solder (0.5 mm pitch versus 0.4 mm), and has dedicated hardware for audio instead of PIO. Also, the USB (and the supplied stack is not TinyUSB incidentally) supports Full Speed 480Mbps so for general USB projects it could be better than the Pico.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz 18 days ago in reply to jc2048

    Hi Jon,

    Looking forward to hearing how it goes with the I2S mics!

    Despite the Pi Pico being able to handle PDM (filtering done in software), I'm slowly coming to the idea than maybe I ought to pick a different microcontroller if I want to experiment more with audio, even though I have managed to get the mics running with the Pico today, the audio sounds good (I am using IM72D128V01XTMA1‎ microphones).

    I had a look for different microcontrollers, and ordered some samples of MCXN236VKLT which is an NXP part, I've never used NXP microcontroller before.. it is more suitable than RP2040, but not as powerful as RP2350, but on the other hand is easier to hand-solder (0.5 mm pitch versus 0.4 mm), and has dedicated hardware for audio instead of PIO. Also, the USB (and the supplied stack is not TinyUSB incidentally) supports Full Speed 480Mbps so for general USB projects it could be better than the Pico.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz 18 days ago in reply to shabaz

    There's a very low-cost ($20) development board for the MCXN236. Looks extremely good.

    image

    Even has CAN FD on-board! Plus, it has the really nice MCU-Link on-board, which is a CMSIS-DAP Debug Probe, which works with most ARM Cortex-M microcontrollers (might be tied to the target microcontroller on the board though), works with the usual OpenOCD with (say) GDB, and is quite speedy compared to some other debuggers. This board would be great for audio experiments too.

    image

    I've started creating a custom dev-board (since I want to use the TQFP package, not BGA). I'll bring out all pins to headers.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 17 days ago in reply to shabaz

    It's proceeding to a degree.. not fully thought out yet, but may look something like this, about 80x80mm board (I've not routed any signals, just positioned parts approximately where they could go).

    image

    If anyone wants to look over the circuit to make any suggestions, the schematic is here:

    imagePDF

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 15 days ago in reply to shabaz

    A bit more progress from the weekend (about 70% routed).

    image

    Also, there is a MCXN547VKLT part, which could be a drop-in replacement! It has dual core, more RAM and Flash, a neural processor unit (NPU), a second USB interface, plus Ethernet. For the second USB interface, I've placed test pads. The Eth PHY could connect to the P1MISC header, but would also need one signal from the SPI header, so unfortunately the MISO pin would not be available if Ethernet was used. Anyway, it's just a test board, to try out the IC(s), the MISO won't even be needed if that SPI is only used for a display, and MCXN547VKLT is just a stretch goal, so I'm not too concerned about that.

    The supported ICs are:

    MCXN236VKLT: 1MByte Flash, 352k RAM

    MCXN235VKLT: 512kByte Flash, 192k RAM

    MCXN547VKLT:  2MByte Flash, 512kByte RAM, dual USB, 100Mbps Ethernet, NPU