Sensors
  • Technologies
  • More
Sensors
Sensor Forum Is there really a need for battery-based sensors in the home beyond windows and doors?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 342 subscribers
  • Views 49785 views
  • Users 0 members are here
  • sensing
  • home automation
  • sensors
  • battery
Related

Is there really a need for battery-based sensors in the home beyond windows and doors?

user4517
user4517 over 3 years ago

I am in the process of completing a Fuel Oil Tank sensor for my home. I originally worked on code to maximize battery life assuming the need to have a battery, but recently realized I could just implement a USB power converter near the oil tank to feed the sensor. It made me wonder what sensors would require battery support over low voltage direct cable. Here is a list of sensors I believe would not require batteries, and after that list which one's would need batteries. I would enjoy hearing feedback on my list and your perceptions on use of batteries in home sensors.

Don't need batteries:

1 Appliance sensors, including plugs, lights, switches, kitchen appliances, water heater, laundry appliances, HVAC, overall power monitoring and water monitoring.

2. Human location and environmental sensors, including PIM or room movement, environmental (air/gas, temp, level of light, etc.). Also, mmWave sensing for GPS like functionality in the home.

3. Security camaras for outside house where the camaras are mounted on the house (Wi-Fi and POE). In-house camaras that are mounted in the ceiling or in entertainment\computer devices.

Do need batteries:

1. Stand-alone camaras for in-house (Naney cams, or other hidden cameras) Note: many room camera could be connected to existing entertainment or computer devices in a room eliminating the need for batteries

2. External disconnected cameras and environmental sensors (weather stations), and other remote monitoring for security or eventing.

3. Human wearable devices

as you can see the list of Do not need is extensive and the need for most of the do need are limited use, with the only exception being wearable devices.

Let me know what you think.

Pat

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +3
    Hi, This is a good list, but there are circumstances that can cause this to change a bit, especially environment sensors, occupancy sensors and so on, for homes and businesses. Sometimes homes need…
  • dougw
    dougw over 3 years ago +2
    I avoid batteries whenever possible. What does need a battery? flashlight, TV remote, DVM, camera, cell phone, robot, possibly fire alarm.
  • Andrew J
    Andrew J over 3 years ago in reply to dougw +2
    I’m the complete opposite and prefer batteries over trailing cables. Having said that I prefer to not have sensors or such like in the home because I find a switch, my finger and my legs very useful for…
  • robogary
    robogary over 3 years ago in reply to dougw

    AA , AA, rechargeables and 3.7V, 7.4v, 11.1 V Lipos and 9V 

    10 flashlights, digital night binoculars won in an E14 contest, 6 TV remotes, 4 Wii remotes, 2 firestick remotes, 6 clocks, 8 robots,  5 smoke alarms, 4 CO2 alarms, DVMs and NCV detectors, numerous kiddie toys, air mattress pump,  wifi motion sensor in mailbox, Ring, ........yadda yadda yadda 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to shabaz

    No, I know you are pretty much on your own when it comes to licensed radio frequency interference. They are happy to take your money for the license fee but not so keen to enforce the regulations.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to dougw

    I don’t really Doug.  The remote for my tv and CD-R is actually an old iPad so there’s obviously a cable for recharging that.  Smoke alarms are battery driven but they last for years. I’m now struggling to think what I do have thst requires non-rechargeable batteries!!  Ah, my thermostat for central heating requires AA batteries and I probably go through eight a year.  I’m really not into home automation Grinning

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to kmikemoo

    I have to keep a stock of batteries, cables and wall warts because as a techie, wherever "someone" needs something, I am just expected to have whatever they need...Confused

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago

    Enocean makes a whole line of IoT sensors that don't need batteries or wires. They are very low power and use energy scavenging. They sponsored a design challenge on element14 where we got to experiment with them. So to answer your question - mostly you don't need batteries for sensors around the house, not even on windows and doors.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago

    My perspective would be what are the requirements for a battery.

    Battery are either the primary or secondary power source to run the equipment.

    Primary it runs on all the time. Secondary is power when the primary is not available. A third now that I think of it, is constant clean power because I cannot get it from AC mains.

    As shabaz as indicated, each user case has requirements. I can think of a requirements case for a camera needing batteries and I can also think of a use case for not needing a battery

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • user4517
    user4517 over 3 years ago in reply to beacon_dave

    Wow, that is a lot

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • user4517
    user4517 over 3 years ago in reply to beacon_dave

    the usb plugs are a nightmare. I have so many wires with slightly different forms which include differences for even USB 3.x. They need to reduce the usb connecter to just one, the small one. I don't see any value in the older larger one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • user4517
    user4517 over 3 years ago in reply to michaelkellett

    Yea, that crossed my mind too. I did isolate all electronics from access to the tank internals only exposing the two sensor fronts. There is a sealed boundary between the sensor electronics (both PI Pico and sensor circuit board) and the oil tank.

    Low voltage 5v connection might be allowed but I'm finding it difficult to find any answers on that. I'm looking into it right now. Relying on AA batteries just doesn't make it for daily operational use and putting in a lithium ion is dangerous. 

    What you have to do to keep the sensor in deep sleep is more complicated than I expected but I will write code to do it just to learn. If I can deep sleep. If I can get a battery to last a couple of months, I might go with that.

    The electronics and code are common now so the housing was my one innovation which I'll share when it's done. A nice package for under $7 using just PVC type piping components.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • user4517
    user4517 over 3 years ago in reply to robogary

    Well in my use case being down isn't a big deal as I'm measuring changes over days not hours. How much oil do you use per week my be valuable, but I suspect hourly would be below the range error rate.

    Still, I will implement one version that has a battery system with optional charging just to do it. I plan on using the same solution to monitor my sump pump well, but I want to add a GPIO for when the pump turns on and off, for statistics. That will require tapping into the circuit or some coil sensor on the powerline.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<