Test & Tools
  • Technologies
  • More
Test & Tools
Blog Keithley DMM6500 Scanner Card - wiring
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 9 Feb 2023 10:49 PM Date Created
  • Views 2009 views
  • Likes 11 likes
  • Comments 3 comments
  • 88ad1490-a97d-11ed-afa1-0242ac120002
  • 2000-scan
  • dmm6500
  • scan-2000
Related
Recommended

Keithley DMM6500 Scanner Card - wiring

Jan Cumps
Jan Cumps
9 Feb 2023
Keithley DMM6500 Scanner Card - wiring

I road tested the  Keithley Bench Digital Multimeter DMM6500. I recently purchased a 2000-SCAN 10 channel scanner card. This 2nd post shows 2 ways I wired it: for easy use and for least resistance

image

Twisted pair

For my first tests I wired channel 1 and 6 with twisted pairs.

image

I used these channels to do my first tests, because they allow for a few scenarios:

  • 2 x 2 wire voltage, resistance, temperature
  • 4 wire resistance
  • these channels can also measure current if you solder a shunt resistor

image

I'll post my measurement of the first two scenarios later. I have no intention (yet) to place shunts on channel 1 and/or 6.

Flat flex

A convenient way to get all 10 channels out is with a flat flex. This cable gives access to all 10 in an orderly way. The copper is thinner though, and you can't twist the pairs.

image

I tinned the wires before inserting them, and tried to make the whole thing neat.

image

I reused a little gizmo I made years ago to break out a 2x10 connector to a breadboard:.

image

Resistance, including the connections from the meter to the card, the relays, the flat flex + connector, my gizmo, a breadboard and a patch wire: 1.9 Ohm.
With the pins bridged right at the flat flex connector, it's less than 1 Ohm:

image

Good enough for a lot of measurements.

link to all posts

  • Sign in to reply
Parents
  • genebren
    genebren over 3 years ago

    This looks to be a couple of good solutions to wiring up scanner card.  Well done!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 3 years ago

    This looks to be a couple of good solutions to wiring up scanner card.  Well done!