Test & Tools
  • Technologies
  • More
Test & Tools
Blog MP710086 / MP710087: Lab Bench Power Supply Quick Review!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 18 May 2026 8:35 PM Date Created
  • Views 806 views
  • Likes 10 likes
  • Comments 9 comments
  • power supply
  • mp710086
  • bench psu
  • MP710087
  • psu
  • bench supply
Related
Recommended

MP710086 / MP710087: Lab Bench Power Supply Quick Review!

shabaz
shabaz
18 May 2026

I've desired a decent linear low-noise power supply for ages, and I think I've finally found one at a reasonable price.

image (Image source: Farnell website)

It's actually been around for ages. fmilburn reviewed the 30V 5A 150W model several years ago! I had forgotten about that review, and recently rediscovered it. I went for the 60V 3A 180W model, since that will suit my needs I think.

It's well worth reading Frank's review, and special thanks to both Frank and (+) Gough Lui - element14 Community for figuring out how to interface the instrument to a PC; I'm looking forward to using that feature as well.

I created a brief video review with a mobile phone so the video quality is a bit shaky. First, here's a quick bullet-point review:

Things I Loved

* The compact size (although it's very heavy of course, due to the internal transformer)

* A really simple, easy-to-use user interface! 

* Surprisingly low-noise

* Good behavior when the PSU output is enabled/disabled, and under changing loads

* Very large, easy-to-read display

* Dual interfaces for programming; RS-232 and USB

Things I Liked

* Construction seems solid

* Proper front-panel rocker switch for power

Things that could be Improved

* The charting capability could do with some more work

* Ethernet interface option would be useful

* The font could be cleaned up, seems weird to have 7-segment-style characters on a dot-matrix TFT.

* Price is admittedly quite fair, but it would be nice to see a discount, and perhaps a saving for a bundle of two PSUs

Video


You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Thanks for reading / watching!

  • Sign in to reply

Top Comments

  • shabaz
    shabaz 5 months ago in reply to kk99 +1
    Zero or low audible noise is definitely a good thing : ) Interestingly I'd seen some reports that the Owon badge version of this MP71008x PSU made a lot of noise, but the fan noise seemed reasonable…
Parents
  • kk99
    kk99 5 months ago

    Nice review. I also thought about Siglent SPD1305X or something used from series HP/Agilent E36xx, but it is worth adding this one to the list.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 5 months ago in reply to kk99

    Those look like great choices too. I too considered the 1305X model, it's more feature-rich, but costs about 30% more here. The display is considerably larger on the Multicomp unit though (3.7 vs 2.8 inch). But the 1305X has Ethernet and USB versus RS-232 and USB. Also annoyingly there isn't a 60V 1305X option (I happen to already have a high-current PSU, so preferred to obtain a 60V model even though max current on this one is 3A).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz 5 months ago in reply to kk99

    Those look like great choices too. I too considered the 1305X model, it's more feature-rich, but costs about 30% more here. The display is considerably larger on the Multicomp unit though (3.7 vs 2.8 inch). But the 1305X has Ethernet and USB versus RS-232 and USB. Also annoyingly there isn't a 60V 1305X option (I happen to already have a high-current PSU, so preferred to obtain a 60V model even though max current on this one is 3A).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • kk99
    kk99 5 months ago in reply to shabaz

    I saw used 1305X model around 176euro, but yes, the drawback is that it does not have 60V. Additionally, I am not sure if it behaves well in the case of power on/off on different loads. I also saw HP E3610A for around 100 euro, but is limited only to 0-8V 0-3A or 0-15V 0-2A and lacks programming etc. The only benefit is that it does not have a fan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 5 months ago in reply to kk99

    Zero or low audible noise is definitely a good thing : )  

    Interestingly I'd seen some reports that the Owon badge version of this MP71008x PSU made a lot of noise, but the fan noise seemed reasonable to me (i,e. as expected, for a linear PSU, and it adjusts depending on the load).

    I also have this crude thing built ages ago, assembled from ready-made modules and Velleman project kits:

    image

    It's quite low-noise, just a couple of tens of mV p-p perhaps. At that ballpark level and at the frequencies involved, the noise rarely becomes a limiting factor, especially since most projects will have some element of filtering and regulation too. I've used it a lot with op-amp experiments, and the dual outputs are useful.

    There is no current limit adjustment (doesn't really need it, since it cannot provide more than a few hundred mA). Anyway, particularly for (say) sub-500mA uses, personally I'd definitely consider a DIY build (hopefully constructed better than this, and maybe with a better regulator, say LT3081 or LT1963? - don't know though!) since then it can be completely silent, and considerably lower-noise than most cheap ready-made power supplies, and to keep it simple, as mentioned, personally I wouldn't miss a current limit in that case; I know that wouldn't suit everyone. I sometimes look to see if there are nice PSU DIY projects online, but most of them overcomplicate things. There are LT1963 boards with large heatsinks pre-assembled on AliExpress, for low-cost, and that seemed appealing to me.

    Photo of the insides:

    image

    The voltage regulators, P1823 kits, are LM317 based:

    image

    Really ugly hole drilling, I didn't have many tools at that time:

    image

    The power entry uses an IEC inlet block. Could have added a filter there:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kk99
    kk99 5 months ago in reply to shabaz

    Nice power supply. Yes, the DIY kit has a good educational aspect. With manually selected components and, let's say, your own project of a PCB, it probably can end with a really nice device. Similarly, with enclosure, where these days we have the possibility to use 3D printers, etc.