Test & Tools
  • Technologies
  • More
Test & Tools
Blog Seeing the Smaller Picture – Magnifiers Shoot-out
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 10 Nov 2021 1:55 PM Date Created
  • Views 8069 views
  • Likes 5 likes
  • Comments 18 comments
  • magnification
  • pcb_inspection
Related
Recommended

Seeing the Smaller Picture – Magnifiers Shoot-out

shabaz
shabaz
10 Nov 2021

Table of Contents

  • Introduction
  • Previous Magnifiers
  • Coil 8277 ATMax
  • Coilcraft Free Magnifier
  • Edmund Optics 35359 10x Magnifier and BelOMO Triplet
  • Donegan OptiVISOR
  • Carson MG-88 MagniGrip 4.5x Magnifier with LED and Tweezers
  • Carson 2.5X CrystalView Aspheric Magnifier with 5x Spot Lens
  • Carson Lume Series COB LED 2.5X Magnifier with 7x Spot Lens
  • Carson 5x 2.5" Aspheric Magnifier SV-50
  • Other Recommendations
  • Summary

 

Introduction

Since none of us are getting younger, we eventually need to consider how to see small parts in the electronics engineering world. There are thousands of options, including handheld magnifiers, microscopes and video cameras. Even a mobile phone can be effective to view things close-up.

 

Over the years, I've tried quite a few magnifiers, ranging from a cost of free to perhaps $100, and the main use-cases have been to be able to read surface-mount component part numbers, inspecting solder joins looking for shorts, and for aiding me to solder small parts with an iron. For this blog post, I won't cover the previous magnifiers again, but I will look at some additional ones I've tried in the past few years.

 

From the previous magnifiers, the most outstanding one was made by UltraOptix. It has lasted more than 5 years, survived a couple of battery leaks, and the image quality and the LED light quality is good. Furthermore, it's really low-cost (under $10). The only disadvantage is availability; it is cheap and easily available in the US, but in the UK it is a bit harder to obtain, there are just a few sellers on Amazon, and they charge more.

 

This shoot-out covers:

  • Coil 8277 ATmax
  • Coilcraft Freebie
  • Edmund Optics 35359 10x Magnifier
  • BelOMO 10x Triplet
  • Donegan OptiVISOR DA-4 2x Head Mount MagnifierDonegan OptiVISOR DA-4 2x Head Mount Magnifier
  • Carson MG-88 MagniGrip 4.5x Magnifier with Tweezers
  • Carson CrystalView 2.5x Aspheric Magnifier with 5x Spot Lens
  • Carson Lume Series COB LED 2.5x Aspheric Magnifier with 7x Spot Lens
  • Carson 5x 2.5" Lighted Aspheric Magnifier SV-50

 

From the magnifiers examined here, the best ones were the OptiVISOR, and the Carson 2.5X handheld magnifiers (CrystalView and Lume), which come in illuminated and non-illuminated options.

 

There is a 15-minute video that attempts to show what it is like looking through each magnifier.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Previous Magnifiers

From an earlier blog post Building a Digital PCB Inspection Microscope with the Gizmo 2 , the photo here shows UltraOptix 7x Aspheric 1.5 inch LED Lighted Magnifier along with others not really worth mentioning. The UltraOptix is very good for examining part markings, and it is very low-cost.

image

 

Coil 8277 ATMax

This magnifier was quite expensive, and performed poorly from my perspective. This is a 7X magnifier made from a biconvex lens, with a touch-sensitive built-in LED light, and contains two AA batteries. It comes with a storage bag.

image

 

The magnification is quite high (7X) which in part makes it harder to accurately position, although the far cheaper UltraOptix magnifier (with better aspheric lens rather than biconvex) managed just fine. With the ATmax magnifier, everything is heavily distorted, and there's plenty of colour fringing anywhere off-center too. There are also lots of reflections off room lighting. Also, I have encountered situations where the touch-sensitive light would stay on even though the magnifier was placed on a desk, so it's not completely reliable. The only positives are that the device is constructed nicely and its very ergonomic with the rubbery grip.

 

The photo below shows it centered on a SOT-23 component. Everything else is distorted.

image

 

Coilcraft Free Magnifier

Buying a Coilcraft inductor kit results in receiving a free magnifier inside the box : ) It's actually not bad, I have several of these now, and they are quick to use with their plastic stand. They are good enough to read part markings. This style of foldaway magnifier is usually known as a Linen Tester or Linen Magnifier.

image

 

Edmund Optics 35359 10x Magnifier and BelOMO Triplet

A loupe can be quite handy to read part markings. They are intended to be used with the eye close-up, and this particular one would only be of use if you can get your head close to the object to be inspected. Despite being close to the object, the eye still focuses at a distance, and therefore there is no eye strain.

image

 

The image quality with the Edmund Optics magnifier is great with no distortion (see the photo below, but when actually using it, it is possible to position it so that the entire board is clear without the white blur visible in the photo), however the room needs to be well-lit, otherwise the loupe and your head will block out light. I think an illuminated loupe would be a better idea.

image

 

The earlier photo also another loupe, called BelOMO Triplet, which is a bit too small I feel. I keep it on a neck-strap, but I don't use it often, it suffers from the same issue that good lighting is needed.

 

Donegan OptiVISOR

The OptiVISOR OptiVISOR is one of my favorite magnifiers – it's simply brilliant. This head-mounted magnifier can be worn for hours without tiredness. It can be easily swung up when normal vision is needed. I like positioning it such that I can look down and have normal vision, or raise eyes to look through the lenses; that way, I don't need to frequently swing the lenses up and down.

 

This magnifier can be used for soldering. Objects are in focus approximately 6 inches away from the end of the magnifier, and so although you'll need to bring your head in while soldering, it's not uncomfortable.

 

Different strength lenses can be fitted. Mine came with number 4 lenses, they seem fine.

image

 

This magnifier could single-handedly make the difference between being able to do surface-mount work, and not being able to do it, if you're no longer blessed with perfect vision.

 

The photo below was taken with the OptiVisor placed in front of the camera; the field of view when actually wearing it is just slightly more than the width of a Raspberry Pi.

image

 

Carson MG-88 MagniGrip 4.5x Magnifier with LED and Tweezers

These tweezers have an LED attached to one arm of tweezers, and a combined watch battery compartment and twist switch at the back of the device. The magnifier is on a long arm hinged at the joint. 

 

I really wanted to like this product, but despite the magnifier itself being semi-reasonable, the other parts of it were a let-down; the tweezers are not really intended for precise work with electronics, this is not their target market. The tweezers are hard to squeeze and are not made with the accuracy needed for electronics. I don't think they could be improved with a bit of DIY either; the entire tweezers would need replacing. The length is too short too – I expect tweezers to be about 120 mm long, but these ones are barely 100 mm long, and the battery section falls into the palm on the hand. I don't know how long the three L926F watch batteries would last.

image

 

Carson 2.5X CrystalView Aspheric Magnifier with 5x Spot Lens

This magnifier is physically large, does its job, and is low-cost (about £10) – it's excellent. It comes with a sock to protect the lens portion.

image

 

The lens is plastic and aspheric. The image quality is great, with no noticeable distortion when using it. It can be placed about 5 inches away from the circuit board, and so it is feasible to solder using this magnifier, provided it can be clamped in position. I used a DIY clamp: Building Custom Helping Hands

image

 

Carson Lume Series COB LED 2.5X Magnifier with 7x Spot Lens

This magnifier has thee diffused LEDs spaced around the edges, and the power switch provides two brightness settings. It takes two AAA batteries.

image

 

The image quality from the plastic aspheric lens is very good. It is possible to perform soldering work with this magnifier provided it can be clamped into position.

 

I also liked the smaller 7X lens next to the power switch, it is useful if extra magnification is briefly needed to read part markings. The LED lighting is effective for that too, since the light arrives at a shallow angle, which works well with etched markings to provide good contrast.

image

 

Carson 5x 2.5" Aspheric Magnifier SV-50

This magnifier is quite a decent size, with an approx. 50 mm diameter lens. It's aspheric, so the image quality is decent, but it's not to the same standard as the image quality from the larger diameter 3x magnifiers mentioned above (Carson Lume and Carson CrystalView). The image has some distortion in the outer 30% or so of the image, but it's not anywhere near as bad as the Coil 8277. It's very usable. 

image

The LED illumination is quite a nasty cold white, but it gets the job done.

image

There is some glare from the LED, but it's not too bad.

image image

Inside, three AAA batteries are required (not supplied) and they should last a very long time since there's only one LED to light up. From experience with the physically smaller 7x version of this product, I can confirm that the slide switch will last for many years in normal use. 

image

Overall, it's not a bad product, it gets harder to find decent 5x magnifiers at good prices, and this one is for sure usable.It doesn't come with a protective pouch, but the lens won't hit the desk easily, because it is protected by the deep plastic rim.

Other Recommendations

If you have any favorite magnifiers, it would be great to learn about them, since there may be excellent ones that I don't know about. It would be very useful information - saves people spending on poor-performing magnifiers!

image

 

Summary

The table here shows my conclusions. Thanks for reading!

 

Magnifier Name Conclusion Cost (GBP or USD)
UltraOptix 7x Aspheric 1.5 inch LED Lighted Magnifier Excellent image quality, good built-in LED light, extremely low cost $9.95
Coil 8277 ATmax Awful image quality with heavy distortion and color fringing. Comes with a zip-up cover. £55
Coilcraft Freebie Very usable for reading part markings $0 with any inductor kit (or maybe ask them nicely?)
Edmund Optics 35359 10x Magnifier Excellent image quality, but needs good lighting because your head will block the light £25
BelOMO 10x Triplet Excellent image quality, but same issue as the Edmund Optics magnifier £35
Donegan OptiVISOR DA-4 2x Head Mount Magnifier Excellent image quality, and ideal for soldering surface-mount components $43
Carson MG-88 MagniGrip 4.5x Magnifier with Tweezers Great image quality, but poor tweezers for engineering purposes (fine for beauty work I expect!) £12
Carson CrystalView 2.5x Aspheric Magnifier with 5x Spot Lens Excellent image quality, and good depth for soldering, provided it can be clamped in position. Comes with a sock/cover. £10
Carson Lume Series COB LED 2.5x Aspheric Magnifier with 7x Spot Lens Excellent, as good as the Carson CrystalView, but has really great LED lighting too (with two brightness levels). Doesn't come with a cover. £15
Carson 5x 2.5" Aspheric Magnifier SV-50 Good image quality, but could be better. Large 50mm diameter lens. Has an LED light that should last a long time.  £15
  • Sign in to reply

Top Comments

  • genebren
    genebren over 4 years ago +1
    Excellent comparison of magnifiers. I too have quite a collection of handheld magnifiers, but most them are less than useful. My go to magnifier, for taking a quick peak at electronics is the TRIPLET 10x…
  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago +1
    My favourite magnifiers (besides the Mantis microscope at work) at clip-on lenses on my glasses. I saw at jeweler wearing them at our local farmers market. They only do about 2.5x but that is sufficient…
  • beacon_dave
    beacon_dave over 4 years ago +1
    I have been after a new magnifier for a while and after reading this, I got hold of the Carson CrystalView 2.5x magnifier. First impressions are that its main 2.5x lens is quite impressive for the money…
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    I have been after a new magnifier for a while and after reading this, I got hold of the Carson CrystalView 2.5x magnifier. First impressions are that its main 2.5x lens is quite impressive for the money. 

    As for other magnifiers, I use a Visible Dust  'Sensor loupe 7x' which is an older version of the 'Quaser Sensor Loupe 7x' as shown here: 

       visibledust.com/technology.php

      I find the loupe a lot easier to use than the 5x spot feature of the Carson though e.g. when looking at the likes of 'small print' on ICs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 4 years ago

    I have been after a new magnifier for a while and after reading this, I got hold of the Carson CrystalView 2.5x magnifier. First impressions are that its main 2.5x lens is quite impressive for the money. 

    As for other magnifiers, I use a Visible Dust  'Sensor loupe 7x' which is an older version of the 'Quaser Sensor Loupe 7x' as shown here: 

       visibledust.com/technology.php

      I find the loupe a lot easier to use than the 5x spot feature of the Carson though e.g. when looking at the likes of 'small print' on ICs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave over 4 years ago in reply to beacon_dave

    ok, so that link didn't work... and I can't edit...
    https://visibledust.com/products/quasar-plus-sensor-loupe-7x-magnifier-improved-focusing-system/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to beacon_dave

    Hi Dave,

    I'm not receiving notifications on comments on this blog for some reason : (

    Very interesting loupe : ) The built-in LEDs would solve my problem using loupes, in that a lot of ambient light gets blocked.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to shabaz

    Hi Shabaz,

    Experiencing similar with the notifications here.

    Getting good illumination onto the subject is often an issue. In general the lighting on loupes could be greatly improved if there was more user control available.

    This loupe though was marketed at cleaning DSLR camera sensors, so it can still focus when positioned around 30-35mm above the subject, e.g. when the loupe is placed flat on the lens mounting ring of the camera observing the surface of the imager chip located behind the lifted reflex mirror down below.

    This also means if your work area has good lighting either side of the subject being viewed, then you don't always need the built-in LED lighting as you aren't blocking the ambient light. It's different for the camera situation as there you are looking into a dark hole and you need to rely on the built-in lighting.