Test & Tools
  • Technologies
  • More
Test & Tools
Blog The Modular Bench Power Supply ++, testing it all on the bench with the BreadBoard
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Robert Peter Oakes
  • Date Created: 28 May 2015 4:56 AM Date Created
  • Views 3197 views
  • Likes 5 likes
  • Comments 5 comments
  • tutorial
  • bench
  • meter
  • supply
  • load
  • dc
  • power
Related
Recommended

The Modular Bench Power Supply ++, testing it all on the bench with the BreadBoard

Robert Peter Oakes
Robert Peter Oakes
28 May 2015

Back to the Main post The Modular Bench Power Supply ++, The Essential DIY Build for Every EE Student and Old Timer alike...

 

Ok, so based on the last two or three videos an posts it is time to test everything out on the bench with a breadboard and read power to see how it performs

 

so this is the final schematic I have, I still am pondering changing it up a bit more but I will play with it a little first, ideas I have are around using 10V control signals instead of 5V and of course adding a pre-regulator switching in order to reduce heat dissipation in the regulator significantly, but thats for a future epesode image

image

RPO: The Schematic was updated to reflect the correct volts on the op amps of +12 and -12

 

and of course the video to explain it all

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to nikolajbrinch +1
    yes, the op amps are running on their own 12V +- supply, 9 volts would also work ok. there are many techniques you can use to derive the supply for the op amps but it does need to be isolated from raw…
Parents
  • paulv
    paulv over 11 years ago

    Hi Peter,

     

    I also left this msg on your blog.

    There is a small error on the diagram.

    The +12V is labeled +2V.

    You may want to clean-up the connections to the feedback resistor of the voltage comparator.

    Your schematic capturing probably messed that up.

     

    Looking forward to the next episode, I'm glued to the Tube.

     

    Paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • paulv
    paulv over 11 years ago

    Hi Peter,

     

    I also left this msg on your blog.

    There is a small error on the diagram.

    The +12V is labeled +2V.

    You may want to clean-up the connections to the feedback resistor of the voltage comparator.

    Your schematic capturing probably messed that up.

     

    Looking forward to the next episode, I'm glued to the Tube.

     

    Paul