Test & Tools
  • Technologies
  • More
Test & Tools
Forum Diode identification and car radio repair
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 387 subscribers
  • Views 6761 views
  • Users 0 members are here
Related

Diode identification and car radio repair

edumcg
edumcg over 6 years ago

Hello,

 

 

I'm trying to repair my nissan car radio model: Clarion BTS33

 

 

The problem began when the fuel volumen line of my car shortcircuited with 12V.  As soon as that happened my radio turned off and never came back again. I sent the radio with some folks to repair it, they replaced some ICs that were burned out but they couldn't replace one specific diode.

 

 

Right now, when I plug the radio into my car only the screen shows up but it prints nothing. Just a blank orange screen. No audio output no matter what buttons I press.

 

 

I found the cable on Amazon: https://www.amazon.com/20-pin-Subaru-Headunit-Harness-Steering/dp/B01D9K3L44

 

 

I also found the user manual of the radio: https://fccid.io/2ABGYBTS33-CLARION/User-Manual/User-guide-2150158

 

 

The only component that looks burned out is the diode D402. The diode is the same as de diode D403 so I can see the marking is "C308" the 08 is fllipped to the right 90 degress.

 

 

My plan is to replace the diode but I haven't been able to find a datasheet.

 

 

I've attached images of the radio and the circuit board. Any help would be appreciated.

 

 

Thanks!

Attachments:
image
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 6 years ago in reply to MDeGrauw +3
    Well now, would you lookie there. Thanks MdG & JC, I learned something. SOT-23 packaging never existed before my absenteeism from electronics. I noticed the more bright members ignored my comments and…
  • fiddler_in_the_lab
    fiddler_in_the_lab over 6 years ago +2
    I would not have to high hopes that replacing that diode will fix the problem.... but as it is an easy thing to do if you (or a friend) have a multimeter and basic soldering skills. So it sure is worth…
  • msbettyhunt
    msbettyhunt over 6 years ago in reply to fiddler_in_the_lab +2
    It is a good idea of replacing the diode with the general purpose diode. Hope it will work.
Parents
  • colporteur
    colporteur over 6 years ago

    image

    I don't wish to rain on your repair parade but, I question the suggestion the component D402 (A) is a diode. Diodes typically have two leads and not three leads as D402 has. D401 (B) could be a diode and ZD402 (B) could be a zenor diode (guessing because of the prefix Z). This two component have two leads. D304 & D303 (C) are diodes according to the symbol. Component D305 (D) might be a diode. It is fairly large and just two leads.

     

    There are transistors, I suspect the components prefixed with a Q,  that typically have three leads. D402 having three leads causes me to question if in fact the components is a diode. Maybe someone with SMD experience can chime in on the call.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to colporteur
    SMD CodePackageDevice Name
    C3SOT‑231SS226
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to colporteur
    SMD CodePackageDevice Name
    C3SOT‑231SS226