Test & Tools
  • Technologies
  • More
Test & Tools
Forum Ti LDC1000EVM A Question on Inductance
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 24 replies
  • Answers 2 answers
  • Subscribers 386 subscribers
  • Views 7615 views
  • Users 0 members are here
  • ldc1000evm
  • inductors
Related

Ti LDC1000EVM A Question on Inductance

jw0752
jw0752 over 11 years ago

Inspired by shabaz I purchased a TI  LDC1000EVMLDC1000EVM Evaluation Kit and set it up If you want more information on the kit itself check out Shabaz's blog as it is very interesting Getting Started with the LDC1000 - Small Metal Detection!

 

After setting up the board I wanted to confirm some of the things I thought I understood about inductors and so I performed a couple of experiments and my results leave me with a question that I am hoping you can help me with.

 

My first experiment was to look at the inductor in free air.

 

image

 

The GUI for the Evaluation board was reading 19.496 uH with an open air core.

 

image

 

For my next experiment I inserted a small ferrite core into the inductor.

 

image

 

My expectation was that this ferrite core would increase the inductance of the coil. I was not disappointed as the inductance rose to 30 uH.

 

image

 

My next experiment was to replace the ferrite core with a soft steel rod of similar length to the ferrite one.

 

image

 

To my surprise and confusion the inductance of the coil dropped to 16.811 uH which was almost 3 uH lower than open air. I am hoping that someone can explain this behavior to me. I did not expect the steel core to do as well as the ferrite but I did expect it to do better than open air.

 

image

 

I have my physics book open right now and I am reviewing inductors to see if I can better understand why a steel core would lower the inductance of a coil instead of raising it.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago in reply to jw0752 +3
    I snapped off that resonant circuit and applied it to the VNA, this is the result I get (it could be inaccurate, the VNA is freshly built and could have issues. I'm still learning how to use it). I've…
  • DAB
    DAB over 11 years ago +2
    Hi John, After reading your post I remembered something I wrote in my book about how the crystalline structure of iron behaves under a magnetic field. The ferrite core is a very homogeneous material, so…
  • shabaz
    shabaz over 11 years ago +2 verified
    Hi John and Everyone, Chris Oberhauser from TI replied : At the higher frequencies (>500kHz) that LDC devices typically operate, the eddy currents on the target surface overwhelm the permeability and…
  • michaelkellett
    0 michaelkellett over 11 years ago

    I suspect that the problem is that the steel core is much more lossy than the ferrite at the operating frequency of the chip, or possibly that the inductance has increased too much and is out of range.

    What happens if the steel slug is  close to the coil but not inside it ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago

    Hi John,

     

    Very interesting results!

    It is impressive that the LDC1000 circuit can reveal so much detail about inductance and the effect of cores. However, interpreting this is hard I think.. : (

    I also think the same, the steel has caused the inductor to become lossy, i.e. it now has significant resistance at operating frequency. According to the LDC1000 datasheet, it computes inductance by observing resonant frequency. With the lossy inductor, a higher current is needed to maintain a particular amplitude oscillation, and this can be observed by calculating Rp which is the parallel resistance of the resonant circuit.

     

    There is a formula on page 12 of the datasheet which shows how to see the Rp value, I put that formula in Excel, and this was the output (x-axis is sample number, y-axis is calculated Rp in kohms) -

    the value dropped from 11kohms to just over 7kohms.

    image

     

    The graph above initially shows nothing close to the coil. As the steel was brought close to the coil, the Rp dropped. I then removed it, hence the graph went back up to 11kohms.

     

    The graph below shows the result with ferrite, where the only relevant bits are at the beginning and at the end of the graph.

    At the beginning, there was nothing near the core. At the middle, I was busy securing it to the coil using tape. The end of the graph shows the actual

    result, and it is at a higher value (about 12kohms) than at the beginning (11kohms). I only used a tiny piece of ferrite (ferrite type 61 - there are various mixes of ferrite possible).

    image

     

    Another way we could dig deeper is by subjecting that coil to a vector network analyzer (VNA), which would basically show us the equivalent circuit of the inductor with the steel or ferrite. I do have a (home-made) VNA but it needs calibration (and some practice) to be useful, and I still need to do that : (

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to michaelkellett

    Hi Michael,

    Thank you for your reply. As the steel core is brought closer to the coil it gradually shows a drop from approx 20 uH to the approx 17 uH. Your idea that the steel core is introducing core losses into the setup is probably the source of the problem. With its granular nature the ferrite would not be as susceptible as the solid piece of steel to eddy currents. I will do some more experiments as, for me, this exercise is about learning about inductance and how this circuit works more than any real application for it. Thanks again for your insight.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to shabaz

    Hi Shabaz,

    Thanks for the quick reply and nice analysis of my question. I can see that your graphs show the same phenomenon that I was observing and confirm the suspicions of michaelkellett I have to confess that last night in my eagerness to play with the new toy I did not read the Data Sheet which is on the schedule for today before I ask anymore questions I also have a 14 page article on inductors that I want to review Thanks again for introducing the  LDC1000EVMLDC1000EVM in your blog

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to jw0752

    Hi John,

     

    The datasheet, while good, could maybe do with more detail on examples and their explanation (like you're trying to do). Still, the datasheet is pretty good - I'm being over-critical.

    Most of the analysis in my comment is still vague guesswork to be honest, since I'm assuming that the change in Rp has had sufficient effect to however the LDC1000 internally measures the inductance (and Rp has 16-bit resolution), but now I think of it, perhaps the

    change in Rp, and the change in drive to maintain oscillation level may affect the resonant frequency, e.g. the parallel capacitance may change slightly. Often this can be seen by a LC oscillator when the voltage is varied - the

    frequency does shift slightly (but this is a guess. I don't think that bit alone is enough to explain 20uH -> 17uH).

    A good book is "RF Circuit Design" by Bowick, by the way.. it has a good (although brief - the entire book is short, but easy-to-read) section on inductors and resonant circuits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to shabaz

    Hi Shabaz,

    Thanks for the book recommendation. I have ordered a good used one through Amazon. As is the case with most questions involving multiple variables it is difficult to get an exact answer but rather we approach the answer slowly by degrees as we learn and understand the system better.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 11 years ago in reply to shabaz

    Hey thanks! A good reason to re-polish my passives theory. Gone are the days when I could do the calculations (and pass the exam image ) myself.

    I'll be looking for some reference to revamp the theory and the brain.

     

    On a side note - but related: I did the online Georgia Institute of Technology's "Linear Circuit" training on Coursera last year. A great refresher.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 11 years ago

    Hi John,

     

    After reading your post I remembered something I wrote in my book about how the crystalline structure of iron behaves under a magnetic field.

     

    The ferrite core is a very homogeneous material, so all of the induced currents will flow in the same direction and initiate an induced magnetic field, which is why the measured inductance goes up.

     

    In steel, you have iron mixed with other metals, forming irregular crystals.  When you apply the magnetic field, you get interactions at various angles depending upon how the crystals are aligned inside the steel core.

     

    The various induced magnetic fields will interact, creating an impure conductance path, hence the drop in apparent inductance.

     

    Your experiment does a good job of showing how important the alignment of the material and crystal patterns can really affect magnetic fields.

     

    Nice job.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to DAB

    Hi DAB,

    Thanks for your insights on the Physics behind the scenes. I have been digging through the old college physics book today to refresh my understanding of inductors.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelwylie
    0 michaelwylie over 11 years ago

    John;

     

    Any chance that it's stainless steel?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>