Test & Tools
  • Technologies
  • More
Test & Tools
Forum Ti LDC1000EVM A Question on Inductance
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 24 replies
  • Answers 2 answers
  • Subscribers 386 subscribers
  • Views 7631 views
  • Users 0 members are here
  • ldc1000evm
  • inductors
Related

Ti LDC1000EVM A Question on Inductance

jw0752
jw0752 over 11 years ago

Inspired by shabaz I purchased a TI  LDC1000EVMLDC1000EVM Evaluation Kit and set it up If you want more information on the kit itself check out Shabaz's blog as it is very interesting Getting Started with the LDC1000 - Small Metal Detection!

 

After setting up the board I wanted to confirm some of the things I thought I understood about inductors and so I performed a couple of experiments and my results leave me with a question that I am hoping you can help me with.

 

My first experiment was to look at the inductor in free air.

 

image

 

The GUI for the Evaluation board was reading 19.496 uH with an open air core.

 

image

 

For my next experiment I inserted a small ferrite core into the inductor.

 

image

 

My expectation was that this ferrite core would increase the inductance of the coil. I was not disappointed as the inductance rose to 30 uH.

 

image

 

My next experiment was to replace the ferrite core with a soft steel rod of similar length to the ferrite one.

 

image

 

To my surprise and confusion the inductance of the coil dropped to 16.811 uH which was almost 3 uH lower than open air. I am hoping that someone can explain this behavior to me. I did not expect the steel core to do as well as the ferrite but I did expect it to do better than open air.

 

image

 

I have my physics book open right now and I am reviewing inductors to see if I can better understand why a steel core would lower the inductance of a coil instead of raising it.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago in reply to jw0752 +3
    I snapped off that resonant circuit and applied it to the VNA, this is the result I get (it could be inaccurate, the VNA is freshly built and could have issues. I'm still learning how to use it). I've…
  • DAB
    DAB over 11 years ago +2
    Hi John, After reading your post I remembered something I wrote in my book about how the crystalline structure of iron behaves under a magnetic field. The ferrite core is a very homogeneous material, so…
  • shabaz
    shabaz over 11 years ago +2 verified
    Hi John and Everyone, Chris Oberhauser from TI replied : At the higher frequencies (>500kHz) that LDC devices typically operate, the eddy currents on the target surface overwhelm the permeability and…
Parents
  • shabaz
    0 shabaz over 11 years ago

    Hi John and Everyone,

     

    Chris Oberhauser from TI replied:

     

    At the higher frequencies (>500kHz) that LDC devices typically operate, the eddy currents on the target surface overwhelm the permeability and hence the inductance drops. If you change the sensor to one that operates at a much lower frequency (~40kHz), then you will see an increase in inductance when the steel is brought into the field. There is a transition region where you will see a minimal change in inductance due to a steel target position; this frequency range will vary based on the type of steel.

     

    The Rp measurement will still show a shift due to target presence.

     

    So, our initial hypothesis that inductance ought to go up was true, but only at lower frequencies in the case of steel. According to Chris, at higher frequencies the presence of steel causes sufficient eddy currents that will have a greater effect than permeability.

     

    The eddy currents cause a magnetic field which opposes the field from the inductor, and this reduction in flux density results in a reduced inductive reactance.

    Hence we see the resonant frequency of the LC circuit to go up.

     

    Some sources (such as this onehttp://https//www.nde-ed.org/EducationResources/CommunityCollege/EddyCurrents/Instrumentation/impedanceplane.htm) state that for steel, permeability has a greater effect than eddy currents, but I guess that the information on those sites is presuming a lower frequency measurement which is not the case for us.

     

    There is a great 'Eddy Current Applications' document here (PDF).

    (Perhaps the book is aimed specifically at eddy current testing at frequencies relevant to industry convention for aeronautics).

     

    Figure 8-47 shows some graphs at a fixed frequency, where they have a coil, and they show on the X and Y axis the impedance (resistance on x-axis, inductive reactance on y-axis) when the coil is in free air (marked the 'Air Point'), and when a material is brought closer to it.

    The arrow shows the path the impedance takes (all the time at that fixed frequency) as item is brought closer.

    Diagram (c) in that figure is the scenario for ferrite, which is as we expect (bringing ferrite closer will increase the inductance).

    Diagram (b) is what we thought should occur with steel, and apparently it does at lower frequency.

    Diagram (a) is something like copper ( - and from what we're seeing is also the behavior of steel at the higher frequency).

     

    So, your question and experiment appears to have an answer which is inconsistent with some books/resources because they assume a lower frequency for test (perhaps because they are related to particular traditional industry tests/equipment),

    compared to the higher frequency that the LDC1000 is capable of!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago

    Hi John and Everyone,

     

    Chris Oberhauser from TI replied:

     

    At the higher frequencies (>500kHz) that LDC devices typically operate, the eddy currents on the target surface overwhelm the permeability and hence the inductance drops. If you change the sensor to one that operates at a much lower frequency (~40kHz), then you will see an increase in inductance when the steel is brought into the field. There is a transition region where you will see a minimal change in inductance due to a steel target position; this frequency range will vary based on the type of steel.

     

    The Rp measurement will still show a shift due to target presence.

     

    So, our initial hypothesis that inductance ought to go up was true, but only at lower frequencies in the case of steel. According to Chris, at higher frequencies the presence of steel causes sufficient eddy currents that will have a greater effect than permeability.

     

    The eddy currents cause a magnetic field which opposes the field from the inductor, and this reduction in flux density results in a reduced inductive reactance.

    Hence we see the resonant frequency of the LC circuit to go up.

     

    Some sources (such as this onehttp://https//www.nde-ed.org/EducationResources/CommunityCollege/EddyCurrents/Instrumentation/impedanceplane.htm) state that for steel, permeability has a greater effect than eddy currents, but I guess that the information on those sites is presuming a lower frequency measurement which is not the case for us.

     

    There is a great 'Eddy Current Applications' document here (PDF).

    (Perhaps the book is aimed specifically at eddy current testing at frequencies relevant to industry convention for aeronautics).

     

    Figure 8-47 shows some graphs at a fixed frequency, where they have a coil, and they show on the X and Y axis the impedance (resistance on x-axis, inductive reactance on y-axis) when the coil is in free air (marked the 'Air Point'), and when a material is brought closer to it.

    The arrow shows the path the impedance takes (all the time at that fixed frequency) as item is brought closer.

    Diagram (c) in that figure is the scenario for ferrite, which is as we expect (bringing ferrite closer will increase the inductance).

    Diagram (b) is what we thought should occur with steel, and apparently it does at lower frequency.

    Diagram (a) is something like copper ( - and from what we're seeing is also the behavior of steel at the higher frequency).

     

    So, your question and experiment appears to have an answer which is inconsistent with some books/resources because they assume a lower frequency for test (perhaps because they are related to particular traditional industry tests/equipment),

    compared to the higher frequency that the LDC1000 is capable of!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 11 years ago in reply to shabaz

    Hi Shabaz,

    Excellent pursuit and resolution of this mystery. Since I am committed to the consistency of the physics of the universe I knew an explanation existed. Thanks for the effort above and beyond call of duty to get an answer for my question though I suspect your own curiosity had a little to do with it too.

    John