Test & Tools
  • Technologies
  • More
Test & Tools
Forum Hot Air Station suggestions?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 12 answers
  • Subscribers 390 subscribers
  • Views 4962 views
  • Users 0 members are here
  • hot_air_stations
Related

Hot Air Station suggestions?

ajens23
ajens23 over 9 years ago

Hi All,

 

I find myself wanting to do more surface mount work.

While a toaster oven works pretty good for the whole board, I would like to try a hot air station.

After looking at a Weller station at over $700 US, then looking at $50 stations on E-bay,

I would like to hear from some actual users and their experiences and recommendations.

 

So what is a reasonable brand of hot air station that will last for several years and not break the bank.

(I.e. under $200US would be nice.)

 

Thanks,

Al

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +3
    Hi Al, I have the same unit 21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14 that michaelwylie has. When I got it I modified it to include a shut off in the cradle. I was pretty…
  • mcb1
    mcb1 over 8 years ago +3 suggested
    I have the same unit as kas.lewis referred to Tenma 21-10130 21-10130 it has the cutoff feature when you place the handpiece down, and the picture doesn't show it, but includes a temperature controlled…
  • dougw
    dougw over 8 years ago +3
    I use an Aoyue because it was low cost, but it works fine for my needs. I use it for rework (chip removal) and small heat shrink tubing.
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    I have the Weller WXR 3000 workstation that includes  Hot Air rework and it is awesome, but as you say, it is very expensive WXR3003 - WELLER - Rework Station, Multifunctional, 450 °C, 120 V | Newark element14  , you can get the various parts separately and that will be way less money, for instance, just the Hot Air.

    I produced a few videos on it (Sorry but mine was sponsored to me by Weller themselves along with RS-Components, so RS Logos are in the video) but you can also get this from Element 14 using the link above.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    What I think is important to look out for is the following

     

    The FAN for the hot air is in the base, not the pencil, this makes it easier to wield and typically gives better range of Air flow. It is all too easy to simply blow away the part you're trying to re-work if the flow is too high. To go with this you also need a good range of temperature, especially if you also consider Lead Free Solder and big pads that double as heat dissipators.I have also a cheap EBAY Atten/SEIK  that works but is very temperamental with the Fan and will change speed as I rotate the hot air pencil. Now that i have tried the Weller, I see why paying more for good quality German Engineering is worth it.

     

    As a separate note. I have been using the same Weller Iron for close to 40 years and it is still going strong, paid more for it of course but never needed to buy another for all this time. Lets hope the new one will last as long.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    I have the Weller WXR 3000 workstation that includes  Hot Air rework and it is awesome, but as you say, it is very expensive WXR3003 - WELLER - Rework Station, Multifunctional, 450 °C, 120 V | Newark element14  , you can get the various parts separately and that will be way less money, for instance, just the Hot Air.

    I produced a few videos on it (Sorry but mine was sponsored to me by Weller themselves along with RS-Components, so RS Logos are in the video) but you can also get this from Element 14 using the link above.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    What I think is important to look out for is the following

     

    The FAN for the hot air is in the base, not the pencil, this makes it easier to wield and typically gives better range of Air flow. It is all too easy to simply blow away the part you're trying to re-work if the flow is too high. To go with this you also need a good range of temperature, especially if you also consider Lead Free Solder and big pads that double as heat dissipators.I have also a cheap EBAY Atten/SEIK  that works but is very temperamental with the Fan and will change speed as I rotate the hot air pencil. Now that i have tried the Weller, I see why paying more for good quality German Engineering is worth it.

     

    As a separate note. I have been using the same Weller Iron for close to 40 years and it is still going strong, paid more for it of course but never needed to buy another for all this time. Lets hope the new one will last as long.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer