Test & Tools
  • Technologies
  • More
Test & Tools
Forum Hot Air Station suggestions?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 12 answers
  • Subscribers 390 subscribers
  • Views 4948 views
  • Users 0 members are here
  • hot_air_stations
Related

Hot Air Station suggestions?

ajens23
ajens23 over 9 years ago

Hi All,

 

I find myself wanting to do more surface mount work.

While a toaster oven works pretty good for the whole board, I would like to try a hot air station.

After looking at a Weller station at over $700 US, then looking at $50 stations on E-bay,

I would like to hear from some actual users and their experiences and recommendations.

 

So what is a reasonable brand of hot air station that will last for several years and not break the bank.

(I.e. under $200US would be nice.)

 

Thanks,

Al

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +3
    Hi Al, I have the same unit 21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14 that michaelwylie has. When I got it I modified it to include a shut off in the cradle. I was pretty…
  • mcb1
    mcb1 over 8 years ago +3 suggested
    I have the same unit as kas.lewis referred to Tenma 21-10130 21-10130 it has the cutoff feature when you place the handpiece down, and the picture doesn't show it, but includes a temperature controlled…
  • dougw
    dougw over 8 years ago +3
    I use an Aoyue because it was low cost, but it works fine for my needs. I use it for rework (chip removal) and small heat shrink tubing.
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Al,

     

    I have the same unit 21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14  that michaelwylie  has. When I got it I modified it to include a shut off in the cradle. I was pretty disappointed in the quality of the circuit board. I have seen six year old kids who can solder better than this. On the other hand, once it was modified to suit me it has gone on to work without problems for a couple years now. I do not know if this speaks to the quality of Tenma but if solder jobs like this bother you then perhaps paying a little more for quality is a good idea.

     

    image

     

    image

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 9 years ago

    Hi Al,

     

    I have the same unit 21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14  that michaelwylie  has. When I got it I modified it to include a shut off in the cradle. I was pretty disappointed in the quality of the circuit board. I have seen six year old kids who can solder better than this. On the other hand, once it was modified to suit me it has gone on to work without problems for a couple years now. I do not know if this speaks to the quality of Tenma but if solder jobs like this bother you then perhaps paying a little more for quality is a good idea.

     

    image

     

    image

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ajens23
    0 ajens23 over 9 years ago in reply to jw0752

    Thanks for the great responses everyone, my internet is pretty flakey tonight so bear with me.

     

    I have too many wants for the money I make.

     

    I saw some replacement heater elements on e-bay, has anyone had much luck with a DIY hot air station?

     

    With the price of components off e-bay and some of the new power IGFETS from Mouser, this should be a walk in the park, or am I missing something?

     

    How critical is the temperature regulation? On a standard iron it's better to be too hot than too cold, are we looking at the same principle here or does the temp need to be pretty close?

     

    I can just get away with a 900F (type J?) thermocouple yes?

     

    Al

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jbundock
    0 jbundock over 8 years ago in reply to jw0752

    Hi John,

     

    I ordered the same unit 21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14

    I probably wouldn't have if I saw your post first.  Anyway I noticed the description as "100V" after I ordered it.  Is that a typo

    or does this thing require Japan standard 100VAC or does it come with a standard 120V standard USA plug? I've seen

    models with the same part number specified for 220V and when I look on the TENMA website for the manual it throws

    an error.  What manufacturer would have the exact same part number for devices that have different power requirements?

     

    Regards,

     

    Jim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to jbundock

    Hi James,

    My unit runs on 120 volts just fine. Once I closed the case and stopped looking at the solder job it has continued to work well and properly. I have had it for about three years now and I have had no problems. Yours will probably have a better solder job than mined did as I can't believe things could have gotten worse.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jbundock
    0 jbundock over 8 years ago in reply to jw0752

    Thanks John,

     

    I was weirded out by the "100V" spec on the Newark site.  As long as it has a USA plug like yours I'm all set.  I'm hopeful the workmanship has improved, but I'll take a peek.  I tried looking everywhere to verify that the thing I ordered had a US plug, but to my chagrin, I discovered the manufacturer uses the same part number for the 220V unit so I thought wow, will this one be Japanese (100VAC)?  I wish they'd show a picture of the back or have a spec sheet that is actually a spec sheet, or put the manual online (the Temna website is useless).  Oh well, I feel a little better now that it I know it is almost certainly going to have a US power plug. Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to jw0752

    I've always fancied these things:

     

    PCB Pre-heaters. Preheat for SMT, SMD, BGA. Lead-Free Solder Preheaters. Rework Pre-heat.

     

    Not very cheap (but competitive with Weller and the like) but they look as if they're pretty focused on what they do.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer