Test & Tools
  • Technologies
  • More
Test & Tools
Forum Hot Air Station suggestions?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 12 answers
  • Subscribers 390 subscribers
  • Views 4948 views
  • Users 0 members are here
  • hot_air_stations
Related

Hot Air Station suggestions?

ajens23
ajens23 over 9 years ago

Hi All,

 

I find myself wanting to do more surface mount work.

While a toaster oven works pretty good for the whole board, I would like to try a hot air station.

After looking at a Weller station at over $700 US, then looking at $50 stations on E-bay,

I would like to hear from some actual users and their experiences and recommendations.

 

So what is a reasonable brand of hot air station that will last for several years and not break the bank.

(I.e. under $200US would be nice.)

 

Thanks,

Al

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +3
    Hi Al, I have the same unit 21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14 that michaelwylie has. When I got it I modified it to include a shut off in the cradle. I was pretty…
  • mcb1
    mcb1 over 8 years ago +3 suggested
    I have the same unit as kas.lewis referred to Tenma 21-10130 21-10130 it has the cutoff feature when you place the handpiece down, and the picture doesn't show it, but includes a temperature controlled…
  • dougw
    dougw over 8 years ago +3
    I use an Aoyue because it was low cost, but it works fine for my needs. I use it for rework (chip removal) and small heat shrink tubing.
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Al,

     

    I have the same unit 21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14  that michaelwylie  has. When I got it I modified it to include a shut off in the cradle. I was pretty disappointed in the quality of the circuit board. I have seen six year old kids who can solder better than this. On the other hand, once it was modified to suit me it has gone on to work without problems for a couple years now. I do not know if this speaks to the quality of Tenma but if solder jobs like this bother you then perhaps paying a little more for quality is a good idea.

     

    image

     

    image

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ajens23
    0 ajens23 over 9 years ago in reply to jw0752

    Thanks for the great responses everyone, my internet is pretty flakey tonight so bear with me.

     

    I have too many wants for the money I make.

     

    I saw some replacement heater elements on e-bay, has anyone had much luck with a DIY hot air station?

     

    With the price of components off e-bay and some of the new power IGFETS from Mouser, this should be a walk in the park, or am I missing something?

     

    How critical is the temperature regulation? On a standard iron it's better to be too hot than too cold, are we looking at the same principle here or does the temp need to be pretty close?

     

    I can just get away with a 900F (type J?) thermocouple yes?

     

    Al

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ajens23
    0 ajens23 over 9 years ago in reply to jw0752

    Thanks for the great responses everyone, my internet is pretty flakey tonight so bear with me.

     

    I have too many wants for the money I make.

     

    I saw some replacement heater elements on e-bay, has anyone had much luck with a DIY hot air station?

     

    With the price of components off e-bay and some of the new power IGFETS from Mouser, this should be a walk in the park, or am I missing something?

     

    How critical is the temperature regulation? On a standard iron it's better to be too hot than too cold, are we looking at the same principle here or does the temp need to be pretty close?

     

    I can just get away with a 900F (type J?) thermocouple yes?

     

    Al