Test & Tools
  • Technologies
  • More
Test & Tools
Forum Reverse polarity protection circuit & output backward flow control
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 7 answers
  • Subscribers 387 subscribers
  • Views 6042 views
  • Users 0 members are here
  • reverse polarity protection
Related

Reverse polarity protection circuit & output backward flow control

tim687
tim687 over 9 years ago

I am building my own (2 channel) lab bench. This is the conversion board I'm using to convert 12V (input) to 1-24V (one for each channel).

 

In the product description they say

Input reverse connect protection: No (If necessary, please input series schottky diode)
Output control flow backward: No (If used for battery charging or load is bring electricity load, please on the output side series schottky diode)

This does mean that there is no reverse polarity input protection (that is not needed anyways), but does this mean that there is reverse polarity output protection?

In the datasheet of the LTC3780 I found the following pin descriptions in the pinout:

 

SENSE+ (Pin 3/Pin 1):

The + Input to the Current Sense

and Reverse Current Detect Comparators. The ITH

pin voltage and built-in offsets between SENSE– and SENSE+ pins,

in conjunction with RSENSE, set the current trip threshold.

SENSE– (Pin 4/Pin 2):

The (–) Input to the Current Sense

and Reverse Current Detect Comparators.

 

Is this the reverse polarity protection feature and output backward flow control I'm looking for?

 

If yes, I don't have to design the circuitry to protect the output, if no, could you provide a solution which can accept variable voltages?

This is one solution I found very interesting due to the indicator LED and the 'no power loss' (claim).

Due to inefficiency of a schottky diode I am only going to use it if necessary.

 

Thanks in advance for helping me out!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago +1 suggested
    This board will make a truly dreadful bench supply - unless you only want it to work light bulbs or heaters then please think again. I recently helped a customer trouble shoot a new design where they had…
  • rachaelp
    rachaelp over 9 years ago in reply to michaelkellett +1 suggested
    Michael Kellett wrote: For a general purpose bench supply you can't beat a decent linear design - just learn to live with the size, weight and heat MK You can also do a hybrid design to try and get the…
  • michaelkellett
    michaelkellett over 9 years ago in reply to tim687 +1 suggested
    Hello Tim, The noise is un-fixable by any reasonable means - it consists of bursts of very large amplitude 50-130 MHz decaying sine bursts as the power devices switch. We put at least 160 hours of engineering…
  • jw0752
    0 jw0752 over 9 years ago

    Hi Tim,

     

    While the LTC3780 may support some protections the advertising indicates that there is no protection. Schottky diodes are relatively inexpensive and if you feel that there is any danger of reverse voltages being applied it won't hurt to put a diode in parallel for the input and in series for the output. You will only loose 0.4 volts on the output. There is no loss for the use of the polarity protection diode in parallel on the input.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • tim687
    0 tim687 over 9 years ago in reply to jw0752

    Hi John,

     

    At 10 Amps that is 4 Watt of power, I am not concerned about the power loss, but more of the heat. I want the lab bench to be very reliable and putting the diodes to handle this load is not making me very confident about the lab bench.

    There is no relay circuit for variable voltages?

     

    The input of the DC-DC converter will be the right way around at all times, so no protection is needed there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 9 years ago in reply to tim687

    Hi Tim,

     

    I'm not saying this is the correct diode, but it is similar to what I would use in your application. Search Newark for a diode that has twice your expected output voltage and as low a junction voltage as possible. This one will handle 16 Amps. Of course you will have to heat sink it to get this amount of power through it. Another possibility might be to use a P Channel MOSFET as a switch but I will have to investigate how that would work. P Channel Power MOSFET can have very low impedance at saturation.

     

    http://www.newark.com/ixys-semiconductor/dss16-01a/diode-schottky-16a-to220ac/dp/96K8814

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tim687
    0 tim687 over 9 years ago

    Hi John,

    I saw an circuit that used mofsets to fix this issue and I gather three n channel mosfets. I might have a few other (p channel) laying around.

    Is there any drawback at using this method to solve my problem?

     

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 9 years ago in reply to tim687

    Hi Tim,

    Can you post the schematic of the circuit that you mentioned. If I can't render an opinion there are many guys on the site smarter than me who can.

    Thanks

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tim687
    0 tim687 over 9 years ago in reply to jw0752

    Hi John,

     

    I found this on instructables.com. This is an extended version of that same instructables.com instruction, but on a different website.

    They both look very promising.

     

    Thanks for your help!

     

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago

    This board will make a truly dreadful bench supply - unless you only want it to work light bulbs or heaters then please think again.

     

    I recently helped  a customer trouble shoot a new design where they had used the LTC3780 - the network connections would not work dues to power supply noise.

     

    I made two different versions of test boards, bought  a board  a bit like yours from Amazon and also tested the Linear Technology demo board - all of the boards were still very very noisy - quite unusable for a general purpose bench supply.

     

    The conversion efficiency that can be achieved with this chip is great - but the noise is a huge issue.

     

    We moved over to using buck only switchers on the original board (since we didn't have to have the LTC3780's boost capability) and this worked much better.

     

    For  a general purpose bench supply you can't beat a decent linear design - just learn to live with the size, weight and heat image

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

    For a general purpose bench supply you can't beat a decent linear design - just learn to live with the size, weight and heat

     

    MK

    You can also do a hybrid design to try and get the best of both worlds (with a little compromise). If you use a switcher to get the voltage to a few volts above your desired output and then use a linear regulator to step down to your desired output voltage, you get a reduction in switching noise because the power supply rejection ratio (PSRR) of the linear regulator is high without too much heat in the linear regulator as the switcher reduces the voltage drop across it.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • tim687
    0 tim687 over 9 years ago in reply to michaelkellett

    Hi Micael,

     

    The noise is something which I guess can be fixed with a few capacitors? Unfortunately I need the boost capability of the LTC3780. I am using a server powersupply as a 12V provider that will go into the LTC board. I do have a few (couple of hunderd) capacitors laying around that I can use to smooth out the output of the power supply.

     

    Is there any formula or rule of thumb to picking the right capacitor for a variable voltage/amperage output?

     

    Thanks,

     

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tim687
    0 tim687 over 9 years ago in reply to rachaelp

    The voltage is variable so I'm not sure how I'd make such a circuit with regulators. I only have a few 5V linear regulators available currently.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>