Test & Tools
  • Technologies
  • More
Test & Tools
Forum MULTICOMP PRO MP750065 Function Generator - Programming Pt6: LabVIEW Driver Lib: High Level Functional blocks
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 383 subscribers
  • Views 2724 views
  • Users 0 members are here
  • MP750065
  • function_generator
  • labview
  • scpi
Related

MULTICOMP PRO MP750065 Function Generator - Programming Pt6: LabVIEW Driver Lib: High Level Functional blocks

Jan Cumps
Jan Cumps over 4 years ago

In this 5th post in this Program the Device series I develop a Virtual Instrument Read, Write and Close block.
It's the follow up of MULTICOMP PRO MP750065 Function Generator - Programming Pt5: LabVIEW Driver Lib Read, Write and Close blocks.
For the MP750668, UTG900C-II, UTG1010 owners: this will very likely work for you too.

image

I'm designing LabVIEW Virtual Instrument functional blocks that allow you to control and query the instrument without reading the programming guides.

Functional Blocks approach

The goal of these blocks, is that you can use them in your test setup easily. You don't have to read the manuals to understand the commands and register addresses.
To set the instrument or read values, you:

  • set what channel you want to talk to
  • select the function from a drop-down list
  • in case of reading, that's it. You'll get the value.
  • when you want to set a function, the drop-down list helps with the valid input values.

image

With the Get Parameters and Set Parameters block, you can build a decent automation flow.
Even though some of the functions, such as sweep and modulation, aren't listed in the drop-downs, they can be set with a combination of these blocks.
Once I'm more familiar with that part of my instrument, I may add specific functions for those.

In the previous post you could see that I reused the Error block in other blocks.
In this level, I'm reusing the Read and Write blocks. You will not find any UCI dll calls in these, because they are encapsulated in the layer below.

Get Parameters block

Read any of the instrument settings that can be controlled by software.

image
2 inputs:

  • channel (0, 1)
  • function (frequency, waveform, amplitude, ...)

1 output:

  • the requested value

Usage example: get the current output frequency

image

Set Parameters block

Control any of the instrument settings.

image

3 inputs:

  • channel (0, 1)
  • function (frequency, waveform, amplitude, ...)
  • value to set. Check the drop-down list for the acceptable inputs.


Usage example: set the output waveform and activate that output:

image

The last object to review is a utility block that converts the raw output bytes of a read operation into a number:

Output To Double block

Takes the 8 bytes that are returned by a Read operation, and convert them into a double.

image

The Get Parameter block uses this one to transform the output in what you need.
I made it a separate block because it can also be used in combination with the low level Read block.
There's a number of manipulations to do with the output to get it as a valid double: deal with the endianness, and cast into the final format.
This block handles that. I should have documented it in the low level post, but ran out of time :).

Example Flows

Virtual Instrument drivers in LabVIEW often come with examples. I've done the same:

image

There's one for the functional blocks, and another for the low level approach.

Functional block example

  • initialise instrument
  • set output frequency
  • get output Vpp
  • get output frequency
  • set output waveform to square
  • switch output on
  • close instrument

Control panel:

image

Block diagram:

image

Low Level block example

  • initialise instrument
  • set output frequency
  • get output frequency
  • close instrument

Control panel:

image

Block diagram:

image

I've attached the project. It's in LabVIEW Community Edition. The attached library can not to be used for commercial activities and other uses that are excluded by its license.
The design that I described here comes without license. Feel free to use as you like.

driver.zip

Drivers on the accompanying CD need to be installed.
You will also need the UCI dll. You can find that in the install directory when you install the software on the instrument's CD. It's also part of the SDK distribution (see post #1).
I don't have an additional PC where I can test this. I expect that when you first run this example, LabVIEW will prompt for the DLL. Comment here if that's not true.

Happy Testing!

Related blog:

MULTICOMP PRO MP750065 Function Generator - 1st impressions
Programming Pt1: SDK Demo
Programming Pt2: LabVIEW tryout (a)
Programming Pt3: LabVIEW tryout (b)
Programming Pt4: LabVIEW Driver Lib Init block
Programming Pt5: LabVIEW Driver Lib Read, Write and Close blocks
Programming Pt6: LabVIEW Driver Lib: High Level Functional blocks
  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 4 years ago +3
    action video: https://youtu.be/19Hv33z5KmQ
  • Jan Cumps
    Jan Cumps over 4 years ago

    action video:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +3 Vote Down