Test & Tools
  • Technologies
  • More
Test & Tools
Forum Keithley DMM6500 Scanner Card - mystery component hidden in one of the channels
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 382 subscribers
  • Views 5098 views
  • Users 0 members are here
  • pt100
  • 88ad1490-a97d-11ed-afa1-0242ac120002
  • 2000-scan
  • keithley
  • scan-2000
Related

Keithley DMM6500 Scanner Card - mystery component hidden in one of the channels

Jan Cumps
Jan Cumps over 3 years ago

When I was wiring my Keithley 2000-SCAN card, I found a little component hidden inside the connector for channel 3. I hadn't spotted it before, just saw it during my work.
I initially thought it was a wire bridge used to measure the relay resistance. But it was a tiny component:

image

A little device on a ceramic chip.

I regret that I didn't take a photo first. Fortunately, I saw that it was visible on a photo I took for my first blog (and I hadn't deleted the original high resolution version yet):

image

I measured it, and it was around 100Ω. 108Ω actually. I thought that it could be a shunt for current measurement. But that's not very precise for a 100Ω resistor. When I touched it, I saw that the resistance increased fast. And that's when I realised it's a local temperature reference: Pt100 /RTD. The Pt100 is a common player in the measurement- and control (control theory) practice.

I found one on the e14 shop that looks very similar to the one embedded in my card: NB-PTCO-152  RTD SENSOR, THIN FILM PLATINUM, 100R. The photo on the Farnell page isn't the same, but the picture in TE's datasheet is very similar. The blackish look of the leads on my component seem to point that they are the silver version.

image

Mystery solved

link to all posts

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago in reply to wolfgangfriedrich +3
    These are things you don't learn when you buy new things. Second hand comes with a story.
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to scottiebabe +3
    Side story: I made an app for the meter. To calculate a microcontroller's power envelope, and using the EEVBog µCurrent as test probe. It works.
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps +3
    What a time to be alive, installing apps on our color touchscreen multimeters , that's great work!
Parents
  • Jan Cumps
    Jan Cumps over 3 years ago

    Yesterday, I tried to put the device back inside the connectors. In channel 1, so that the default scripts for the DMM6500 would work.
    Unfortunately, even while I was careful, one of the leads of the Pt100 broke off. It was not a surprise - I was extra careful because I could feel that this was a weak point.

    Once I have saved some more equipment budget, I'll buy a new Pt100. Or if you have one that you can miss, send it to me.
    I'll post a comparison of temperature measurement, one with a simulated cold junction temp value, one with a Pt100 ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    It's ridiculously easy to break the leads off them : ( I destroyed my only PT1000 that way too, barely flexed but its a weak point there. Does DMM6500 allow for thermistor params to be configured for cold junction compensation? Not as ideal but I've got at least a hundred of them here (mostly surface mount but easy to tack wires onto). I can easy shove a load of them into a envelope tomorrow.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz

    I ordered a little set of 5 "RTD PT100 Tiny thin film type Class A".

    That 'll be enough to at least try to get one of them inside the screw terminals of channel 1 and let it sit there forever.

    I'm going to put that on channel one, because that's the assumption on the DMM6500 / 2000-SCAN combo when using a cold junction reference.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz
    shabaz said:
    Does DMM6500 allow for thermistor params to be configured for cold junction compensation?

    Yes. And one of those options is to enter that temperature by hand. The error you make (if you just guess it) will influene the measurement error.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz

    My order arrived:

    image

    The leads are short. There will be some fiddling required.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz

    My order arrived:

    image

    The leads are short. There will be some fiddling required.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • BigG
    BigG over 3 years ago in reply to Jan Cumps

    Not sure if these would be suitable for your application. I've had these 3 samples sitting in a box for over 10 years and still to find a proper use for them.

    {gallery:autoplay=false}IST PT100

    image

    image

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to BigG

    The ones I have work. I just placed one. It is finicky but doable.