Test & Tools
  • Technologies
  • More
Test & Tools
Forum Solder station selection
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 388 subscribers
  • Views 3963 views
  • Users 0 members are here
Related

Solder station selection

davebullockmbe
davebullockmbe over 7 years ago

Hi everyone,

Having worked for many years with an ERSA  Analog 60A and then an ERSA  Digital 2000A both equipped with the TechTool iron I am spoiled when it comes to choosing a similar machine.

My son is getting interested in electronic construction and a solder station for Christmas seems like a great present.

However to set him up with a full ERSA kit with spare tips and maybe a replacement heating element would be well over £500.

I love the ERSA ease of tip change and the instant availability of continuous heat when soldering large components (you can solder a washer to a battleship..LOL) but how do less expensive setups perform?

Each alternative I follow up has both glowing praise and dire reviews in equal measure, it's so confusing!

So what are you you all using, and can I have some recommendations/warnings of what to choose/avoid from the Farnell range please?

Thanks in anticipation.....

Dave

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +5
    I have several irons, but the one I use all the time is an old Hakko 936 - it has worked consistently well for many years. There seem to be other companies either cloning or licensing Hakko designs. This…
  • Jan Cumps
    Jan Cumps over 7 years ago +4
    I'd keep it very simple for a kid. It's not the gear that counts, but the pleasure of soldering.
  • michaelkellett
    michaelkellett over 7 years ago +3
    I've been using i-con picos for years (since ERSA stopped supporting the big expensive station I had.) I've found them to be pretty good. I also have an RS Pr Ds90 which is good for heavier work and has…
Parents
  • dougw
    dougw over 7 years ago

    I have several irons, but the one I use all the time is an old Hakko 936 - it has worked consistently well for many years. There seem to be other companies either cloning or licensing Hakko designs. This model does not have a digital thermometer, I set the temperature to a point where I can make a joint quickly. As with just about all irons, the temperature control setting needs to change based on thermal mass of the tip and thermal mass of the component and area of the trace. I have a "feel" for what will work for any given situation, so I pretty much set the temperature automatically without thinking. I don't even know what the temperature is, I just know how long I want to take to make a good joint. Temperature is marked on the dial, but I have never checked to see if it is accurate. Obviously it doesn't measure the temperature right at the tip and that temperature there will fluctuate depending on what it is touching. I generally use a fairly fine point tip, but might swap it for a bigger one if the job requires a lot of heat.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 7 years ago

    I have several irons, but the one I use all the time is an old Hakko 936 - it has worked consistently well for many years. There seem to be other companies either cloning or licensing Hakko designs. This model does not have a digital thermometer, I set the temperature to a point where I can make a joint quickly. As with just about all irons, the temperature control setting needs to change based on thermal mass of the tip and thermal mass of the component and area of the trace. I have a "feel" for what will work for any given situation, so I pretty much set the temperature automatically without thinking. I don't even know what the temperature is, I just know how long I want to take to make a good joint. Temperature is marked on the dial, but I have never checked to see if it is accurate. Obviously it doesn't measure the temperature right at the tip and that temperature there will fluctuate depending on what it is touching. I generally use a fairly fine point tip, but might swap it for a bigger one if the job requires a lot of heat.

    • Cancel
    • Vote Up +5 Vote Down