Test & Tools
  • Technologies
  • More
Test & Tools
Forum Solder station selection
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 388 subscribers
  • Views 3954 views
  • Users 0 members are here
Related

Solder station selection

davebullockmbe
davebullockmbe over 7 years ago

Hi everyone,

Having worked for many years with an ERSA  Analog 60A and then an ERSA  Digital 2000A both equipped with the TechTool iron I am spoiled when it comes to choosing a similar machine.

My son is getting interested in electronic construction and a solder station for Christmas seems like a great present.

However to set him up with a full ERSA kit with spare tips and maybe a replacement heating element would be well over £500.

I love the ERSA ease of tip change and the instant availability of continuous heat when soldering large components (you can solder a washer to a battleship..LOL) but how do less expensive setups perform?

Each alternative I follow up has both glowing praise and dire reviews in equal measure, it's so confusing!

So what are you you all using, and can I have some recommendations/warnings of what to choose/avoid from the Farnell range please?

Thanks in anticipation.....

Dave

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +5
    I have several irons, but the one I use all the time is an old Hakko 936 - it has worked consistently well for many years. There seem to be other companies either cloning or licensing Hakko designs. This…
  • Jan Cumps
    Jan Cumps over 7 years ago +4
    I'd keep it very simple for a kid. It's not the gear that counts, but the pleasure of soldering.
  • michaelkellett
    michaelkellett over 7 years ago +3
    I've been using i-con picos for years (since ERSA stopped supporting the big expensive station I had.) I've found them to be pretty good. I also have an RS Pr Ds90 which is good for heavier work and has…
Parents
  • Jan Cumps
    Jan Cumps over 7 years ago

    I'd keep it very simple for a kid. It's not the gear that counts, but the pleasure of soldering.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 7 years ago

    I'd keep it very simple for a kid. It's not the gear that counts, but the pleasure of soldering.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • davebullockmbe
    davebullockmbe over 7 years ago in reply to Jan Cumps

    Hi Jan,

    No he's not a little-un he's 32! and is a software/web designer.

    However he is now into home electronics and had been using my cast-off Weller TCP which isn't ideal for modern components.

    So I want to get him a 'proper' soldering iron for Christmas...LOL!

    Thanks

    Dave

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rsjsouza
    rsjsouza over 7 years ago in reply to davebullockmbe

    At work I use a Metcal and a Hakko FX-951 and I prefer the Hakko - it is a great general purpose station but IMHO a bit expensive for hobby projects. 

     

    In the past I have used the Weller WES51 which is quite comparable to my current Hakko  FX-888FX-888 to me these two stations have a great price/performance for home projects especially if tied to four or five additional tips that help with both large copper areas and narrowest pads and parts

     

    (a stereo microscope is another great accessory to accompany the iron, which can be had for the price difference).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to rsjsouza

    I have a Hakko  FX-888FX-888 at work along with a few Wellers of some sort. At home I have a Metcal  PS-900PS-900 and a Tenma combination hot air and soldering iron station. To be honest, for lots of basic repair work I don't find the choice of iron particularly critical as long as the tip is in decent shape and it makes a decent amount of heat. For many years I soldered with the "awful" nichrome wire direct-mains irons with no big issue aside from the tips eroding way too quickly. I shoved in a Weller tip that wasn't quite right but did the job for many many years ...

     

    Once you develop a feel for the iron and how "hot" it seems to be - you can get into a rhythm in regards to soldering. If you watch the solder as it melts and wets the joint, it's not hard to get a good joint even with a crappy iron that fluctuates in temperature provided it produces enough heat. It's a matter of patience though ... although some parts aren't as heat tolerant or "patient" as others.

     

    I'm not advocating anyone get the awful direct-mains iron for delicate electronics, but I'd have to say the difference between a basic soldering station and a high end professional one isn't that meaningful for most hobbyists.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • davebullockmbe
    davebullockmbe over 7 years ago in reply to rsjsouza

    Hi Thanks for your advice :-)

    Dave