Test & Tools
  • Technologies
  • More
Test & Tools
Forum Need help with some measurements.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 387 subscribers
  • Views 5427 views
  • Users 0 members are here
  • non_slip_probes
Related

Need help with some measurements.

jw0752
jw0752 over 7 years ago

I need some help collecting data about Oscilloscope Probes. I am thinking of making some low frequency Non-Slip probe tip adapters for Oscilloscope probes. With the limited number of Oscilloscope probes with in my reach it does not look like there is any standardization.

 

image

As you can see the two probes that I own each have different diameter probe tips. It would help me plan my project if I could find out what the diameter and length of oscilloscope probes from as many of you as possible. Please measure length of the consistent diameter of the tip and also the diameter itself. I can accept measurement in inches or millimeters. Here is what I hope to be able to build without having to custom make each one.

 

image

 

Your help would be appreciated.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago in reply to dougw +9
    I have 3 types of probe: pin diameter = PD pin length = PL ground ferule diameter = GD ground ferule length = GL plastic barrel diameter = BD plastic barrel length = BL all dimensions in mm
  • Gough Lui
    Gough Lui over 7 years ago in reply to Gough Lui +7
    jw0752 - I decided to give my improvised method a go - I grabbed a piece of foil and corrugated cardboard, punched the probe tip through the foil into the cardboard and scanned the foil at 4800dpi to judge…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to jw0752 +7
    w2aew - a field engineer of Tektronix - has made nice videos on (among other interesting subjects) probing techniques. I use this one at times when direct probing with the pig tail ground is not enough…
Parents
  • hlipka
    hlipka over 7 years ago

    OK, here are my two probes:

    First a Keysight N2140A (from a DSOX1000 series): the tip is (apart from the sharp end) slightly conical - from 1.00 to 1.20mm. Total length of the tip is 4.65mm

    Second, a Tektronix TPP0201 (from a TBS1000B-EDU series): its also conical, from 0.6mm to 0.85mm, total length is 4.5mm.

     

    Looking into the hook fixture of the probes, their internals look like a double-spring contact (kinda like a IC socket, but two-sided). But the actual mechanism to attach the hook part to the probe is different between the two probes.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hlipka
    hlipka over 7 years ago

    OK, here are my two probes:

    First a Keysight N2140A (from a DSOX1000 series): the tip is (apart from the sharp end) slightly conical - from 1.00 to 1.20mm. Total length of the tip is 4.65mm

    Second, a Tektronix TPP0201 (from a TBS1000B-EDU series): its also conical, from 0.6mm to 0.85mm, total length is 4.5mm.

     

    Looking into the hook fixture of the probes, their internals look like a double-spring contact (kinda like a IC socket, but two-sided). But the actual mechanism to attach the hook part to the probe is different between the two probes.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jw0752
    jw0752 over 7 years ago in reply to hlipka

    Thanks Hendrik,

     

    I have added your measurements into my data base. Thanks for looking inside the attachments. I have been curious about them as well but they are likely unique to a given manufacturer.

     

    John