Test & Tools
  • Technologies
  • More
Test & Tools
Forum Can an ESD mat be tested without special tools?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 385 subscribers
  • Views 9529 views
  • Users 0 members are here
Related

Can an ESD mat be tested without special tools?

baldengineer
baldengineer over 7 years ago

There are inexpensive continuity testers that let you verify a loop between you, your wrist strap, and ground.

 

Without investing into special weights (probes), is there an effective way to measure an ESD mat’s resistance? Or more simply, verify areas of an ESD mat are still effective?

 

Can it be done with “just” a multimeter and a power supply?

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 7 years ago +6
    I've tried it with the two kinds of mat I have. This is with 10V from a bench PSU and my 5.5 digit Fluke meter (I also put a 100 ohm resistor in series, in case I touched the probes together, though I…
  • rsc
    rsc over 7 years ago +6
    ANSI / ESD S4.1-2006 Test Procedure According to ANSI / ESD S20.20-2014, an acceptable work surface will have a point to point and a point to groundable point resistance of less than 1.0 x 10^9 ohms. ANSI…
  • Gough Lui
    Gough Lui over 7 years ago +5
    I suspect some meters which cam measure in the tens of megohms can probably produce a reading on some carbon impregnated rubber mats. Then again there are other with a lot higher resistance rubber - I…
Parents
  • shabaz
    shabaz over 7 years ago

    Hi James,

     

    I just tested a couple of mats here, with a multimeter set to ohms, and the probes about 1 inch apart (near center of mat).

    The first mat was plastic-y, not rubbery. It measures around 12k ohm, although the resistance varies depending on the pressure I use. It's 12k with normal probe troubleshooting force.

    I don't actually use this mat for soldering or as a work-surface - I chopped it up and used it to line some drawers.

    The second mat is some 2-layer material, softer, and has a light-brown side and a black side (the light-brown side is the top surface). The black side has a resistance of about 10 Mohm and again that varies with probe force (more than order of magnitude reduction if pressed more firmly). However the light-brown side I cannot measure this way (I could apply an insulation tester to it, but have not done that yet), so it's at least 50M ohm, the limit of the multimeter, no matter how hard I press.

    Nether mat was expensive, the first one was maybe £25/$30 USD, the second is about $50, and both were larger than my desk (maybe 1500mm long, I have not measured).

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago

    Hi James,

     

    I just tested a couple of mats here, with a multimeter set to ohms, and the probes about 1 inch apart (near center of mat).

    The first mat was plastic-y, not rubbery. It measures around 12k ohm, although the resistance varies depending on the pressure I use. It's 12k with normal probe troubleshooting force.

    I don't actually use this mat for soldering or as a work-surface - I chopped it up and used it to line some drawers.

    The second mat is some 2-layer material, softer, and has a light-brown side and a black side (the light-brown side is the top surface). The black side has a resistance of about 10 Mohm and again that varies with probe force (more than order of magnitude reduction if pressed more firmly). However the light-brown side I cannot measure this way (I could apply an insulation tester to it, but have not done that yet), so it's at least 50M ohm, the limit of the multimeter, no matter how hard I press.

    Nether mat was expensive, the first one was maybe £25/$30 USD, the second is about $50, and both were larger than my desk (maybe 1500mm long, I have not measured).

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Gough Lui
    Gough Lui over 7 years ago in reply to shabaz

    Very interesting readings - thanks for sharing. If I had a mat, I'd go and measure it too ...

     

    - Gough

    • Cancel
    • Vote Up +4 Vote Down