Test & Tools
  • Technologies
  • More
Test & Tools
Documents Programmable Electronic Load - ADC and DAC BoosterPack test
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 24 Nov 2017 11:12 AM Date Created
  • Last Updated Last Updated: 2 Dec 2017 10:04 AM
  • Views 5738 views
  • Likes 7 likes
  • Comments 35 comments
Related
Recommended

Programmable Electronic Load - ADC and DAC BoosterPack test

WIP

 

This blog documents the characteristics of the DAC/ADC BoosterPack of the electronic load that Robert Peter Oakes, jc2048 and Jan Cumps are designing.

We have the same DAC/ADC BoosterPacks so we can compare the measurements of each ADC and DAC channel. Check the main document for anything related to hardware and firmware.image

 

Test Setup

 

Peter has created a GUI that we can use to shoot SCPI commands. We can control the DACs and read the ADCs.

Measurements are performed with and without the power driver BoosterPack installed. We'll use 5V to power the DACs and ADCs in both situations.

 

image P1 and P2 on the bottom of the DAC/ADC BoosterPack have to be open. Else you'll inject 5V onto the LaunchPad 3V3 rail and you'll damage components.

 

It's not critical if you switch on the power supply before or after you connect the LaunchPad to your computer. The circuits are isolated.

All measurements use P3.10 as GND reference and P3.1 as reference voltage.

 

image

 

Setup without the power driver BoosterPack:

Mount the DAC/ADC BoosterPack on the LaunchPad.

Use a +5V power supply. It should be a decent one, current is approximately 5 mA.

Connect image with DAC/ADC BoosterPack P4.2  and image with P4.1.

 

Setup with the power driver BoosterPack:

Mount the DAC/ADC BoosterPack on the LaunchPad and the Power Driver BoosterPack on top of that.

On the Power Driver BoosterPack, bridge pins P2.4, P2.5 and P2.6 to tie both opamp inputs of opamp 3D to ground.

Use a +12V power supply. It should be a decent one, current is approximately 50 mA.

Connect image  with Power Driver BoosterPack P1.1 image  and with P1.2.

 

image

 

Measurements

 

In the table, the first column shows what we're measuring, the second column the SCPI command to execute with Peter's GUI.

The next columns are the measurements for Peter, Jon or Jan with and without the Power Driver BoosterPack.

The last column is for comments. We can indicate odds, errors, learnings.

 

JonPeterJan
Data PointSCPIWithoutWithWithoutWithWithoutWithMeasurement method
SupplyN/A4.989 V11.88 VDMM
DAC/ADC V+N/A4.989 V5.035 VDMM
VREFN/A2.046 V2.046 VDMM
ADC A GNDDEVE:ADC1?2SCPI output
ADC A VREFDEVE:ADC1?10918SCPI output
ADC ADEVE:ADC1?1138SCPI output
ADC B GNDDEVE:ADC2?12SCPI output
ADC B VREFDEVE:ADC2?10920SCPI output
ADC BDEVE:ADC2?1
SCPI output
ADC C GNDDEVE:ADC3?22SCPI output
ADC C VREFDEVE:ADC3?1092010919SCPI output
ADC CDEVE:ADC3?26868SCPI output
ADC D GNDDEVE:ADC4?83SCPI output
ADC D VREFDEVE:ADC4?1091910919SCPI output
DAC A 0DEVE:DAC1 00.000 V0.001 VDMM
DAC A maxDEVE:DAC1 655352.040 V2.040 VDMM
DAC B 0DEVE:DAC2 00.005 V0.005 VDMM
DAC B maxDEVE:DAC2 655352.046 V2.046 VDMM
DAC C 0DEVE:DAC3 00.000 V0.000 VDMM
DAC C maxDEVE:DAC3 655352.039 V V2.039 VDMM
DAC D 0DEVE:DAC4 00.000 V0.000 VDMM
DAC D maxDEVE:DAC4 655352.039 V2.039 VDMM

 

 

To resolve

With the power driver installed, ADC C and D act strange (probably also A and B, but I didn't inject a voltage in them because they are connected to opamp pins).

In particular strange for ADC D, because that one isn't routed. Strange.

I will try to decrease the frequency of the sample speed and the i²c speed to see if it's related to that ...

 

Follow up: the cause is that OPAMP 3C injects -0.8V into ADC A. All measurements are off when that happens. As soon as I force ADC A positive (by tying it to ground or a positive voltage) all measurements are correct.

 

image

 

We have a separate document to analyse the summing node at zero.

  • metrology
  • boosterpack
  • msp432
  • ti-rtos
  • launchpad
  • laboratory
  • instrument
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago +3
    Hi Jan, I was wondering, what are the expected values, is it reading a value representing 1.602V when it should read a value representing 2.048V? I'm wondering if it could be due to conversion time (i…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to shabaz +3
    yes, Shabaz, I have a controlled value of 2.040 V. Once I mount my additional driver board (self-designed so many things can be wrong ) the ADC says it’s 1.6 V. I checked signals with my scope to see if…
  • jc2048
    jc2048 over 6 years ago in reply to Andrew J +3
    Andrew J , have you read the blog I did when building Jan and Peter's load? That has some material on the low end of the DAC. Long story short, I adapted the analogue stuff after the DAC so the output…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    no. Nothing from the off-board power components. I haven't purchased them yet. So the inputs for the sense opamp are floating -> output can be anything -> may be the cause for the woes ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps

    Do you have the current sense resistor attached?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    owkey. There's -0.799V on that pin and the ADC doesn't like that at all. Once I push that ADC pin to 0 or higher, all channels work fine.

    So we can now look at the opamp that's feeding ADC A.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    For some yet to understand reason: if I tie ADC A to ground then all others work fine. odd ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago

    For some reason it's working now. I'm not comfortable because I don't know the reason.

    I've removed and plugged in everything - but I've done that umphteen times before.

     

    With the board:

    (I didn't drive ADC C because that's a diret output from an opamp without any resistor between opamp and ADC so I don't want to fidle with that)

     

    DEVE:ADC1 = -0.006

    DEVE:ADC2 = 0.000187500

    DEVE:ADC3 = -0.00468750

    DEVE:ADC4 = -0.00431250

     

     

    DEVE:ADC1 = 2.03662

    DEVE:ADC2 = 0

    DEVE:ADC3 = 2.03888

    DEVE:ADC4 = 2.03944

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago

    Without board loaded, sampling ADC A - D

     

    With 2.046 attached (connected to VREF)

    DEVE:ADC1 = 2.04731

    DEVE:ADC2 = 2.04731

    DEVE:ADC3 = 2.04731

    DEVE:ADC4 = 2.04731

     

    With 0V attached (connected to ground)

    DEVE:ADC1 = -0.000375000

    DEVE:ADC2 = -0.000375000

    DEVE:ADC3 = -0.000375000

    DEVE:ADC4 = -0.000375000

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    for the channel C (pulled up to 5v by default) I applied several voltages between 0 and 2.40 V. Channel D is unconnected on the power board. I did the same there. They both are similarly wrong when the Power Driver board is mounted, correct when only the ADC/DAC board is mounted.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps

    "I'd like to trace this down before they start building up the load."

     

    Don't worry, you are way ahead of me. I received your package during the week but I haven't had time to build anything.

     

    I'm not clear what you are doing. Input C would normally be the thermistor. Are you connecting the reference to that pin in place of the thermistor?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to shabaz

    This one was connected to ground. The error for 0V is small, results in a slightly negative reading (without the power board mounted it's very close to 0, say +8 - +12). Once the voltages are higher, the error is very significant.

    All the time I'm also checking the pins with a voltmeter and a scope to see if anything is off or if the i2c or analog traces are corrupted/noisy.

     

    I'm currently trying to find reasons for this more than going into resolution mode.

    Once I've checked those -digital domain first because that's the simplest, then analog - I'll exclude the ones that don't make a difference and go in troubleshoot mode.

    I don't mind, because that's a more interesting job than the actual design image .

     

    Jon and Peter are using the same PCB and components as me. I'd like to trace this down before they start building up the load.

    I'm somewhat restricted in available bench time because I work abroad on weekdays and I can't drag my lab along image.

     

    For today, the plan is to get a full i²c capture of ADC channel D. That's not used at all on the power board but has different behaviour.

    I'll do a capture of the communication when it's attached to GND and when it has a stable 2.40 V on the input.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to Jan Cumps

    Hi Jan,

     

    What was the analog input wired to, that corresponded to this logic capture? The reading of 0xFDA2 is -606, which sounds like the input is very close to 0V.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>