Wireless
  • Technologies
  • More
Wireless
Blog The Best HD Radio Receiver
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gervasi
  • Date Created: 18 Sep 2013 4:04 PM Date Created
  • Views 1999 views
  • Likes 1 like
  • Comments 5 comments
  • hd_radio
Related
Recommended

The Best HD Radio Receiver

gervasi
gervasi
18 Sep 2013

A few weeks ago when I started researching HD Radio, I found that there are few high-quality receivers.   I asked Jessica Crotty of C. Crane, a high-end radio retailer, which radio they recommended.  The answer was none of them.  They tested many of them, and they couldn't find any that had good AM performance.  The only one they liked was Sony XDR-F1HD, which is discontinued.  image

 

I had not planned to revisit HD radio again, but someone lent me a Sony XDR-F1HD, so I decided to test it to see how good HD can get.  I compared it to the Insignia NS-HDRAD and an ICF-2010.

 

XDR-F1HD is a receiver only with line-level audio output.  I does not have an amplified output for headphones or a loudspeaker.  It comes with a dipole antenna for FM and a loop for AM. 

 

Analog Reception

Reception using the provided antennas was excellent.  The FM dipole pulled in signals about as well as the whip on the Insignia NS-HDRAD.  The AM loop pulled in many weak stations that I could not hear on other radios. 

 

Connecting the XDR-F1HD to an outdoor vertical antenna did not lead to any intermodulation.  Connecting this same antenna to the Sony ICF-2010 results in so much intermodulation that it’s unusable on the FM band.  (Sony ICF-2010 is a great radio for HF but not so good for FM broadcast reception.)

 

Insignia NS-HDRAD did not experience noticeable intermodulation on this antenna either, but XDR-F1HD picked up more stations.image

 

Digital Reception

The digital portion of broadcast signals is 20dB down from the analog carrier, so you only can expect to listen to the digital portion of strong signals.  XDR-F1HD did a good job recovering digital signals.  There is a lot of hysteresis in XDR-F1HD's signal strength threshold for HD reception.  A strong signal is required for it to start decoding HD.  From there I can drop the signal quite a bit before it switches back to analog.  I never had any problem of it needlessly switching back and forth. 

 

There is a blinking HD indicator to indicate the presence of an HD signal.  On many distant AM stations at night, this indicator blinked without the radio ever switching over the HD signal.  The indicator lets you know the signal is there even if it's too weak to listen to. 

 

Some stations have multiple HD digital sub-channels with different audio fidelity.  For example, my public radio station has two sub-channels with high-fidelity music and a third sub-channel for talk programing with much lower fidelity.  The Insignia NS-HDRAD has the annoying problem of the volume being proportional to fidelity.  So when you switch from a low-fidelity sub-channel to a high-fidelity one, you must turn the volume down or it will get very loud.  The XDR-RF1HD does not exhibit this problem at all.

 

Under the Hood

image

The heatsink on the right is connected to a 3.3V linear regulator.  The linear drives 1.8V linear regulators that supply power to the tuner and the baseband digital module, the two modules in cans. I would love to know if they used two linears in series to filter noise or for some other reason. 

image

The board on the top of the enclosure (on the left side of the picture above) has no parts on it.  It appears to be a stiffener.

 

The boards have mask and copper etch on one side only.  They use jumpers for “solder-side” connections.  This cannot have saved that much money.  You’d think the added cost of the jumpers would outweigh savings from omitting copper and mask from one side. 

 

Conclusion

If HD radio had been adopted before Internet streaming audio was popular, it might have caught on.  It also would have helped if the digital subcarrier were not 20dB below the analog carrier.  When I started reviewing HD Radio a few weeks ago, I thought the world needed someone to make a radio with good enough performance to be used for DXing but that also supports HD.  The lower power, though, makes HD incompatible with DXing.  People willing to adopt a new technology and wanting more audio programming can more easily listen to radio with an app on their phones. 

 

If AM/FM radio is used primarily by people who are not adopting new technology, the service may disappear in the next few decades.  Twenty-five years ago there were stations on shortwave packed in 5kHz intervals, and now there are only a few stations on each band.  Is this the future of AM/FM radio? 

 

Further Reading

  • Brian Beezley does an amazing teardown and review of Sony XDR-F1HD with high-quality pictures.
  • The Sony XDR-F1HD Service Manual
  • A nice discussion of how adjacent channel interference from HD subcarriers is a problem for DXers
  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    Yes, it is a really different world than the one I grew up in. We mostly used the AM/FM radio to keep up with local events, news and weather. The music in most instances was the filler they used to gain…
Parents
  • 2dogs
    2dogs over 9 years ago

    I own two of these Sonys. They're pretty good but very aggravating. Programming is not user-friendly. And when I have an electrical outage they had to be reprogrammed. I had them both going on at each end of my flat. On the NPR HD3 rock station, the one Sony was 1.5 seconds behind the other. I can't figure that one out at all.

    I've had three different JVC HD radios in my car. Two got stolen. They've all behaved really well. So well, in fact, that I've considered replacing the Sonys with JVC car HD radios and use computer power supplies for the 12 volts.
    I've been a radio geek all of my life, 1st Phone and all. I love HD radio and wish it would get greater adoption and have a wider range of receiver hardware. Thanks for the coverage.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 2dogs
    2dogs over 9 years ago

    I own two of these Sonys. They're pretty good but very aggravating. Programming is not user-friendly. And when I have an electrical outage they had to be reprogrammed. I had them both going on at each end of my flat. On the NPR HD3 rock station, the one Sony was 1.5 seconds behind the other. I can't figure that one out at all.

    I've had three different JVC HD radios in my car. Two got stolen. They've all behaved really well. So well, in fact, that I've considered replacing the Sonys with JVC car HD radios and use computer power supplies for the 12 volts.
    I've been a radio geek all of my life, 1st Phone and all. I love HD radio and wish it would get greater adoption and have a wider range of receiver hardware. Thanks for the coverage.