Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog Stirling Blue - Project Summary - Blog 14
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
  • Author Author: dougw
  • Date Created: 20 Jul 2018 10:37 AM Date Created
  • Views 2774 views
  • Likes 12 likes
  • Comments 12 comments
  • type-n-text
  • doug wong
  • bluetooth unleashed
  • bluetooth unleashed design challenge
Related
Recommended

Stirling Blue - Project Summary - Blog 14

dougw
dougw
20 Jul 2018

image

This roller coaster project had some ambitious goals because it is always fun to try and stretch to see if you can achieve them. Dealing with 7 MCUs and all the different development environments wasn't too difficult, but it was still lots of work. Designing the PCBs was fun and they worked well. However assembling 5 PCBs was a bit of a chore because they had hundreds of switches to mount. I definitely did not properly anticipate the time required to design 66 different 3D printed parts and printing hundreds of 2 tone keycaps is also pretty tricky.

The major achievements of the project were:

  • Design, build and program a PSoC4 based Bluetooth terminal with dual LCDs and 60 button keyboard - demonstrate communicating with an android tablet via Bluetooth
  • Design, build and program 2 wireless Type-N-Text micro:bit systems also with LCD and QWERTY keyboard - demonstrate TNT-to-TNT wireless communications
  • Getting a PSoC4 to communicate with a micro:bit via SPI
  • Design a complete package for the Type-N-Text device (66 different plastic parts for each device)
  • Designing and printing 2 types of PCB and assembling 5 PCBs
  • Research Stirling engines, how they work, acquire an engine and measure temperatures, speed. output voltage and output current.
  • Developed a method of measuring fuel level using capacitance
  • Learn about the PSoC6 and make some working programs towards monitoring a Stirling engine

The project objectives that still need work:

  • Automated monitoring of the Stirling engine
  • publishing engine data via Bluetooth

Stats:

14 blogs, 11 videos, buckets of fun

imageimageimageimageimage

image

Capacitive Fuel Measurement

imageimageimageimage

I had fun with this project, it was a lot of work but I'm happy I took it on. The project had perhaps a few more obstacles to overcome than usual and some of the tasks were underestimated but it is all about how you deal with adversity, because sometimes it just happens. I do regret not getting further with the Stirling automation, but I think the Type-N-Text system has far more potential to be adopted by many users. There are over a million micro:bits out there and they could all use the Type-N-Text system.

When I realized the potential of the Type-N-Text system, I re-prioritized the objectives of the project. Projects can really benefit from maintaining the flexibility to exploit interesting and useful spin-off ideas. I am very pleased to be the first one to finally bring a full text interface and full text wireless communications to the micro:bit platform at a nice low cost.

 

 

Related Links:

Bluetooth Unleashed Design Challenge

Bluetooth Unleashed Design Challenge: The Challengers

Bluetooth Unleashed Design Challenge: About This Challenge

 

Links to other blogs for this project:

Stirling Blue - Project Description - Blog 1

Stirling Blue - Unboxing Hero - Blog 2

StirlingBlue1

Stirling Blue - micro:bit TXTR - Blog 3

Stirling Blue - Fuel Measurement - Blog 4

FuelMeasurement1

Stirling Blue - Interface Description - Blog 5

Stirling Blue - BBC micro:bit LCD - Blog 6

microbitLCD1

Stirling Blue - Power Measurement - Blog 7 (updated)

PowerMeasurement1

SpeedMeasurement1

Stirling Blue - Bluetooth Terminal Awakening - Blog 8

BluetoothTerminalAwake1

Stirling Blue - PSoC Bluetooth Terminal Keyboard - Blog 9

PSoC4KeyboardScanning1

Stirling Blue - Bluetooth Terminal - First Contact - Blog 10

BluetoothTerminal1stContact

Stirling Blue - micro:bit QWERTY keyboard & LCD - blog 11

MicroBitKeyboardLCD

Stirling Blue - TNT (Type-N-Text) - blog 12

TNT1

Stirling Blue - TNT Ignition - Blog 13

TNT2

Stirling Blue - Project Summary - Blog 14

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago +4
    Superb finish to the project : ) I'd never seen a Stirling engine before. The TNT actually reminds me of one of the very popular home computers here at one time - the ZX81 : ) The heart of your design…
  • mcb1
    mcb1 over 8 years ago +3
    Well done. It was impressive to see the progress, and yes the Micro:bit TNT is something taht has more potential ... after all not everyone has a Stirling engine It seems that this Design Challenge could…
  • genebren
    genebren over 8 years ago +3
    Excellent wrap up to a very interesting project. It seems that the TNT project in itself is fulfillment of the BT challenge. It will be interesting to see where this beginning will take you. Thanks for…
Parents
  • shabaz
    shabaz over 8 years ago

    Superb finish to the project : ) I'd never seen a Stirling engine before.

    The TNT actually reminds me of one of the very popular home computers here at one time - the ZX81 : )

    The heart of your design, the Micro:bit, is several orders of magnitude more powerful!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 8 years ago

    Superb finish to the project : ) I'd never seen a Stirling engine before.

    The TNT actually reminds me of one of the very popular home computers here at one time - the ZX81 : )

    The heart of your design, the Micro:bit, is several orders of magnitude more powerful!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 8 years ago in reply to shabaz
    1. The ZX81 was a cool device. I almost bought one. If I add my keyboard to the PSoC6 hero card it would be a complete computer that really outperforms any of those early computers,  maybe even the original Apple Mac.