Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog Stirling Blue - TNT Ignition - Blog 13
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
  • Author Author: dougw
  • Date Created: 20 Jul 2018 8:35 AM Date Created
  • Views 2029 views
  • Likes 8 likes
  • Comments 8 comments
  • micro:bit
  • type-n-text
  • doug wong
  • tnt
  • bluetooth unleashed
  • bluetooth unleashed design challenge
Related
Recommended

Stirling Blue - TNT Ignition - Blog 13

dougw
dougw
20 Jul 2018

This blog wraps up work on the Type-N-Text (TNT) devices. It has come right down to the wire with only hours left in the challenge and I really wanted to get these devices working. I miscalculated the amount of effort the project would take pretty badly so everything would have had to go perfectly in the last 2 week to complete everything I wanted to achieve. But of course things weren't going to go perfectly and they definitely didn't. After completing the micro:bit-to-PSoC communication in the last blog, it should have been a simple matter of whipping up a little radio program. However the IDE was unable to load the radio library. It turns out I had to upgrade to the latest IDE to have radio support. The latest editor version does have radio support, but it totally broke my existing code, refusing to configure the micro:bit pins the way they were designed to work - and were working fine in the old IDE. This was a major setback with just one day left in the challenge, but I decided to put my head down and just focus on getting the TNT working. I had to go back to the drawing board, develop new schematics, tear the devices apart, rewire them, reprogram the micro:bits to reflect all the changes and then debug some nasty ping-pong run-on issues. So here it is about 5am on the final day and still trying to get the blog published.

At least the effort paid off in a working system as you can see in this video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

There is nothing like having to redesign, teardown, rebuild and reprogram a 3 month project in one evening I may sound a little tired in the video....

I don't really have time to publish all the material I have on Stirling engines and further work with the PSoC6, but I will try to make a wrap-up blog.

 

Related Links:

Bluetooth Unleashed Design Challenge

Bluetooth Unleashed Design Challenge: The Challengers

Bluetooth Unleashed Design Challenge: About This Challenge

 

Links to other blogs for this project:

Stirling Blue - Project Description - Blog 1

Stirling Blue - Unboxing Hero - Blog 2

StirlingBlue1

Stirling Blue - micro:bit TXTR - Blog 3

Stirling Blue - Fuel Measurement - Blog 4

FuelMeasurement1

Stirling Blue - Interface Description - Blog 5

Stirling Blue - BBC micro:bit LCD - Blog 6

microbitLCD1

Stirling Blue - Power Measurement - Blog 7 (updated)

PowerMeasurement1

SpeedMeasurement1

Stirling Blue - Bluetooth Terminal Awakening - Blog 8

BluetoothTerminalAwake1

Stirling Blue - PSoC Bluetooth Terminal Keyboard - Blog 9

PSoC4KeyboardScanning1

Stirling Blue - Bluetooth Terminal - First Contact - Blog 10

BluetoothTerminal1stContact

Stirling Blue - micro:bit QWERTY keyboard & LCD - blog 11

MicroBitKeyboardLCD

Stirling Blue - TNT (Type-N-Text) - blog 12

TNT1

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +4
    Well done. Yes it is frustrating when all your hard work gets undone by what should be a simple upgrade. Good luck I'm sure there will be a few hours room for your completion. No-one can deny you this…
  • aspork42
    aspork42 over 8 years ago +3
    Glad you found a use for that old floppy disk Great case! For buttons, i try to link the together inside the case to keep them all lined up; so it is one big piece instead of many.
  • dougw
    dougw over 8 years ago in reply to mcb1 +2
    have to go to work now. Lots of meetings scheduled....
Parents
  • aspork42
    aspork42 over 8 years ago

    Glad you found a use for that old floppy disk image

    Great case! For buttons, i try to link the together inside the case to keep them all lined up; so it is one big piece instead of many.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 8 years ago in reply to aspork42

    Linking is a good idea, I used square guides in the bezel and square flanges under the key caps to maintain alignment, but the tolerances need to be spot on.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 8 years ago in reply to dougw

    I ordered some window tint film, but it hasn't come in yet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 8 years ago in reply to dougw

    I ordered some window tint film, but it hasn't come in yet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 8 years ago in reply to dougw

    The window tint came in and it works great:

    Improving the micro:bit LED display