Design For A Cause 2021
  • Challenges & Projects
  • Design Challenges
  • Design For A Cause 2021
  • More
  • Cancel
Design For A Cause 2021
Blog ACE - Blog #7 - Improving the device construction
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: amgalbu
  • Date Created: 22 May 2021 12:45 PM Date Created
  • Views 1415 views
  • Likes 6 likes
  • Comments 6 comments
  • ace
  • design_for_a_cause_challenge
  • design for a cause - design challenge
  • design for a cause
  • design for a cause design challenge
  • design_for_a_cause_2021
Related
Recommended

ACE - Blog #7 - Improving the device construction

amgalbu
amgalbu
22 May 2021

In this post, I will provide some details about the case I built for the ACE wearable device

 

Building the case

Compared to the first version I made, I created a new case from a plastic bottle. The resulting case has many qualities

  • it's free
  • it's made of recycled materials
  • it's light and surprisingly rigid
  • it's easy to build (event if it needs some practice to get good results)

All in all, this technique it's a good solution to make parts with simple shapes quickly and at no cost

 

Bill of materials

The bill of materials for this build is

  • a board of plywood cut at the same width of the better. Length is not important
  • two round bars of aluminum. Again, length is not important here
  • a 66 centiliter plastic bottle
  • tape

Required tools are

  • scissors
  • cutter
  • hot air gun

 

image

 

Forming the case

Use same adhesive tape to keep the round bars close the the plywood board

Cut the top and the bottom of the plastic bottle place the plywood board with the aluminum bars inside the bottle

 

image

With the hot air gun, heat the plastic bottle until it shrink and takes the shape of the plywood board. I need some more practice here, because the temperature at which the thermoplastic material can be modeled is very closed to the temperature where the material becomes liquid. Of course, the material should not be melted down, or the final result will not be so good to look

 

image

This is the final result. As I said, I need more practice for a perfect result...

image

Remove the aluminum bars and then the plywood board. With the scissors and the cutter, finish the edges

imageimage

 

The batteries and the boards fits perfectly in the case. I wrapped batteries with some tape to be absolutely sure they will not slide out

 

imageimage

 

Finally, I added two clips made of harmonic steel to join the two halves and make a sort of clothespin you can pin to your trousers

 

image

And this is the final result

 

image

 

Update

After some practice results are getting better

image

The trick is to use to be patient and move the hot air flow away for a couple of seconds when the plastic starts shrinking

 

 

Previous postSource codeNext post
ACE - Blog #6 - Adding simplicityhttps://github.com/ambrogio-galbusera/ace2.gitACE - Blog #8 - Offloading computation to LSM6DS3
  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 5 years ago in reply to 14rhb +3
    Hello Rod Thanks for the advices! I will give a try for sure! Cheers
  • jduchniewicz
    jduchniewicz over 5 years ago +3
    Very good idea to reuse what you have handy! Keep the good work up
  • 14rhb
    14rhb over 5 years ago +2
    The low-cost housing is a great idea, thanks for sharing. I think PET bottles soften and melt at a temperature much lower than a typical hot-air gun, hence the scorching: maybe try a larger outer enclosure…
Parents
  • 14rhb
    14rhb over 5 years ago

    The low-cost housing is a great idea, thanks for sharing.

     

    I think PET bottles soften and melt at a temperature much lower than a typical hot-air gun, hence the scorching: maybe try a larger outer enclosure like bricks/old oven carcass/metal barrel to retain the heated air so you can keep the hot-air gun further away...would take longer but perhaps a more uniform shrink. A domestic oven would be nice but might leave a horrible taste on food cooked in there afterwards !

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 14rhb
    14rhb over 5 years ago

    The low-cost housing is a great idea, thanks for sharing.

     

    I think PET bottles soften and melt at a temperature much lower than a typical hot-air gun, hence the scorching: maybe try a larger outer enclosure like bricks/old oven carcass/metal barrel to retain the heated air so you can keep the hot-air gun further away...would take longer but perhaps a more uniform shrink. A domestic oven would be nice but might leave a horrible taste on food cooked in there afterwards !

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • amgalbu
    amgalbu over 5 years ago in reply to 14rhb

    Hello Rod

    Thanks for the advices! I will give a try for sure!

     

    Cheers

    • Cancel
    • Vote Up +3 Vote Down