Experimenting with Extreme Environments
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Extreme Environments
  • More
  • Cancel
Experimenting with Extreme Environments
Blog Backyard Secrets 1
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Extreme Environments to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 13 Jun 2024 5:35 AM Date Created
  • Views 1712 views
  • Likes 6 likes
  • Comments 7 comments
  • dougw
  • Pi Camera 3
  • PicoPorch
  • Midas MC42005A6W-SPTLYI-V2
  • Experimenting with Extreme Environments
  • Amphenol BrightConnX
  • Hammond Manufacturing
Related
Recommended

Backyard Secrets 1

dougw
dougw
13 Jun 2024

Intro

I really wanted to get the multi-camera system setup in the back yard to see how the whole system would work in practice. So this is an overview of where everything is placed and some images from the various cameras. I did get some unexpected video which I wasn't sure about including, so be warned if you are squeamish.

3 MotionEyeOS cameras in action

image

Backyard Video

The system is set up with 3 cameras on the deck and one camera inside the house. The PicoPorch motor controller and temperature display is on a table on the deck. Two of the cameras on the deck are running MotioneyeOS on Raspberry Pi Zero 2W hosts while the third deck camera is Raspberry Pi camera module 3 autofocus. All of the deck cameras are powered from the PicoPorch subsystem. The camera inside is a Raspberry Pi HQ camera hosted bt a Raspberry Pi 3B running MotioneyeOS.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Here is a shot from the 3 MotionEyeOS cameras in the rain:

image

Cam 3 in the rain

image

Looking at these shots I think it would be better to put an "mini umbrella" over each camera to keep the rain off the lens area, But at least the systems are all functioning properly in the rain. Score one for waterproof Hammond boxes..

Discussion

The system works - yay. It is always a big relief when powering up a complex system that took a long time to build. Tearing the system down to fix problems would not be high on my list of fun activities. I discovered my Wi-Fi could handle all 4 cameras, but if a couple of other computers were also using Wi-Fi the system would not connect all cameras. I also discovered these cameras are all pretty bad in low light, so I will need to provide illumination if I want to see anything in low light conditions. I did buy an IR illuminator, but have not hooked it up yet. I have a porch light which might show some activity but not with any quality. The Pi Camera Module 3 is a definite step up in camera performance. I like the autofocus capability, although I wonder how long it will last in continuous autofocus mode.

One unexpectedly useful feature is that the PicoPorch displays temperature with a backlit display. This makes it perfectly readable in all lighting conditions, particularly at night when my other outdoor thermometers are not readable.

The cameras are not setup yet with correct focus because there are logistics involved that impact other members of the family. Specifically I have to find a time when they are not using Wi-Fi.Relaxed

Links:

  • Garden Secrets System
  • ComputeCam and PicoPorch - Early Muddling
  • PicoPorch and ComputeCam - The Motor System
  • PicoPorch - LCD PCB & Bezel
  • PicoPorch power wiring
  • PicoPorch Motor Controller Demo
  • PicoPorch System Demo
  • PicoPorch Final Touches
  • Deep Dive On Kit Components
  • Backyard Secrets 1
  • MotionEyeOS Tutorial
  • Garden Secrets Project Summary
  • Experimenting with Extreme Environments Design Challenge
  • Pi 4 Compute Module Datasheet
  • Pi 4 Compute Module I/O Board Datasheet
  • Midas Display Datasheet
  • Enclosure Drawing
  • Enclosure Manufacturer Page
  • Antenna Datasheet
  • Connectors Datasheet
  • Sign in to reply
Parents
  • genebren
    genebren over 2 years ago

    Very cool!  I have been wanting to set up some cameras similar to what you have to catch more images of the birds, squirrels, raccoons, foxes and other nature in my backyard.  I will have to study your setup and see what I might want to do.

    Keep up the good work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to genebren

    It's the 'other nature' you have to be worried about e.g. neighbours doing strange things... Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 2 years ago in reply to beacon_dave

    Now that is a scary thought.  I would have to make sure that I pointed any and all cameras in save directions, mostly pointing upward to be sure.  We live on a half-acre so we should need to much of an upward angle to avoid capturing that sort of nature. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago in reply to genebren

    My backyard is totally enclosed by fences - anything that manages to find their way in is fair game...Camera

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago in reply to genebren

    MotionEyeOS has lots of options to capture images or video in any resolution based on motion triggering, or time , or manual.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 2 years ago in reply to genebren

    MotionEyeOS has lots of options to capture images or video in any resolution based on motion triggering, or time , or manual.