Experimenting with Extreme Environments
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Extreme Environments
  • More
  • Cancel
Experimenting with Extreme Environments
Forum Driving the LCD - share your experience
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Extreme Environments to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 37 subscribers
  • Views 6770 views
  • Users 0 members are here
Related

Driving the LCD - share your experience

Anthocyanina
Anthocyanina over 2 years ago

Hi! So, I've been working on the software for this challenge and have reached the point where i need to figure out the LCD. The datasheet has a character map and and the addresses for the position of each character. I don't have much experience with driving LCDs so I'm struggling with where to start. Have any of you figured out the LCD yet? 

I found a couple threads on the arduino forum that talk about this display, with people saying you could use the HD44780 libraries, or similar to drive it. I'll be trying that with an arduino board first, but still would like to hear about your experience with this display so far. 

Thank you!

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 2 years ago in reply to BigG +5
    This one is even simpler.. github.com/.../cfah2004ac community.element14.com/.../IMG_5F00_1443.mov
  • javagoza
    javagoza over 2 years ago in reply to jc2048 +5
    jc2048 A quick adaptation of your script. Works! Thanks for sharing! from smbus2 import SMBus LCD_CLEARDISPLAY = 0x01 LCD_FUNCTIONSET_4LINE_5x8DOTS_BITMODE = 0x38 LCD_DISPLAYCONTROL_ON = 0x0C LCD_ENTRYMODESET_LEFT…
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to shabaz +4
    update time! when i soldered the board to the LCD, which also served as an I2C breakout board, the flux residue was so hard to clean, i couldn't get it all out. I decided to remove that board, which i…
  • JWx
    JWx over 2 years ago

    I think that HD44780 is pretty standard, but - as you have written - driven mainly from small MCUs 

    Here is some example of using from Raspberry Pi:

    https://tutorials-raspberrypi.com/raspberry-pi-lcd-display-16x2-characters-display-hd44780/?utm_content=cmp-true

    didn't tried it but looks as one would expect it to look...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to JWx

    Thanks! yeah, the thing is, the LCD from the kit doesn't use an HD44780, but the arduino forum posts i found mention it could be driven as if it was the HD44780. This LCD doesn't appear to be commonly used by hobbyists, so there isn't much out there on practical implementations of drivers for it

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to Anthocyanina

    ok - sorry, I have only today got my kit so I didn't check the documentation yet.

    AFAIK HD44780 is considered some sort of standard, with many compatible chipsets. Our LCD seems to be based on/compatible with RW1063 ("For full design functionality, please use this specification in conjunction with the RW1063 specification. (Provided Separately)") - but, according to the datasheet, this driver is 2x8 character max, so maybe some variation of it is installed.

    RW1063  seems to have many interfaces: parallel 4b/8b, serial SPI and I2C, of which our module uses I2C

    https://www.crystalfontz.com/controllers/datasheet-viewer.php?id=227

    https://www.sparkfun.com/datasheets/LCD/HD44780.pdf

    After quick checking, RW1063 parallel interface looks similar to HD44780, so there is a good chance it can be driven with I2C HD44780 Arduino library...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 2 years ago

    I haven't received the kit yet. How are you connecting the LCD. Are you using external pull-ups resistors? Can you get the actual I2C address using a I2C scanner?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to javagoza

    I just opened the box, haven't connected anything yet, I've been working on the software side for the past few days waiting for the kit to arrive, and it just got here last night before i went to bed. I'll be trying the LCD in the next few days as i'm also busy with uni today and tomorrow

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to Anthocyanina

    Well! I haven't tried it, but this library looks promising if you're going to program in Python.

    charlcd · PyPI

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 2 years ago in reply to Anthocyanina

    Searching on the site comes up with this old thread:  Midas I2C LCDs 

    Midas also have a github page. Not sure if relevant: https://github.com/orgs/midas-displays/repositories

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 2 years ago

    I did a project, informally as part of the PiCasso design challenge, that used some I2C LCD displays. They were 2 rows of 16 and had the common Hitachi chip compatible registers. The datasheet was very messy, and muddled up the different variants in a really confusing way (the panel was available as either a I2C, SPI, or parallel build), so I had to do some experimenting to get the interface to work.

    /challenges-projects/design-challenges/picasso/b/blog/posts/9-pieces-of-pi-slice-2-manifesto-for-art-electronic

    That might give you some ideas, but be warned that the interface to your panel looks different to the one I had, so don't blindly copy what I did there.

    One important aspect to be aware of is that the controller on the panel has an embedded microcontroller, but it runs very slowly, to minimise the power consumption, so you have to be careful to ensure that it can keep up with your much faster device. One of the registers has a status bit that can be polled to see if the last command is finished. That's the fastest way of talking to the panel, if you can read the registers. In the case of the panel I chose, the I2C interface was write-only, so I had to instead look at the timings given by the datasheet for the various commands and make sure I exceeded them. If you use a library, it's likely that it will make use of that register bit and would fail if the registers can't be read, but hopefully the panel you've been given will allow for reading back from the registers.

    A second factor that may not be obvious, if you've not worked with the panels, is that the voltage for the LCD section has a separate pin to the logic supply for the controller. That's so that the contrast can be adjusted. The complication is, though, that internally the common voltage between the logic part and the segment drive part is normally the positive logic voltage, not the ground that you might expect. For the panel I used, the LCD supply (Vo) had to be about 6V, so ended up negative relative to the ground for good contrast (easy to achieve because the panel itself had a charge-pump generator on it). In the case of your panel, it looks like the LCD supply only needs to be about 4.5V, so your Vo will be approx 0.5V above ground and you can just use a pot between the logic supplies to supply it. Adjust it to the right sort of area initially with a meter, because if it's too far out the display will look blank rather than just having poor contrast.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to javagoza

    I’ve tried this library with an Arduino mega and it works fine

    https://github.com/JeffVi/Arduino-I2C-RW1063-0B-002

    image
    The Python charlcd doesn’t work for me without modifying. So I think I will try to adapt this to rpi next week

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to BigG

    This one is even simpler.. github.com/.../cfah2004ac

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
>