Experimenting with Supercapacitors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Supercapacitors
  • More
  • Cancel
Experimenting with Supercapacitors
Blog SuperCap Magic Meter Circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Supercapacitors to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 14 Aug 2023 3:42 AM Date Created
  • Views 2592 views
  • Likes 14 likes
  • Comments 16 comments
  • dougw
  • SuperCap Magic Meter
  • experimenting with supercapacitors
  • supercapacitors
Related
Recommended

SuperCap Magic Meter Circuit

dougw
dougw
14 Aug 2023

image

Intro

This episode describe the circuit in my SuperCap Magic Meter. The meter circuitry is designed into an Arduino shield which will plug onto an Arduino Uno R4 Minima. This MCU has a 14 bit A/D and a 12 bit DAC that will be used with the shield, allowing the voltages and currents to the supercapacitor under test to be measured and controlled. There is a 6 position rotary switch that selects which mode the meter will operate in. The charging circuit will charge at a constant 100 mA and the discharging circuit will discharge at a programmable rate set by the DAC. The reason for doing the schematic now is that I need to get the PCB on order to stay on schedule.

The SuperCap Meter Circuit

Here is a description of the circuit and how it works:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Here is the schematic of the supercapacitor meter shield:

image

Basically the circuit includes a constant current source fixed at around 100 mA and a separate variable current sink, both can be turned on and off by the UNO R4, which also can monitor voltages across both current shunts and across the supercapacitor under test. It also controls measurement cycles and the precise timing involved. Those cycles will be described in the software blog when the software has been tested. However you can deduce that for a constant current, capacitance can be calculated from the time taken to charge the capacitor. (C=i*dt/dv).

Since this is a one-off build, all voltages and currents can be calibrated by measurement with bench instrumentation. The discharge current is controlled by a DAC on the MCU. This is needed since the recommended measurement method suggests the discharge current should be 1 mA/F. All opamps are chopper-stabilized to minimize errors due to offset voltages and offset drift. The capacitor voltage measurement is buffered by a high impedance unity gain amp to minimize stray leakage from the supercapacitor under test. There are a couple of extra control FETs to ensure the current shuts off completely when the MCU wants it off.

There is an redundant current sense chip which will not be populated because it doesn't improve current measurement accuracy.

There are still a couple of tweaks in the works, such as adding more test points, but the PCB will be complete in a day or so..

Discussion

The PCB is being designed early to allow time for it to be fabricated.  This is before the software can be worked on so it needs to have enough flexibility to accommodate software revisions. I did think about how the firmware might help improve performance and accuracy, but that is a lot different than writing code. The Uno R4 has a USB port that allows interfacing to a host computer if the instrument needs to eventually talk to other instruments and computers, however that is not in the plan for this project. Some of the design choices for the system were dictated by what I had on hand, but there is also a significant amount of ordering to procure everything needed. At this time there is so much planning and design work going on, it is tough to put blogs together.

This circuit took longer than expected to design and has morphed quite a bit as I learned more about how supercapacitors work and what needs to be done to measure their parameters.

Next I need to spend time on the other 5 systems to get their PCBs designed and make sure all needed parts are at least on order. I have already ordered a bunch of stuff, but until the detailed design is done, I won't be sure I have everything on order.

Links:

 The Magic of SuperCaps 

 SuperCap Magic Meter Circuit 

 The SuperCap Rack 

 The SuperCap Magic Meter Shield 

 SuperCap Meter Shield Functional Test 

 SuperCap Magic Meter - Operational 

 SuperCap Magic Meter - Experimenting with Supercapacitors 

Experimenting with Supercapacitors Design Challenge

Cornell Dubilier Supercapacitor Technical Guide

Cornell Dubilier Supercapacitor Handling Guidelines

Challengers

Leaderboard

  • Sign in to reply
  • michaelkellett
    michaelkellett over 2 years ago in reply to dougw

    Thanks - I've taken a good look at it. I think you may regret that 100mA current limit - although of course it depends a lot on how much you use the meter with big caps.

    It's a problem testing normal caps too, the range of currents and pulse widths in common use is rather huge.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to dougw

    Interesting! That would be 2700s to fully charge/discharge a supercap, that's not far off from the 1C rate for rechargable batteries. Extra interested to follow along 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 2 years ago in reply to dougw

    Phew, I am not as old as I thought I was. I was worried that precision stuff with passive components had changed.

    The tail end question on how are you preventing the cap from being discharged is still outstanding.

    Good luck on your build. Thanks for the response.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago in reply to scottiebabe

    Cornell Dubilier recommends discharging at 1 mA/F when measuring.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago in reply to michaelkellett

    Good idea - I will do that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>