Experimenting with Supercapacitors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Supercapacitors
  • More
  • Cancel
Experimenting with Supercapacitors
Experimenting with SuperCapacitors Connectors Forum Is EDC and EDS family ESR really in ohm unit?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Supercapacitors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Subscribers 42 subscribers
  • Views 4274 views
  • Users 0 members are here
  • confusion
  • experimenting with supercapacitors
  • esr
Related

Is EDC and EDS family ESR really in ohm unit?

misaz
misaz over 3 years ago

In EDC (and EDS) datasheets ESR @1kHz for all caps is specified in Ohm unit

image

but in most other supercap families it is specified in mili ohm unit, for example from DGH datasheet:

image

Is it correct or is it mistake in datasheet? I searched for methods for measuring ESR, but unluckily I do not have required vaweform generator and I did not find any way how to easily replace it. So, my only way is checking documentation. I originaly thought that it is mistake and Gough Lui in his comparison blog ( What’s Super about Supercapacitors? – Part 2: Types, Vendors, Safety & Specifications ) also "corected" it to miliuohm units, but in comparison sheet (https://www.cde.com/resources/downloads/Briefs/Supercap-compare.pdf) it is refered with the same unit and I do not think that CDE did the mistake twice.

So my question to all who can measure ESR is what is true? Is ESR of EDC and EDS capacitor families in range of ohms or miliohms?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago in reply to Gough Lui +3
    There's some crazily-low ESR EDLC types in a flat format. TDK has some: https://product.tdk.com/en/search/capacitor/edlc/edlc/catalog For a project a while back I obtained one which is claimed 300…
  • Gough Lui
    Gough Lui over 3 years ago +2 verified
    Nice catch - my apologies, I didn't even notice the unit switcheroo. I had assumed they all used the same units based on reading the radial datasheets first that I didn't see that they said ohms! CDE are…
  • misaz
    misaz over 3 years ago in reply to Gough Lui +2
    Nice. Thanks for clarification. Looks like EDS and EDC has significantly different structure internally in comparison to radial supercaps.
Parents
  • Gough Lui
    +1 Gough Lui over 3 years ago

    Nice catch - my apologies, I didn't even notice the unit switcheroo. I had assumed they all used the same units based on reading the radial datasheets first that I didn't see that they said ohms! CDE are correct.

    If you look at my measurements, I would say it is correct as I was measuring multiple ohms for all coin cells:

     What’s Super about Supercapacitors? – Part 3: Measuring Capacitance & ESR 

    As a result, what I thought was out of spec is actually in-spec! A nice finding indeed.

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • misaz
    0 misaz over 3 years ago in reply to Gough Lui

    Nice. Thanks for clarification. Looks like EDS and EDC has significantly different structure internally in comparison to radial supercaps.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 3 years ago in reply to misaz

    Yes, it is likely they are something more akin to a battery in a paste composition perhaps or maybe layers, as there isn't space for the "scroll" type structures which increase surface area and reduce ESR as a result.

    That being said, I haven't opened up a coin-type one yet, but I might do now that you mention it ...

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • misaz
    0 misaz over 3 years ago in reply to Gough Lui

    thanks, but you do not need to destroy it just because of me. I am not chemistry expert, so I still will not understand it very much.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    0 anniel747 over 3 years ago in reply to Gough Lui
    Gough Lui said:
    I haven't opened up a coin-type one yet, but I might do now that you mention it ...

    Thumbsup That would be quite interesting. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 3 years ago in reply to misaz

    The challenge is to learn, and that's one way to do so. I've already destroyed many as part of my learning journey so that's all good. Might do it sometime in the next couple of days ... it'll probably make its way to my final blog too ...

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to Gough Lui

    There's some crazily-low ESR EDLC types in a flat format. TDK has some: 

    https://product.tdk.com/en/search/capacitor/edlc/edlc/catalog

    For a project a while back I obtained one which is claimed 300 milliohm and is thinner than a PCB (quite handy for hiding, for "dying gasp" scenarios if someone disconnects a battery!). However the Cornell Dubilier ones look a lot more robust, and I wonder if they maybe prioritised other features over ESR for that particular range. I've no idea though.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • baldengineer
    0 baldengineer over 3 years ago in reply to Gough Lui

    If you do open one up, please do so with care. The electrolytes used in coin cells tend to be very acidic. (Some vendors literally use a form of sulfuric acid.)

    I can't speak to the CDE construction, but I assume they use similar techniques to other vendors who make similar cells.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 3 years ago in reply to baldengineer

    Thanks for the tip - I did go through a few MSDSes in this blog but none of them seemed applicable to coin-cell types. Yes, protection is required as the compounds are known irritants, but quantities are relatively small.

    I suspect their design are based on being equivalents or replacements for the discontinued and rather popular Matsushita/Panasonic GoldCaps. Based on their brochure (https://industrial.panasonic.com/content/data/CP/PDF/Electric_Double/EDLC_TechnicalGuide_e.pdf), I'm expecting to find this:

    image

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • baldengineer
    0 baldengineer over 3 years ago in reply to Gough Lui

    On my first read of that datasheet, I noticed the word "electrolyte" was used without any chemical names. Then I saw on page 2 they say the electrolyte used in Gold Capacitors is non-water soluble. Which, to me, says it is not sulfuric acid.

    However, if an EDLC is using an "aqueous electrolyte," then I would think otherwise.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • baldengineer
    0 baldengineer over 3 years ago in reply to Gough Lui

    On my first read of that datasheet, I noticed the word "electrolyte" was used without any chemical names. Then I saw on page 2 they say the electrolyte used in Gold Capacitors is non-water soluble. Which, to me, says it is not sulfuric acid.

    However, if an EDLC is using an "aqueous electrolyte," then I would think otherwise.