Experimenting with Thermal Switches
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Thermal Switches
  • More
  • Cancel
Experimenting with Thermal Switches
Challenge Blog 3D Printer Thermal Runaway / Thermistor Tester #6 - Cutting Power to the 3D Printer when Thermal Sensor Detects Thermal Runaway
  • Challenge Blog
  • Forum
  • Documents
  • Files
  • RoadTests
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: guillengap
  • Date Created: 12 Feb 2022 7:42 PM Date Created
  • Views 5235 views
  • Likes 5 likes
  • Comments 4 comments
  • kemet
  • experimenting with Thermal Switches
Related
Recommended

3D Printer Thermal Runaway / Thermistor Tester #6 - Cutting Power to the 3D Printer when Thermal Sensor Detects Thermal Runaway

guillengap
guillengap
12 Feb 2022

Table of Contents

  1. Project Introduction
  2. Testing the OHD1-50B Thermal Sensor
  3. Testing the OHD1-50B and M-TRS5-60B Thermal Sensors
  4. Detecting Transition From ON to OFF on Thermal Sensors
  5. Activation of a Fan with a OHD1-30B Thermal Sensor
  6. Cutting Power to the 3D Printer when Thermal Sensor Detects Thermal Runaway
  7. Project Report Updated

**********************************************************************************************************************

Cutting Power to the 3D Printer when Thermal Sensor Detects Thermal Runaway

In this post I want to use a simple circuit without a programming board to demonstrate that when the thermal sensor detects the thermal runaway, then it interrupts the AC power supply to the 3D printer.

image

The control circuit can be made with discrete logic components or with microcontrollers. TTL, CMOS, LVTTL and LVCMOS logic circuit technologies can be used, below I indicate their working voltages.

  • TTL: 5V
  • CMOS: between 5V and 15V
  • LVTTL: 3.3V
  • LVCMOS: 3.3V, 2.5V or 1.8V

Schematic Diagram

Below you can see the electrical connections to test this project:

image

How does it work?

  • The OHD1-50B thermal sensor is normally closed at low temperature;
  • When the output of the control circuit is high (5V), the threshold voltage of the transistor base (0.6V) is exceeded and therefore a current begins to flow between base and ground. This current brings the transistor to the conduction state (between collector and emitter) closing the circuit of the relay coil and therefore activating it;
  • Under these conditions, the 3D printer turns on and can works;
  • The OHD1-50B thermal sensor is open at 50 degrees Celsius;
  • When the output of the control circuit is low (0V) the base of the transistor will also be low and therefore it will not allow current to pass between the emitter and the collector to activate the relay coil;
  • Under these conditions, the 3D printer turns off; and
  • When we deactivate the relay through the transistor, interrupting the current passing through the coil, the magnetic field present in it induces in it, for a brief moment, a very high voltage of opposite polarity at its terminals. This voltage spike known as "extra opening voltage" can damage the control transistor. To solve this problem, the simplest solution is to connect a reverse biased rectifier diode (1N4007) in parallel with the coil in such a way that it absorbs these voltage peaks of opposite polarity.

Experiment:

  • When the thermal sensor detects the 50 degree Celsius thermal runaway, the 3D Printer AC power supply turns OFF.

Assembling the Test Module

In the figure below you can see the test module once it has been assembled.

image

And now it's ready for thermal runaway testing.

image

I have used a 5v portable charger to power the DC circuit, since this device automatically turns off when it stops powering the circuit for more than 15 seconds. This way we guarantee a permanent power outage on our 3D printer until we arrive and find out that our 3D printer had a thermal runaway.

image

Test

In the video below I show you the tests carried out with the OHD1-50B thermal sensor with the 3D printer working in Preheat PLA mode.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Conclusion:

  • Using the OHD1-50B thermal sensor as a thermal switch to detects a thermal runaway on power module of the heated bed is a good idea. This experiment shows me that the 3D printer turs off on time when it's power module reaches 51 degree Celsius.
  • Please, I recommend you take precautions when working with alternating current, if you don't have experience, ask for the help of someone who does.
  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 4 years ago +1
    I would highly recommend adding a back-EMF protection diode in reverse across the relay coil as this will avoid a high voltage spike being generated as the relay turns off. Such a spike could stress the…
  • guillengap
    guillengap over 4 years ago in reply to DAB

    You are right! I didn't have a smaller box for this experiment. To finish my project, I will try to collect some of my experiments in this box... Kind regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 4 years ago

    Nice build.

    You have room to add some other items to the box.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • guillengap
    guillengap over 4 years ago in reply to Gough Lui

    Gough Lui, thanks for your contribution. I've already updated my post with this important observation... Kind regards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago

    I would highly recommend adding a back-EMF protection diode in reverse across the relay coil as this will avoid a high voltage spike being generated as the relay turns off. Such a spike could stress the power supply and transistor and contribute to eventual failure after an indeterminate number of cycles.

    - Gough