EZ-EV Challenge
  • Challenges & Projects
  • Design Challenges
  • EZ-EV Challenge
  • More
  • Cancel
EZ-EV Challenge
Forum Vape Cell EV - part V - 18650 vs Vape Cell
  • News
  • Projects
  • Forum
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join EZ-EV Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 58 subscribers
  • Views 170 views
  • Users 0 members are here
  • bms
  • ina219
  • 18560
  • uno q
  • cc/cv
Related

Vape Cell EV - part V - 18650 vs Vape Cell

saramic
saramic 2 months ago

shamelessly taking some extra time to complete the project as per the discussion in Challengers, Post your Projects!

Recap

Can random Vape Cells with unknonw histories be bundled into a smart battery system to ultimately power an EV, power wall or other device?

  • Vape Cell EV - part I - What’s in a Vape
  • Vape Cell EV - part II - RS485 comms
  • Vape Cell EV - part III - INA219 power monitor
  • Vape Cell EV - part IV - INA219 on battery charging

18650 vs Vape Cell

I setup a charging and discharging circuit controlled by the UNO Q, tracking using the INA219 power monitor and added a few relays to control cycling between charging (up to 4.2V and currnet draw down to 150mA) and discharging (down to 3.0V). The setup was far from pretty:

image

I hooked up a cheap AliExpress 18650 — label reads 2600 mAh 3.7 V 9.62 Wh

image

and got the following results:

image

Running a full charge then discharge at ~350 mA (10 Ω resistor):

Metric AliExpress “18650” Genuine 18650 (ref)
Claimed capacity 2,600 mAh (9.62 Wh) 2,000–3,600 mAh
Measured capacity 617 mAh 2,000–3,600 mAh
Claimed vs measured 24% of label ~100%
Discharge time to 3.0 V 107 min ~430 min
Avg discharge current ~347 mA —
Voltage sag (full cycle) 0.85 V over 617 mAh ~0.3 V
IR drop at switch-on 284 mV → ~0.81 Ω < 100 mΩ
Flat discharge plateau none — linear drop 3.5–3.7 V
CC charge current 460 mA —
Charge time (CC + CV to 200 mA) ~154 min —
Charge accepted ~604 mAh —

No flat discharge plateau, ~8× the internal resistance of a real cell, and only 24% of the claimed capacity — consistent with a re-wrapped 18350 cell (or a badly degraded pouch cell) inside an 18650 shell. The label’s 9.62 Wh figure is exactly 2,600 mAh × 3.7 V, confirming the capacity claim; neither figure is anywhere near what the cell actually delivers.


I hooked up a Vape Cell — label reads 18450 S50 3.7 V 5.18 Wh (~1,400 mAh claimed)

image

and got the following results:

Metric Vape Cell (18450 S50) AliExpress “18650”
Claimed capacity ~1,400 mAh (5.18 Wh) 2,600 mAh (9.62 Wh)
Measured capacity ~480 mAh (projected¹) 617 mAh
Claimed vs measured ~35% of label 24% of label
Discharge time to 3.0 V ~92 min (est.) 107 min
Avg discharge current ~320 mA ~347 mA
Starting voltage under load 3.35 V 3.85 V
Voltage sag (full range) 0.35 V over ~480 mAh 0.85 V over 617 mAh
IR drop at switch-on 725 mV → ~2.2 Ω² 284 mV → ~0.81 Ω
Flat discharge plateau none — linear drop none
CC charge current ~460 mA ~460 mA
Charge time (CV to 200 mA) ~71 min (CV only) ~154 min (CC + CV)
CV taper rate k ≈ 0.011 /min k ≈ 0.012 /min

¹ Projected from 7 min of stable discharge data at −3.5 mV/min; actual result expected ~14:00–16:00 UTC. ² Instantaneous IR at load switch-on; CV slope method gives ~0.21 Ω — the large discrepancy reflects polarisation overpotential built up during the 71-min CV charge phase.

The 18450 is a real cell format (18 mm × 45 mm vs 65 mm for 18650) — a genuine 18450 typically delivers 650–1,100 mAh. At 1,400 mAh claimed, the label is optimistic. At ~480 mAh measured it sits at 35% of that claim — a pattern eerily similar to the 18650’s 24%.

image

image

Conclusion

Both cells tell the same story: wildly inflated labels, real-world capacity a fraction of what’s printed.

The 18650 came in at 24% of its 2,600 mAh claim. The vape cell looks set to land at ~35% of its 1,400 mAh claim. Neither cell has a flat discharge plateau — a hallmark of healthy lithium chemistry. Both start discharging well below where a genuine cell would: the fake 18650 at 3.85 V under load, the vape cell at only 3.35 V (despite being fully charged to 4.13 V moments earlier).

One genuinely interesting finding: both cells have near-identical CV taper kinetics (k ≈ 0.012 /min). Different form factors, different histories, same electrochemical decay rate — the underlying chemistry is consistent even if the capacity isn’t.

For an EV or power wall application, neither cell is usable as-is. The fake 18650 delivers about 2.2 Wh; the vape cell about 1.6 Wh. A genuine 18650 would deliver 7–13 Wh. You’d need 4–8 of these salvaged cells to match one good one — and that’s before accounting for the matching problem, the safety risk of unknown-history cells, and the cycle life you’d be starting with.

The house didn’t burn down House with gardenXFire, winning!!

Next

I now have a bunch of vape cells that I need to prevent their terminals shorting, no doubt I will have to continue in some fashion to make this experiment come to a safe ending. Although I didn’t achieve all I wanted, I certainly made a solid dint in my knowledge of battery charging and some positive looking results.

Source

https://github.com/saramic/vape-cell-EV

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB 2 months ago

    Nice update.

    Clearly a case of buyer beware.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB 2 months ago

    Nice update.

    Clearly a case of buyer beware.