Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum RDM3600 RFID COMPONENT
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 29 replies
  • Subscribers 8 subscribers
  • Views 4845 views
  • Users 0 members are here
Related

RDM3600 RFID COMPONENT

e14 Contributor
e14 Contributor over 11 years ago

I have been using the Arduino platform for a while now(about 6 months) and I tried to hook up the RDM3600 RFID reader to my Arduino Uno and it seems like the reader does not communicate with the board. I present a card, but the serial interface does not display a serial number or anything. I am following this tutorial:

 

http://tronixstuff.com/2013/11/19/arduino-tutorials-chapter-15-rfid/

 

I modified the code to get an indication that the setup was complete:

 

#include <SoftwareSerial.h>

 

SoftwareSerial RFID(2, 3);

 

int i;

 

void setup()

{

  RFID.begin(9600);

  Serial.begin(9600);

  Serial.println("ready");

}

 

void loop()

{

  if (RFID.available() > 0)

  {

    i=RFID.read();

    Serial.print(i, DEC);

    Serial.println(" next");

  }

}

 

 

 

Does anyone have any idea why I don't get any communication from the RDM3600 when I present a RFID tag.

  • Sign in to reply
  • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to ellardpostma

    Excellent. Glad to hear you're all sorted. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ellardpostma
    0 ellardpostma over 10 years ago in reply to gadget.iom

    Just followed what you stated and the module worked fine.

    Maybe it made a difference that I took the circuit apart and hooked everything up again.

    Tried three completely different tags and all worked.

    Even going back to pin 2 worked for me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago

    Ok. Module arrived today! image

     

    I have hooked up the module to an Arduino Leonardo and run the following code:

    #include <SoftwareSerial.h>
    
    SoftwareSerial RFID(10, 11);
    
    int i;
    
    void setup() {
      RFID.begin(9600);
      Serial.begin(9600);
      Serial.println("ready");
    }
    
    void loop() {
      if (RFID.available() > 0) {
        i=RFID.read();
        Serial.print(i, DEC);
        Serial.println(" next");
      }
    }

    (Note the change from pins 2 & 3 to 10 & 11...)

     

    The output is as follows:

    2 next
    53 next
    49 next
    48 next
    48 next
    55 next
    48 next
    70 next
    49 next
    54 next
    69 next
    66 next
    69 next
    3 next
    2 next
    53 next
    49 next
    48 next
    48 next
    55 next
    48 next
    70 next
    49 next
    54 next
    69 next
    66 next
    69 next

     

    I have tried a couple of tokens in the 125KHz band, and they both work fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kgenskowsky
    0 kgenskowsky over 11 years ago in reply to e14 Contributor

    Mmm, Interesting.

    The main problem is that as you extend the range you will require more and more power to send to the antenna (Remember in passive devices the signal is used to convert to power and to send data so as you get farther and farther away card will get less power.). Just changing the size will not give you extend range. You will be able to get to 10cm as the standard is delivered maybe 15cm with a direct chip connection to a bigger antenna.

    So check on active antennas to extend further away.

     

    For this application i would recommend using different card technology and readers. I know they exist haven't research much to recommend one.

     

     

    Also as you extend the ranges the times will get longer between data transfer and I know some NFC protocols and chips have embedded security to disable longer than 10 cm communications.

     

    I founded a project that might be of help. I had on my old researches.

    http://www.eng.tau.ac.il/~yash/kw-usenix06/

     

    It could work if you convert the doorway in a complete antenna. So the tag will path thru the center of the field, Still the power might be to big and you might and end deleting Hard disks and any other magnetic data device so be careful when testing.

     

     

    Hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kgenskowsky

    I actually work for a public transportation fair collection devise manufacturing company as a mechanical engineer. The company I work for designed and developed a lot of the NFC technologies using in public transport.  I am participating in a hackathone this weekend and my team has proposed an assembly that reads RFID tags on a person as they walk through a door way without the person having to remove the tags from there pocket, wallet, etc...

     

    I have done a little research and have found that antenna diameter has a lot to do with the read range. I was hoping to increase the diameter of the RDM3600 antenna and maybe get a 10" (25.4cm) range so we could mount it on a door frame and read tags in a persons pocket as they walk through the door.

     

    It's just a proof of concept, and if it goes anywhere the real scientist would take over developing the product. But I need something that works to present to the judges.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kgenskowsky
    0 kgenskowsky over 11 years ago

    Paul is correct,   I have developed electronics for a bunch of years and a  generic recommendation i add a Serial port to all my projects as it is the easiest way to debug some times of firmwares.

     

    Regarding extending NFC,  be aware that extending the range on NFC devices is not a small task as the system is designed to be near field communication for security reasons.  We would not like some one reading and tampering with the data on the cards when taking public transportation image . Having said that I remember a proyect on Mifare cards that extended the range for some 1k cards. How much range you want to accomplish? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    kgenskowsky is right. You could connect the module directly to your computer.

     

    It is very common for computers to omit the Serial Port these days. You could use a cable similar to the one I linked-to earlier, and connect that to a USB port. The cable I suggested works on TTL level so there would be no logic level conversion required.

     

    The tag you linked to is an NFC tag that works on 13.56MHz, so if you want to continue using those tags you may need to look at alternative readers.

    I have one of these: SainSmart Mifare RC522 Card Read Antenna RF RFID Reader IC Card Proximity Module 3D Printing, Arduino, Robotics | Sainsm… modules that works on the frequency required but I haven't tested it yet. They are available from many places online.

    There is an article about increasing the range od these modules here: Extend range for MFRC522 RFID Reader

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kgenskowsky

    Kevin, I'm not sure this computer has a serial port. I only see USB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    I was using a WMATA SmartTrip card and some tags I found on Amazon:

     

    http://www.nxp.com/products/identification_and_security/smart_label_and_tag_ics/ntag/series/NTAG213_215_216.html

     

    I chose the RDM3600 because I can modify the antenna to increase the read range.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kgenskowsky
    0 kgenskowsky over 11 years ago

    Hi There,

     

    You can always use a RS232 converter to connect the module to a PC serial port and check that the module is working.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>