Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Seeking your opinion about an Experimenting with Flat Flexible Cables
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 14 subscribers
  • Views 3227 views
  • Users 0 members are here
  • molex
  • community survey
  • experimenting challenge
Related

Seeking your opinion about an Experimenting with Flat Flexible Cables

rscasny
rscasny over 3 years ago

imageLaunching an Experimenting Challenge can be a lengthy process. In general, we have a lot of meetings with the sponsor and a lot of brainstorming within the element14 team. Even choosing the prizes takes some time, with back and forth between us. Perhaps the thing that takes the most time is choosing the products. Sometimes I suggest products that I think will will work. Other times it's a collaboration between element14 and the sponsor. And sometimes we choose a product because it's something new; a good example of that is gesture sensors.

Recently, we were approached by a sponsor who makes flat flexible cables (FFCs) and would like to see element14 members experiment with them. There is a growing use of them, especially for space-constrained electronic sub-assemblies. And some of these FFCs have special characteristics such as EMI protection, hi temp environments, low voltage differential for signal integrity, impedance matching, and so on.

But designing an Experimenting Challenge means building the activity, the kit, and the experiments. That's where I like to ask community members. At face value, offering an Experimenting Challenge with FFCs seems like a hill to climb. Do we just send a kit of FFC's to the participants and see what they do? Or do we add in some other products to fill out the kit. (I did this with the Experimenting with Waterproof Connectors Challenge by adding a imageDFRobot SBC.) Of course, the more specific we get, the more specific (circuit count, length, & pitch, for instance) the FFCs would need to be.

But right now, I would like to toss around some ideas of how we could frame an Experimenting Challenge with FFCs. What should be in the kit? Types of experiments? Even, the kinds of prizes you would like to see for this activity. For myself, I see FFCs as a product we haven't talked about that much, but complements a lot of different kinds of electronics. I suspect that a lot of creative content and blogs could be created for this kind of activity.

Here are some relevant links:

Webpage

Essentials

If you have any thoughts about an Experimenting with FFCs challenge, I invite you to write a comment below.

Some polls

  • Sign in to reply
  • Cancel
  • DAB
    DAB over 3 years ago

    This could be a very interesting challenge.

    I remember in the early days we had to worry about the transmission line characteristics of flat cables and EMI effects.

    I am always surprised at the speeds the current cables can support.

    As for testing these types of cables, you do have a broad range of tests you could run, each with its own set of required equipment.

    I would like to see some testing done on propagation delays with length of cables. Capacitance and EM effects with ferrite cores. EMI effects. Transmission effects when the cable is placed over a CPU or memory chip. Induced EMI due to magnets.

    The sky is the limit to what you could do with just simple tests.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago

    What is needed - at a minimum the mating connectors. Adapter modules would be useful that have a mating connector and standard header. However, as Gough indicated, a custom PCB would likely be needed as well. A LiteVNA-64 might be nice too..Relaxed

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 3 years ago

    I think along with the FF cables, the proper mating connector also needs to be provided that can be soldered onto the PCB. Otherwise, it's going to be diffcult to use them. 
    I have a few potential use cases of FFCs, like connection displays on the front panel of an instrument with the microcontroller PCB, or sensors at the front with the analog hardware. 
    One good example of experiments with FFCs could be to test their capability to carry high speed signals and evaluate crosstalk as the wires inside the FFCs are very close to each other. 
    So a good project would be to use FFCs in some kind of RF/ High speed digital project (not too high of a freq. but something in kHz/MHz range). 
    Or with some kind of flexible and space contrained PCBs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago

    How will the technician fit the cables?

    Cutting, fitting connectors and installing board connectors will all impact this testing. Unless done correctly getting meaningful result will be a challenge.

    I have had reason to use flat ribbon cable in projects. I use JST-XH 2.54mm Wire Connector Terminal chrimps. Not as nice as a clean edge connector but can be done with minimal tools.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago

    I have a potential application. I want to connect little data acquisition modules to a mother board but the twist is that the modules must have at least 500V isolation. So each module will have its own isolating DC-DC converter and 4 isolated high speed signals (2 transmit and 2 receive). The idea is that each module connects to the motherboard by a multi way cable which must use LVDS drivers/receivers on each module to talk to LVDS ports on the FPGA on the motherboard. The flexi cable drivers and receivers are at earth referred potential.

    A classical motherboard with // connections is no help -  I need 10 modules to be star connected and I don't want the mechanical constraints of a Eurocard (or rack) system.

    So the first part of my plan was to do some signal integrity experiments with flexible cables. The minimum required signal speed is 20Mbits/s but 50 would be nicer.

    So to do this experiment I will need a scope and some custom built ends, one with FPGA and one with ADUM14x isolators LVDS transceivers. The cable will need at least 20 ways.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 3 years ago in reply to shabaz

    Lengths come from Molex website. Only offered lengths arenhere.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to misaz

    I think the table could just have values in increments of 10, since there's hardly any board size difference if there are spare conductors, nor any significant cost difference. For length, just (say) 100 and 200 would be OK because people could fold them if the length is too long.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago

    I always find I need one conductor more than the flat flex I choose!

    Anything 0.5 mm or higher pitch will be easily hand-solderable (especially with vertical connectors since they often had odd and even pins splayed on each side, so the pitch becomes 1mm, which then anyone can do with any iron, but even if it is on one side it is doable but that needs a bit more care). 0.4mm and smaller are intolerable to do by hand! Amazing what a difference that 0.1mm delta makes.

    1mm pitch is a pleasure to use, as easy and quicker than soldering pin headers.

    Unless space is super-constrained (which it usually is not, for non-consumer stuff) then it's good to just use (say) 10-way even if just a few conductors are needed, because there's not much board space saved between (say) a 4-way connector and a 10-way connector, and the extra conductors could be used for future expansion or doubling up, and less different inventory items.

    Example use-case where flat flex works out nicely:

    image

    There's a bit of an art folding flat flex for (say) 90 degree turns and positioning things just right to not have any slack on boards! I think flat flex is one of the best cabling inventions ever. Curious to know its history!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago

    This is probably going to be quite challenging to pull off. For one, the best use of FFCs are for board-to-board connections which necessitates the design of PCBs and soldering of surface mount connections which clamp onto the FFC (at least most of the time). There are some broad-pitch FFCs which can be used with crimp connections, but these are probably not being demonstrated. Note that hot-air soldering of FFC connections from the top is likely to be an exercise in futility - you are very likely to melt the plastic due to temperature issues ... but from the underside may be possible.

    If the key is to demonstrate high-speed connectivity, the test of a good connection requires not only a VNA but suitable test fixtures (i.e. open/through) designs to be able to cancel out the influence of the board and connector and determine the transmission characteristic of the FFC itself. Similarly, if we're talking about shielding, a full EMI/EMC set-up with a chamber or cell and a spectrum analyser will often be required. This is not really within the realm of most hobbyists - even myself, as an academic, may not find it easy to run such experiments even if I had the gear (which, sadly, I mostly do not).

    The FFCs on polyimide (Kapton) may take to being gently soldered to, but at such fine pitches, that's probably not the aim either.

    An LCD may well be a good way to demonstrate the stuff ... or a mezzanine board for a microcontroller, extension for a microSD UHS-I bus or something like that ...

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 3 years ago

    In last question I chosen Other. In this question missed option "I do not know".

    I currently have one personal project need in near future when I want to use flex cables but selecting products to flex cables kit is very hard task becase there are tons of variants. Flex cables in selected molex family have between 4 to 60 circuits and they also differ in length. How would you select cables to the kit? FOr example if you select 4pin cables and provide 10 length options that it would be fine for connecting i2c temperature sensors, but unluckily challengers will not be able to connect RGB TFT LCD display which requires about 30-50 wires. In other way if you provide 50 wire option it will be overkill for temperature sensor projects because even the connector will be larger than the whole sensor board. You can think about it form other side. Provide multiple pin count options but with fixed length. It will handle most needs but it will be less flexible in mechanical terms.

    In all case i recommend select one pitch option and provide all cables (and connector) with one selcted pitch. Otherwise it became complex even in this direction.

    The other related question is in provided quantity. For example for temperature sensor application challenger will mos tprobably utilize more than one cable (for connecting more sensors) but for display application one cable is sufficient.

    My idea is to enable challenger to describe his/her needs in application by providing filled excel template which you will provide to download. It can look for example as follow:

    image

    The lengts which I selected in column are standard lengths in which molex offers their cables but note that not all combinations are possible and table requires furhter checking (for example shortest 60pin is 51 and 30 mm variant with this pin cout does not exists), so table require furhter checking before publishing.

    I am not sure that my idea is the best one because there may be some organisational troubles like stock unavalaiblity of some variants which user may select. So take it like an idea but most probably it would be better to go different way and just provide kit of preselected cables and let challenger to adapt their projects and expriments to parts from provided kit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>