N-gaged Design Challenge
  • Challenges & Projects
  • Design Challenges
  • N-gaged Design Challenge
  • More
  • Cancel
N-gaged Design Challenge
N-Gaged Blog Blog #5 : Smart Poultry Farm Monitoring System : Conclusion and Future Enhancements
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wesee
  • Date Created: 22 May 2022 5:39 AM Date Created
  • Views 3724 views
  • Likes 1 like
  • Comments 0 comments
  • smart poultry farm
  • iot system
  • OMEGA’s Layer N EcoSystem
  • n-gaged
  • remote monitoring
Related
Recommended

Blog #5 : Smart Poultry Farm Monitoring System : Conclusion and Future Enhancements

wesee
wesee
22 May 2022

This is the last blog of the Smart Poultry Farm project.  I will do a summary about the project and talk about possible enhancements to the smart farm itself and the Layer-N cloud. 

Blog #1: This is an introduction.  I talked about the concept of my proposed system and some pictures about the kit being used.

Blog #2: This blog explained how to setup and configure the hardware and software.  How to register and navigate the Omega Layer-N Cloud was described in the blog.

Blog #3: Here I described how I set up the gateway, smart sensors and Layer-N cloud configuration for the Smart Farm system.  I showed some pictures of the Smart Farm scenario.

Blog #4: In this post, I configured the alarms and notification setting in the Layer-N cloud.  Few screen captures of the dashboard about the gateway and sensor's reading were displayed.

At the current stage, the smart farm, via Omega Layer-N cloud, has these two capabilities: 

1) remotely monitor the farm's temperature, humidity and light intensity;

2) send alarms and alerts by email and SMS notifications

image

image

This is a simple project.  Of course, there are few enhancements that can be added to the project.  Here are some of them:

1) the system can send mmands to control the temperature, humidity and light intensity whenever these metrics are out of the range of condusiive conditions;

2) add more types of sensors such as gas and moisture, etc;

3) using deep learning, AI model can classify chicken "speech" and inprove poutlry production.

.

As for the Omega cloud, I hope the following features will be included in the future:

1) customisation of the dashboard is allowed.  Charts in the form of widgets can be moved around via drag-and-drop action;

2) a developer friendly API for easier and better integration to other system;

3) a webhook setting for better and deep integration with other system;

4) ability to customise the edge's (both gateway and smart sensor) firmware so that developers can add additional functions and features to the system.

.

.