Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog [Pi IoT] Plant Health Camera #7 - Synchronizing the cameras
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
  • Author Author: gpolder
  • Date Created: 8 Aug 2016 9:39 AM Date Created
  • Views 2054 views
  • Likes 5 likes
  • Comments 6 comments
  • pi 3
  • pi-iot
  • rpi.gpio
  • trigger
  • pi_camera
  • pi iot design challenge
  • plant health camera
Related
Recommended

[Pi IoT] Plant Health Camera #7 - Synchronizing the cameras

gpolder
gpolder
8 Aug 2016

This week I was traveling again, so unfortunately I didn't have much time to work on the project.

Therefore I will share my thoughts on how to synchronize the two cameras.

 

Previous posts:

[Pi IoT] Plant Health Camera #6 - Putting the slave Pi to work

[Pi IoT] Plant Health Camera #5 - OpenCV

[Pi IoT] Plant Health Camera #4 - Putting the parts together

[Pi IoT] Plant Health Camera #3 - First steps

[Pi IoT] Plant Health Camera #2 - Unboxing

[Pi IoT] Plant Health Camera #1 - Application

 

Intro

In the previous post I explained how the two cameras are combined, using the master and slave Pi. Here I will show how the two Pi's are connected hardware wise, and how the two images are taken simultaneously from the two systems.

Hardware setup

The power for the Pi B+ comes from the Pi 3's header block, as shown in the image below.

I wrote some python code which will run on the slave system. It will wait for a trigger pulse on GPIO 23 and then take an image and save it on the share as described in the previous post. The master system will output the trigger on GPIO 18.

image

 

Software

Below is the python code which runs on the slave system, it is based on an example I found on the internet (camera - Problems triggering via GPIO - Raspberry Pi Stack Exchange).

If not done already rip.gpio needs to be installed:

sudo apt-get install python-dev python-rpi.gpio

 

slave_camera.py:

 

#!/usr/bin/python


import RPi.GPIO as GPIO
import socket
import time
import picamera

# PiCamera Setup

camera = picamera.PiCamera()
camera.ISO = 100

image_num = 1
ready = 1

# GPIO Setup

GPIO.setmode(GPIO.BCM)
GPIO.setup(23, GPIO.IN, pull_up_down = GPIO.PUD_DOWN)


# Begin Loop
try:
  while True:

  if GPIO.input(23):

  camera.capture('/home/pi/planthealthcam/slave_image.jpg')
  print('input from master on gpio 23, Picture taken!')
  ready = 1
  image_num += 1
  time.sleep(3)

except KeyboardInterrupt: # trap a CTRL+C keyboard interrupt  
  GPIO.cleanup() # resets all GPIO ports used by this program 

 

In order to start this script on every boot, I added it to /etc/rc.local:

 

#!/bin/sh -e
#
# rc.local
#
# This script is executed at the end of each multiuser runlevel.
# Make sure that the script will "exit 0" on success or any other
# value on error.
#
# In order to enable or disable this script just change the execution
# bits.
#
# By default this script does nothing.

# Print the IP address
_IP=$(hostname -I) || true
if [ "$_IP" ]; then
  printf "My IP address is %s\n" "$_IP"
fi

python /home/pi/planthealthcam/slave_camera.py &

exit 0

 

In a following post I will describe the python code on the master system.

stay tuned.

  • Sign in to reply

Top Comments

  • gpolder
    gpolder over 10 years ago in reply to element14Dave +2
    Hi element14Dave , thanks, any news on the missing Sense HAT, WiPi Dongle and the PiFace digital? In particular the Sense HAT, would be great to add Temperature, Barometric pressure and Humidity to the…
  • gpolder
    gpolder over 10 years ago in reply to DAB +1
    DAB , true it's not super time sensitive, but as the plants can move, for instance due to the wind, I prefer to take the NIR and RED image at the same time. Gerrit.
  • gpolder
    gpolder over 5 years ago in reply to tonyteyer +1
    Hi Tony, thanks for your interest in this project. 2- How do I put the code on the Pi slave? vi or vim? you indeed can logon with a terminal (putty on windows, Terminal on mac) and use vi or any editor…
Parents
  • tonyteyer
    tonyteyer over 5 years ago

    Hi Gerrit, I'm trying to replicate your project and got stuck in the code to sync the cameras. i have 2 Pi's 3b+ instead of the ones you use

     

    I have some doubts:

    1- On the step 6 "Putting the slave Pi to work" we deactivate the graphical user interface, and you mention that the code goes in the pi slave that does not have a graphical interface. that brings me to the first question

    2- How do I put the code on the Pi slave? vi or vim?

    3- and where i should save the file "slave_camera.py".

     

    I know it has been a while since you did this project, but I am very interested in finishing it. Thanks for your contribution.

     

     

    Tony.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • tonyteyer
    tonyteyer over 5 years ago

    Hi Gerrit, I'm trying to replicate your project and got stuck in the code to sync the cameras. i have 2 Pi's 3b+ instead of the ones you use

     

    I have some doubts:

    1- On the step 6 "Putting the slave Pi to work" we deactivate the graphical user interface, and you mention that the code goes in the pi slave that does not have a graphical interface. that brings me to the first question

    2- How do I put the code on the Pi slave? vi or vim?

    3- and where i should save the file "slave_camera.py".

     

    I know it has been a while since you did this project, but I am very interested in finishing it. Thanks for your contribution.

     

     

    Tony.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • gpolder
    gpolder over 5 years ago in reply to tonyteyer

    Hi Tony,

     

    thanks for your interest in this project.

    2- How do I put the code on the Pi slave? vi or vim?

    you indeed can logon with a terminal (putty on windows, Terminal on mac) and use vi or any editor you are convenient with.

    You also can use ftp, curl, ..... It's linux, so you are flexible.

     

    3- and where i should save the file "slave_camera.py".

    Wherever you want, but it need to correspond with rc.local, so in my example it is:

    /home/pi/planthealthcam/slave_camera.py

     

     

    best,

    Gerrit.